The German Aerospace Center opts for Kistler accelerometers to perform its vibration tests

The Institute of Aeroelasticity at the German Aerospace Center uses large numbers of accelerometers from Kistler for vibration tests and modal analyses, both on the ground and in the air. For example: the vibration behavior of ISTAR, the new research aircraft, was accurately imaged with the help of various technologies and advanced piezoelectric sensors.

Streamlined sports cars and coupés have given the general public some awareness of the important part played by aerodynamics in vehicle and aircraft design. But this is not so much the case with aeroelastics, the branch of science that investigates the vibration behavior of aircraft and other vehicles. There is even an institute dedicated to this discipline at the German Aerospace Center (DLR): the Institute of Aeroelasticity in Göttingen, which has a team of around 80 employees. They perform tasks such as structural dynamic testing of aircraft, helicopters, wind turbines and turbo engines so their vibration characteristics can be analyzed in detail.

The Institute carries out wind tunnel tests that investigate the coupling of airflow and structural vibrations (known as flutter behavior), and also simulations to predict aeroelastic behavior as accurately as possible (these even include the digital twin). But the main focus is on ground vibration tests (GVT). These meticulously planned tests use vibration exciters to cause artificial vibrations at various points on the prototype of a new aircraft (wings, tail unit, fuselage, etc.). They are recorded by accelerometers to determine the forms of the structural vibration – known as modes.

The right measurement technology for every testing requirement

Julian Sinske joined the DLR in 2013 and he has held the post of Teamleader Structural Dynamic Tests since 2018. He explains the goals and conditions for a GVT: “Generally speaking, the ground vibration test only takes place six to eight weeks before the maiden flight – and with that timescale, the procedure has to be performed efficiently. For the test, the aircraft is mounted so that its behavior is similar to its in-flight behavior – with damping influences due to the landing gear and tires excluded as far as possible. The experimental results from the GVT can be used to validate the manufacturer's simulation model. In most cases, this is the prerequisite for further in-flight testing of the prototype.”

Over 200 IEPE accelerometers from Kistler were used for the ground vibration tests on ISTAR (In-flight Systems & Technology Airborne Research), the new research aircraft that joined the DLR's fleet in 2020. In addition to these instruments, 62 more IEPE (PiezoStar) and capacitive MEMS accelerometers (K-Beam) from Kistler are permanently installed in ISTAR for in-flight testing. Frank Busch, a Sales Engineer at Kistler, explains how these applications differ: “The MEMS sensors, which measure statically, also take account of gravitational acceleration because they are optimized for low frequencies in the 0 to 50 Hz range. That means they can record the aircraft's flight maneuvers at the same time. In this ground vibration test, the MEMS and IEPE sensors installed permanently in the aircraft could be operated in parallel with the dynamic IEPE sensors and compared with them. The GVT sensors are affixed to the outside of the plane – just temporarily, only for the duration of the test.”

All of these instruments form part of a comprehensive measurement system that the aeroelastics specialists headed by Julian Sinske use to continuously record all the ISTAR data, which they can then evaluate over periods of many years. “By taking this Big Data approach, we create the basis for the digital twin – and that allows us to set up structural health monitoring, for example,” he notes.

We’ve been collaborating successfully with Kistler ever since we first made contact with them at the Space Tech Expo some years ago. We use their sensors for projects involving both large and small aircraft, and also in the wind power segment.”

Julian Sinske, Teamleader Structural Dynamic Tests at the Institute of Aeroelasticity, DLR

 

Robust, flexible instrumentation – plus temperature stability 

Kistler was also selected to equip the ISTAR research aircraft – thanks in particular to an outstanding innovation. The single-axis transducers for the GVT feature a measuring element mounted so that it can be rotated. This allows flexible alignment of the sensor in two spatial directions. “As the result, specific parts of the aircraft can be instrumented differently without sacrificing measurement channels for three-axis sensors, for example,” Sinske adds. This is why the DLR and the Institute are so highly satisfied with Kistler: “Several factors influenced our decision to opt for Kistler's flight test sensors: the high temperature stability of the IEPE sensors and the high signal quality of the MEMS sensors, combined with good advisory support – especially from Dr. Thomas Petzsche. The measurement equipment was ready to operate from day one, and it was equally convincing in terms of design and cost efficiency.”

For the GVT, the research aircraft was excited at about 10 points in succession – often symmetrically, and at several excitation levels so that nonlinearities could be detected and closely adjacent modes could also be differentiated. A taxi vibration test (TVT) has already been performed as well. In this case, the aircraft moves out of the hangar and across the runway at the DLR's Research Airport in Braunschweig; this allows determination of its vibration behavior while it is traveling slowly. The team continued to perfect the methods and procedures as the tests were carried out. As part of a research project on data evaluation, for instance, an AI algorithm was used to achieve faster evaluation and eliminate the human factor. “But it's not yet good enough to replace an experienced engineer – especially in difficult cases,” Sinske points out with a smile.

Data evaluation with the help of artificial intelligence

Students at the Institute have also developed an augmented reality app that can be used on a smartphone to check and simultaneously document the presence of each sensor, including its number, alignment and position, etc. In some cases, over 500 sensors have to be positioned with an accuracy of one centimeter – so this innovation makes the work far easier. “Setups of this sort often have to be completed in just a few days by people working shifts. So it's important to discover any anomalies as quickly as possible, for example if a sensor comes loose or the cable is not plugged in correctly. The earlier the fault is detected during that hectic phase, the less chance there is of falsified measurement results once the action really begins,” Sinske continues.

The Ground Vibration Test and Taxi Vibration Test results have already undergone comprehensive evaluation, and a start has also been made on updating the aircraft manufacturer's computer model. Thanks to these efforts, the aeroelastic part of the digital twin for the ISTAR research aircraft is now within reach. Julian Sinske's final comment: “We're highly satisfied with the way Kistler has implemented the measurement technology. The sensors are robust and they perform excellently. That's why we've already put in several repeat orders, including different cable lengths of one, two, five and ten meters. With so many sensors, this always allows us to ensure optimal cabling – as short as possible – so routing of the signals is guaranteed. We will definitely be opting for solutions from Kistler for future projects in other fields too – such as spaceflight, wind power or innovative air taxis.”

2022. 5. 4.
Daimler Buses relies on MaDaM and jBEAM to further develop of its electric city buses.
2022. 4. 11.
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
2022. 1. 14.
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
2021. 11. 18.
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
2021. 10. 12.
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
2021. 9. 14.
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
2021. 9. 9.
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
2021. 9. 3.
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
2021. 7. 2.
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
2021. 6. 22.
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
2021. 6. 2.
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
2021. 4. 26.
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
2021. 4. 13.
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
2021. 3. 22.
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
2021. 2. 8.
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
2020. 10. 5.
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
2020. 9. 18.
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
2020. 8. 20.
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
2020. 7. 22.
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
2020. 6. 9.
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
2019. 11. 15.
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
2019. 10. 23.
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
2019. 8. 15.
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
2019. 7. 17.
Turkey opts for weight enforcement with WIM technology from Kistler
2019. 6. 24.
For the next manned flight to the moon: safety that can be measured
2019. 6. 20.
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
2019. 5. 14.
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
2019. 4. 18.
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
2019. 4. 2.
NFL's Jaguars boost their fitness levels with Kistler.
2019. 3. 25.
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
2019. 3. 18.
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
2018. 12. 17.
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
2018. 11. 27.
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
2018. 10. 10.
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
2018. 10. 8.
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
2018. 8. 31.
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
2018. 8. 14.
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
2018. 7. 16.
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
2018. 4. 11.
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
2017. 11. 14.
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
2017. 8. 11.
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
2017. 1. 4.
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
2016. 12. 22.
Kistler makes progress in vehicle development possible
2016. 12. 22.
Kistler Sensor Correvit® SFII measures world record
2016. 12. 20.
Kistler sensors deliver a maximum in data quality under any conditions.
2016. 11. 7.
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
2016. 10. 5.
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
2016. 8. 17.
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2016. 2. 19.
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
2015. 11. 4.
Piezoelectric Measurements with CompactRIO™
2015. 6. 15.
Measurement Solutions for Automotive Test Systems
2015. 5. 8.
Quality Assurance in the Automotive Industry
2015. 3. 2.
How Brose improves the quality of its two-component production and automatically separates defective parts
2014. 12. 2.
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
2014. 12. 2.
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
2011. 8. 23.
HEWI and its Customers Benefit from Cavity Pressure Technology
2011. 2. 15.
End-to-end process monitoring for critical medical moldings
2011. 2. 7.
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
연락처
Max 25 MB