Shanghai University of Sport chooses force plates from Kistler for pole vault research

Professor Liu Yu and his Shanghai-based team of colleagues and students are undertaking research into pole vaulting and performance by top athletes. Assisting the researchers: force plate technology from Kistler, including a new development for the planting box to supply critical biomechanical data about the complex sequence of movements in this sport.

The pole vault occupies a unique position among track and field events. In less than a minute, athletes have to complete a technically challenging routine that comprises several different movement sequences: the run-up with the pole, planting, take-off, turn and bar clearance – and finally, a safe landing. This is an event that sets demanding requirements for the athletes – but not only in terms of purely physical performance. They, and especially their coaches, must also fully understand every dynamic detail of the sequence of movements in the vault.

Since 2018, the Sport Performance Research Center (SPRC) at the Shanghai University of Sport (SUS) has completed several projects involving high-level Chinese and foreign athletes, aimed at analyzing and processing the full range of motions involved in pole vaulting. Biomechanical force plates from Kistler deliver outstandingly accurate measurements of dynamic processes, and are also easy to install: due to these advantages, they have played a crucial part in helping the researchers to understand the instantaneous force changes that occur during a pole vault.

Basic research and development of elite athletes

SUS was founded nearly 70 years ago, making it one of China’s longest-established higher educational institutions specializing in sports. The SPRC was added to the university in 2003: its superb hall, including a range of biomechanical equipment, was built with the help of government and municipal funding. The center covers three main research areas. First, biomechanics in competitive sport, with the focus on top athletes and national team members (as well as their trainers, of course): the goal here is to improve performance and athletic abilities in general. The second key area involves collaboration with manufacturers of sports apparel such as footwear, shirts and protective equipment, so that biomechanical information can be exploited to prevent injuries and develop athletes' performance. And the SPRC's third area of interest is research into innovations in various fields: neuropriming is one example. 

The SPRC's pole vault project fulfills a dual purpose: on the one hand, China's best athletes are prepared for the next track and field season in the run-up to the Olympic Games, as part of the "Technology-empowered Olympics" initiative launched by the General Administration of Sport of China. The second objective is to study a sport that is chronically under-researched in China, following on from the success of similar programs for sprint, swimming, and ball sports.

Precisely capturing force actions in the movement sequence

"In earlier biomechanical research, it was actually quite difficult to capture such a wide range of 3D motions in their entirety,” according to Professor Liu Yu, Dean of the Research Institute at SUS, a national award-winner and Fellow of the U.S. National Academy of Kinesiology, who heads the project. He continues: 

Thanks to the system from Kistler, we can capture the movements of the body's center of gravity and also of individual parts of the body, as well as the resultant angles and the length, frequency, and speed of the run-up. What's more, the forces in all three spatial dimensions are measured – including, in particular, the force exerted by the athlete on the ground in his or her last three steps, and when the pole is planted in the box. This kind of information is not available to coaches who only observe athletes with the naked eye."

Professor Liu Yu, Dean of the Research Institute at Shanghai University of Sport

 

In research of this sort, data and model quality is critically dependent on precise acquisition of movements and force measurement in real time. Knowing this, the SPRC decided to opt for leading kinematics and biomechanics technology right from the start of the project. Towards the end of 2018, initial tests with three 9287C force plates from Kistler were carried out in the open-air facility; plans were then drawn up for further integration, including the installation work needed for the pole vaulting project. This already allowed trainers and students to try out the equipment and get to know it, greatly reducing the amount of work and time needed to set up the tests.

With assistance from Kistler, it took only half an hour to install the three sets of force plates in the dedicated measurement track for the project in the hall. But to ensure that the data on each pole vaulter's last three steps was as accurate as possible, the force plates had to be aligned in exactly the right positions prior to every test. This was easily achieved thanks to the simple installation procedure for the equipment, so full data acquisition for three athletes was completed in just one day.

Custom measurement solution for the planting box

In addition, the Kistler engineers developed a multi-component force measuring box specifically intended for pole vaulting applications. The box features an exceptionally robust design, and it precisely replicates the function and geometry of the actual planting box. The integrated piezoelectric sensors supply an accurate force curve – from the moment when the pole touches the planting box, as the force increases continuously, until the tension built up in the pole due to deformation is released and the force then decreases as the athlete gradually lets go of the pole. There are extreme changes in the direction and magnitude of the force within fractions of a second – and these fluctuations can only be captured properly by a measuring instrument that has a wide measurement range, high natural frequency and outstanding dynamic sensitivity.

As an international expert on sports biomechanics, Professor Liu emphasizes the great importance of this project: "In conjunction with optical measurement systems, force plates from Kistler have given us a complete picture of the kinematics and dynamics of the athlete throughout the entire sequence of a pole vault. Based on the data we have obtained, we're able to carry out technical analyses, give training recommendations, and compile an accurate model of the movements and performance of each individual athlete."

2022. 4. 11.
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
2022. 1. 14.
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
2021. 11. 18.
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
2021. 10. 12.
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
2021. 9. 14.
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
2021. 9. 9.
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
2021. 9. 3.
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
2021. 7. 2.
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
2021. 6. 22.
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
2021. 6. 2.
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
2021. 4. 26.
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
2021. 4. 13.
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
2021. 3. 22.
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
2021. 2. 8.
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
2020. 10. 5.
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
2020. 9. 18.
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
2020. 8. 20.
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
2020. 7. 22.
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
2020. 6. 9.
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
2019. 11. 15.
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
2019. 10. 23.
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
2019. 8. 15.
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
2019. 7. 17.
Turkey opts for weight enforcement with WIM technology from Kistler
2019. 6. 24.
For the next manned flight to the moon: safety that can be measured
2019. 6. 20.
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
2019. 5. 14.
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
2019. 4. 18.
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
2019. 4. 2.
NFL's Jaguars boost their fitness levels with Kistler.
2019. 3. 25.
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
2019. 3. 18.
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
2018. 12. 17.
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
2018. 11. 27.
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
2018. 10. 10.
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
2018. 10. 8.
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
2018. 8. 31.
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
2018. 8. 14.
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
2018. 7. 16.
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
2018. 4. 11.
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
2017. 11. 14.
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
2017. 8. 11.
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
2017. 1. 4.
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
2016. 12. 22.
Kistler makes progress in vehicle development possible
2016. 12. 22.
Kistler Sensor Correvit® SFII measures world record
2016. 12. 20.
Kistler sensors deliver a maximum in data quality under any conditions.
2016. 11. 7.
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
2016. 10. 5.
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
2016. 8. 17.
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2016. 2. 19.
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
2015. 11. 4.
Piezoelectric Measurements with CompactRIO™
2015. 6. 15.
Measurement Solutions for Automotive Test Systems
2015. 5. 8.
Quality Assurance in the Automotive Industry
2015. 3. 2.
How Brose improves the quality of its two-component production and automatically separates defective parts
2014. 12. 2.
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
2014. 12. 2.
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
2011. 8. 23.
HEWI and its Customers Benefit from Cavity Pressure Technology
2011. 2. 15.
End-to-end process monitoring for critical medical moldings
2011. 2. 7.
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
연락처
Max 25 MB