How Zinkteknik achieved zero-defect production with Kistler test automation systems

As one of Europe’s leading zinc casting specialists, Zinkteknik aims for utmost quality throughout its portfolio of die-cast parts. These include safety components for seat belt systems in cars, where quality is absolutely critical. By integrating test automation systems from Kistler into its fully automated production lines, this Swedish manufacturer was able to attain true zero-defect production – even for very high volumes. 

Most of us know zinc as a material that can protect iron and steel parts against corrosion. But it is capable of doing far more than that: for example, it can be used for die-casting of high-quality parts in large volumes. The team at Zinkteknik AB knows almost everything about zinc: at the headquarters of this manufacturing company in southern Sweden, you can even attend a “Zinc School” to deepen your knowledge of this versatile material and its industrial applications. Zinkteknik’s CEO Jens Svensson explains the advantages of working with the material: “Zinc is very design-friendly. You can realize almost any geometry from a single block. It’s a highly resilient and ductile material, but it also allows narrow tolerances. A huge variety of different coatings are possible with zinc, and it’s ideal for low-energy recycling thanks to its relatively low melting point.” 

Zinkteknik has achieved successful growth ever since it was founded in 1985. Its 170-strong workforce is split between two European sites – at Bredaryd in Sweden, and Mostar in Bosnia (since 2005). Precision parts manufactured at these plants are mainly supplied to the automotive industry, but also to customers in other sectors including electronics, ICT and construction. “The requirements always get higher over time, especially for safety-critical parts in the automotive industry such as seat belt components. We manufacture more than 300 million parts per year, and we focus our efforts on one goal above all: the highest possible quality,” Svensson adds. As a Tier 2 supplier of parts to OEMs and car manufacturers all over the world, Zinkteknik has to meet demanding quality standards – and “zero-defect production” is the motto for the automotive industry in the 21st century.

Reliable and efficient quality assurance

Per-Erik Edman, Quality Assurance Engineer at Zinkteknik, explains the challenges of achieving zero-defect production in his specialty field of zinc die-casting: “With quantities of 30 to 40 million for just one single part in a year, our volumes are so high that there’s no chance of inspecting each individual part. This prompted us to implement in-process monitoring to ensure the quality of the parts we produce.” Edman’s team had already reduced the complaint rate to less than ten per year and series – a very low figure in relation to the enormous volumes involved. Now the question was: how to improve on that success and attain zero-defect production? “As it is often the case, the last step is the most difficult. But we had a stroke of luck: one of our customers, a Tier 1 supplier, recommended us to take a look at test automation solutions from Kistler,” Edman continues.

Shortly after making first contact with Kistler in 2016, Zinkteknik ordered a KVC-821 – the latest-generation automated test and sorting system for end-of-line quality assurance. Zinkteknik’s engineers joined forces with Kistler’s image processing experts to determine the best camera configuration for identifying faulty automotive safety parts. “When we visited Germany to work on the fault analysis with the Kistler team, we had a very open discussion on what is possible and how best to achieve the desired results. The Kistler experts were also very clear about what was not possible – and at the same time, they explored various alternative ways of meeting the challenge.”

With the help of the KVC-821 from Kistler, Zinkteknik was able to efficiently check millions of manufactured zinc parts for geometry and surface defects – and before long, they reached the all-important zero-defect goal. “The result was very convincing”, Edman recalls. “We supply one of our biggest customers with critical automotive parts that are intended to save lives – and we no longer received any complaints whatsoever from that customer.” 

The result is very convincing. We supply one of our biggest customers with critical automotive parts that are intended to save lives – and we no longer receive any complaints whatsoever from that customer.”

Per-Erik Edman, Quality Assurance Engineer at Zinkteknik

 

Fully automated end-of-line testing and sorting

Encouraged by this success, Zinkteknik then explored the possibility of integrating more test automation cells from Kistler into its production lines so as to achieve perfect results from other manufacturing projects. Zinkteknik now operates seven KVC-821 test systems to monitor production of five different parts - with two more systems to come in the near future: another one for the Swedish site, and the first one for Bosnia. Karl Persson, Production Engineer at Zinkteknik, explains the process: “We started out by using the first machine from Kistler as a standalone solution, so some steps had to be performed manually. But naturally, we wanted to integrate the test cells into our fully automated production lines. At a certain point, we realized that we could only achieve that goal by thinking big.”

Zinkteknik responded to this new challenge by expanding its Swedish production site in 2018 to accommodate full integration of the end-of-line testing solutions from Kistler, which are now installed in a new hall. “We currently have seven machines connected to our automated production lines, so we can easily balance varying volumes of different parts during the year. As a last step, we additionally integrated a fully automated forklift feed,” Persson adds. “We've been operating test automation systems in real production for about three years now, and we've received tremendous support from Kistler throughout that time. Their team was always standing by to answer our questions, they supported us with overcoming many challenges, and they even helped to generate new business opportunities for Zinkteknik.”

The success of zero-defect production has opened up new avenues of approach to the company's existing customers as well as opportunities to win new business. As Kenneth Magnusson, Sales Engineer at Zinkteknik, confirms: “When I visit customers, sales engineers from Kistler are ready to provide support as soon as we ask them. This adds weight to our presentations at meetings with potential customers. And that's yet another reason why we are so appreciative of our partnership with Kistler, and why we want to step up our collaboration with them as time goes on.”

2022. 9. 30.
Process automation in industrial production: Smart Single Stations for assembly and testing according to customers' specifications.
2022. 5. 4.
Daimler Buses relies on MaDaM and jBEAM to further develop of its electric city buses.
2022. 4. 11.
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
2022. 1. 14.
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
2021. 11. 18.
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
2021. 10. 12.
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
2021. 9. 14.
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
2021. 9. 9.
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
2021. 9. 3.
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
2021. 7. 2.
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
2021. 6. 22.
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
2021. 6. 2.
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
2021. 4. 26.
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
2021. 4. 13.
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
2021. 3. 22.
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
2021. 2. 8.
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
2020. 10. 5.
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
2020. 9. 18.
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
2020. 8. 20.
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
2020. 7. 22.
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
2020. 6. 9.
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
2019. 11. 15.
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
2019. 10. 23.
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
2019. 8. 15.
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
2019. 7. 17.
Turkey opts for weight enforcement with WIM technology from Kistler
2019. 6. 24.
For the next manned flight to the moon: safety that can be measured
2019. 6. 20.
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
2019. 5. 14.
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
2019. 4. 18.
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
2019. 4. 2.
NFL's Jaguars boost their fitness levels with Kistler.
2019. 3. 25.
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
2019. 3. 18.
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
2018. 12. 17.
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
2018. 11. 27.
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
2018. 10. 10.
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
2018. 10. 8.
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
2018. 8. 31.
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
2018. 8. 14.
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
2018. 7. 16.
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
2018. 4. 11.
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
2017. 11. 14.
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
2017. 8. 11.
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
2017. 1. 4.
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
2016. 12. 22.
Kistler makes progress in vehicle development possible
2016. 12. 22.
Kistler Sensor Correvit® SFII measures world record
2016. 12. 20.
Kistler sensors deliver a maximum in data quality under any conditions.
2016. 11. 7.
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
2016. 10. 5.
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
2016. 8. 17.
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2016. 2. 19.
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
2015. 11. 4.
Piezoelectric Measurements with CompactRIO™
2015. 6. 15.
Measurement Solutions for Automotive Test Systems
2015. 5. 8.
Quality Assurance in the Automotive Industry
2015. 3. 2.
How Brose improves the quality of its two-component production and automatically separates defective parts
2014. 12. 2.
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
2014. 12. 2.
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
2011. 8. 23.
HEWI and its Customers Benefit from Cavity Pressure Technology
2011. 2. 15.
End-to-end process monitoring for critical medical moldings
2011. 2. 7.
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
연락처
Max 25 MB