How Sartorius meets owing to the process monitoring system ComoNeo stringent quality requirements

Sartorius opts for Kistler's ComoNeo process monitoring and control system for high-precision quality monitoring of plastic parts for pipette systems at its facility in Helsinki. The ComoNeoPREDICT functionality delivers accurate forecasts of part quality while the injection molding process is still live – providing a sound basis for intelligent monitoring.

Products in the medical technology sector have to meet extremely high manufacturing requirements: processes must not only be very precise, but also repeatable and stable so that production results can be verified and undesirable influences can be excluded. Sartorius is a German corporation that can look back on a lengthy tradition of leadership in products for the laboratory and pharmaceutical segments. Founded in 1870, this exchange-listed enterprise operates across the globe from its headquarters in Göttingen. Sartorius supplies laboratories and research facilities with specialized equipment such as high-precision balances, filtration units and centrifuges. The company's Liquid Handling segment is located in the far north of Europe. Its mechanical and electronic pipette systems are developed and parts are manufactured in Helsinki. These products alone account for around six million individual parts every year, and Sartorius has another Finnish facility where it produces vast numbers of pipette tips – over 600 million units per year.

Accurate predictions of part quality while the process is still live 

Tomi Villilä is one of the 'plastics supremos' at Sartorius in Helsinki. As Development Manager Injection Molding, he shoulders responsibility for the quality of the injection molding processes for as many as 50 individual parts that make up one pipette. In response to ongoing developments, he and his strong team recently began using Kistler's ComoNeo process monitoring system with the ComoNeoPREDICT function. Online quality prediction allows forecasting of part quality during the injection molding process, based on numerous learned process parameters and related part-specific quality criteria. Villilä has garnered over ten years of experience in the plastics processing industry, and he is no stranger to the use of cavity pressure sensor technology: "I've known about Kistler for a very long time, and I'm well aware of the excellent performance their sensors deliver. In fact, I focused my degree thesis on cavity pressure sensors made by Kistler! And since then, I've often been involved with Kistler products throughout my career, so I'm very familiar with them."

Although ComoNeo only went into operation just recently, users at Sartorius are already convinced of the system's benefits:

We started out with a fairly non-critical part – a fixture – so we could get to understand the system, practice using it and improve our own process. But even after a short time, the results have been so good that we're planning to deploy six to eight additional ComoNeo units for other critical components as the next step."

Tomi Villilä, Development Manager Injection Molding at Sartorius

 

ComoNeoPREDICT is especially suitable for processes where the quality requirements are very demanding. The first step is to use the associated Stasa QC software to generate a testing plan – known as Design of Experiments, or DoE – that includes all the parameters needed to determine the process. Which dimensions are to be achieved? How must the machine be set to achieve them? Might it be possible to reduce the cycle time? Comprehensive and precise answers to many questions such as these are provided by the Stasa QC PC software and the ComoNeoPREDICT process monitoring feature. For convenience, the DoE can be generated on a PC and implemented digitally in ComoNeo at a later stage. The Kistler sensor technology installed in the mold supplies the basis for transparent process management of all material-related and part-specific attributes – the part's 'fingerprint', so to speak. Based on the measured cavity pressure and the specific part characteristics measured in relation to it, Kistler's system delivers a prediction of part quality while the injection molding process is still in progress. The benefit: intelligent optimization is possible with no need for time-consuming quality measurements. It took Sartorius only two or three days' work with ComoNeo to set up the specific DoE for modeling of the injection molding process for the fixture; then, following optimization with Stasa QC and ComoNeoPREDICT, very precise results were obtained. Because such large numbers of machine parameters are considered, users gain a clear understanding of the limits of the injection molding process and the relevant part characteristics – paving the way for intelligent process monitoring. It takes very little time to understand what is happening in the injection mold, and to gain knowledge about the entire process. Villilä notes enthusiastically: "Even colleagues without lengthy experience can achieve outstanding results in next to no time!"

Fast setup and intuitive operation

Based on the prediction model that is generated, ComoNeo can significantly reduce the percentage of bad parts, and they can be segregated automatically if desired. Here as in other respects, simple operation and integration are the keynotes: "This system is really simple to handle – almost like a smartphone. You only need five or ten minutes to understand how it works. And setting up a DoE poses no problems either, thanks to the software that comes with the product. You don't have to be a mathematician to understand the whole system – which is not the case with other programs. Once you've generated the DoE, you can simply upload it into ComoNeo and then you already get accurate feedback for process optimization in the test phase," Villilä explains.

He already has ambitious plans for the future: "I'm certain that the benefits we can achieve with ComoNeo will also be of interest to other Sartorius units – especially because this system is so flexible. I already gave a presentation to our colleagues about our experiences with ComoNeo at the company's gathering of experts in London. If it were up to me, all Sartorius technical parts that require high precision would be produced with the Kistler system in the future." With this idea in mind, a workshop will soon take place in Helsinki with a practical demonstration of ComoNeo, ComoNeoPREDICT and the online quality prediction feature for interested staff members from the entire Sartorius group.

2022. 4. 11.
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
2022. 1. 14.
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
2021. 11. 18.
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
2021. 10. 12.
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
2021. 9. 14.
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
2021. 9. 9.
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
2021. 9. 3.
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
2021. 7. 2.
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
2021. 6. 22.
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
2021. 6. 2.
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
2021. 4. 26.
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
2021. 4. 13.
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
2021. 3. 22.
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
2021. 2. 8.
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
2020. 10. 5.
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
2020. 9. 18.
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
2020. 8. 20.
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
2020. 7. 22.
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
2020. 6. 9.
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
2019. 11. 15.
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
2019. 10. 23.
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
2019. 8. 15.
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
2019. 7. 17.
Turkey opts for weight enforcement with WIM technology from Kistler
2019. 6. 24.
For the next manned flight to the moon: safety that can be measured
2019. 6. 20.
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
2019. 5. 14.
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
2019. 4. 18.
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
2019. 4. 2.
NFL's Jaguars boost their fitness levels with Kistler.
2019. 3. 25.
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
2019. 3. 18.
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
2018. 12. 17.
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
2018. 11. 27.
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
2018. 10. 10.
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
2018. 10. 8.
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
2018. 8. 31.
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
2018. 8. 14.
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
2018. 7. 16.
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
2018. 4. 11.
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
2017. 11. 14.
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
2017. 8. 11.
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
2017. 1. 4.
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
2016. 12. 22.
Kistler makes progress in vehicle development possible
2016. 12. 22.
Kistler Sensor Correvit® SFII measures world record
2016. 12. 20.
Kistler sensors deliver a maximum in data quality under any conditions.
2016. 11. 7.
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
2016. 10. 5.
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
2016. 8. 17.
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2016. 2. 19.
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
2015. 11. 4.
Piezoelectric Measurements with CompactRIO™
2015. 6. 15.
Measurement Solutions for Automotive Test Systems
2015. 5. 8.
Quality Assurance in the Automotive Industry
2015. 3. 2.
How Brose improves the quality of its two-component production and automatically separates defective parts
2014. 12. 2.
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
2014. 12. 2.
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
2011. 8. 23.
HEWI and its Customers Benefit from Cavity Pressure Technology
2011. 2. 15.
End-to-end process monitoring for critical medical moldings
2011. 2. 7.
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
연락처
Max 25 MB