Effective charging solutions for overloaded vehicles

Turkey's General Directorate of Highways of Turkey (KGM) recently decided to implement a weight enforcement system. During an initial testing phase, the WIM system from Kistler was installed at a trial site by the Mosaş Group, the system integrator. Backed by support from a team of Swiss specialists, Kistler's system delivers reliable measurement data.

The goal: increased road safety

Turkey's General Directorate of Highways (KGM) is keen to improve the condition of the country's roads. There were 7 300 fatalities on Turkish roads in 2016, according to the "Global status report on road safety 2018" by the World Health Organization (WHO). Although road deaths in Turkey have decreased steadily to 8.9 per 100 000 of the population in the last ten years, this figure is more than twice as high as in Central European countries. And in each year during the same period, KGM had to invest double the budgeted amount to maintain the nation's road network.

As well as controlling regular traffic, Turkey's local authorities are responsible for overseeing freight transport. They saw that a weight enforcement routine was necessary for two reasons: to reduce the accident rate, and to limit wear and tear on the infrastructure. To achieve these goals, about 100 weighing stations were installed all over the country. Every truck passing a station had to stop and wait until its weight was measured and approved.

There was no doubt that this process was necessary, but events soon made it clear that there was also potential for optimization. Traffic was slowed down dramatically because all trucks had to stop at the weighing stations. Long queues developed, causing even more potential hazards on the highways. And the weighing stations proved to have relatively short lifetimes due to the huge numbers of vehicles using them.

Preselection with WIM by Kistler

KGM now aims to improve this situation by implementing a preselection routine. It plans to install WIM sensors that measure the weight of vehicles as they drive over them, generating data for preselection: in future, trucks will only have to enter the weighing stations if they are above the weight limit. Fewer lorries will pass through the weighing stations, so traffic will flow more freely.

The Mosaş Group — an experienced partner

To prove the theory right, KGM invited various providers to take part in a test phase. Participants included the Mosaş Group, a Turkish company with over 100 employees and more than 20 years of experience and knowledge in the sector. The specialists at Mosaş provide highly reliable technology and engineering services with the focus on road and railway signaling systems, intelligent transportation systems, vehicle scales, weight measurement and size control systems, and the related software. Mosaş set out in search of a reliable solution from an experienced partner – and they achieved both objectives when they found Kistler and its Weigh In Motion (WIM) system. The project initiated a fruitful exchange between the two companies that soon led to close cooperation.

Accurate weight measurements

To evaluate the participating providers, KGM set up several test sites near existing weighing stations. The location assigned to the Mosaş Group is about 1.5 km from the Akıncılar toll plaza on one of the main highways leading into Ankara, the Turkish capital. The complete WIM system includes Kistler Lineas 9195G quartz sensors and the WIM 5204A data logger. These rugged system components deliver high-precision measurements throughout long service lifetimes.

Installation of the Lineas WIM sensors in the road pavement is fast and easy. Two sensors were installed in a staggered layout on each of the two lanes. After several runs with a calibration truck, a maximum deviation of ±2.3% was recorded – far below the required deviation of ±10% stated in KGM's specifications. Further tests with different vehicle classes are now in progress.

Support from Kistler throughout the project

Kistler specialists were on site to train the integrator on the WIM system. "Kistler's support during the installation phase was ideal," in the words of Ahmet Enec, at the Mosaş Group. "Field results from these products are good, and we are now going ahead to install the remaining sensors. At the same time, we are optimizing the system's performance."

"Field results from these products are good, and we are now going ahead to install the remaining sensors. At the same time, we are optimizing the system's performance."

Ahmet Enec, the Mosaş Group

 

The local authorities will be visiting the site to check the system's performance in the coming weeks. If KGM accepts this preselection method, a business plan will be drawn up to increase the budget. And if all the requirements are met, the Ministry will decide to install WIM at all weighing stations – a step that will help to protect Turkey's highway infrastructure and improve safety on the nation's roads.

2022. 4. 11.
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
2022. 1. 14.
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
2021. 11. 18.
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
2021. 10. 12.
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
2021. 9. 14.
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
2021. 9. 9.
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
2021. 9. 3.
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
2021. 7. 2.
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
2021. 6. 22.
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
2021. 6. 2.
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
2021. 4. 26.
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
2021. 4. 13.
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
2021. 3. 22.
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
2021. 2. 8.
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
2020. 10. 5.
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
2020. 9. 18.
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
2020. 8. 20.
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
2020. 7. 22.
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
2020. 6. 9.
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
2019. 11. 15.
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
2019. 10. 23.
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
2019. 8. 15.
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
2019. 7. 17.
Turkey opts for weight enforcement with WIM technology from Kistler
2019. 6. 24.
For the next manned flight to the moon: safety that can be measured
2019. 6. 20.
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
2019. 5. 14.
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
2019. 4. 18.
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
2019. 4. 2.
NFL's Jaguars boost their fitness levels with Kistler.
2019. 3. 25.
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
2019. 3. 18.
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
2018. 12. 17.
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
2018. 11. 27.
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
2018. 10. 10.
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
2018. 10. 8.
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
2018. 8. 31.
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
2018. 8. 14.
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
2018. 7. 16.
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
2018. 4. 11.
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
2017. 11. 14.
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
2017. 8. 11.
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
2017. 1. 4.
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
2016. 12. 22.
Kistler makes progress in vehicle development possible
2016. 12. 22.
Kistler Sensor Correvit® SFII measures world record
2016. 12. 20.
Kistler sensors deliver a maximum in data quality under any conditions.
2016. 11. 7.
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
2016. 10. 5.
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
2016. 8. 17.
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2016. 2. 19.
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
2015. 11. 4.
Piezoelectric Measurements with CompactRIO™
2015. 6. 15.
Measurement Solutions for Automotive Test Systems
2015. 5. 8.
Quality Assurance in the Automotive Industry
2015. 3. 2.
How Brose improves the quality of its two-component production and automatically separates defective parts
2014. 12. 2.
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
2014. 12. 2.
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
2011. 8. 23.
HEWI and its Customers Benefit from Cavity Pressure Technology
2011. 2. 15.
End-to-end process monitoring for critical medical moldings
2011. 2. 7.
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
연락처
Max 25 MB