Balda Medical Monitors Cavity Pressure

"Safety first" is an important requirement for the injection molding of medical parts, which strictly demands 100% quality. Even minute defects of the molded component can lead to functional deficits and unreliable operation. Hence, Balda Medical GmbH & Co. KG of Bad Oeynhausen/Germany, analyzes all quality-related injection molding parameters before production start-up and as an integral part of the mold qualification process. The specialist decided to introduce a cavity pressure-based system made by Kistler in order to enhance the process analysis-based quality monitoring of its production of lancet holders and housings for blood sugar monitoring systems. This way, the company can guarantee 100% quality, removes defective parts from the production and avoids assembly problems. This approach also speeds up injection molding production start-up processes after mold changes.

Pease download the complete Success Story (PDF) here. 

2022. 4. 11.
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
2022. 1. 14.
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
2021. 11. 18.
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
2021. 10. 12.
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
2021. 9. 14.
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
2021. 9. 9.
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
2021. 9. 3.
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
2021. 7. 2.
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
2021. 6. 22.
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
2021. 6. 2.
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
2021. 4. 26.
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
2021. 4. 13.
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
2021. 3. 22.
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
2021. 2. 8.
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
2020. 10. 5.
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
2020. 9. 18.
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
2020. 8. 20.
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
2020. 7. 22.
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
2020. 6. 9.
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
2019. 11. 15.
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
2019. 10. 23.
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
2019. 8. 15.
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
2019. 7. 17.
Turkey opts for weight enforcement with WIM technology from Kistler
2019. 6. 24.
For the next manned flight to the moon: safety that can be measured
2019. 6. 20.
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
2019. 5. 14.
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
2019. 4. 18.
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
2019. 4. 2.
NFL's Jaguars boost their fitness levels with Kistler.
2019. 3. 25.
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
2019. 3. 18.
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
2018. 12. 17.
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
2018. 11. 27.
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
2018. 10. 10.
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
2018. 10. 8.
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
2018. 8. 31.
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
2018. 8. 14.
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
2018. 7. 16.
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
2018. 4. 11.
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
2017. 11. 14.
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
2017. 8. 11.
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
2017. 1. 4.
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
2016. 12. 22.
Kistler makes progress in vehicle development possible
2016. 12. 22.
Kistler Sensor Correvit® SFII measures world record
2016. 12. 20.
Kistler sensors deliver a maximum in data quality under any conditions.
2016. 11. 7.
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
2016. 10. 5.
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
2016. 8. 17.
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2016. 2. 19.
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
2015. 11. 4.
Piezoelectric Measurements with CompactRIO™
2015. 6. 15.
Measurement Solutions for Automotive Test Systems
2015. 5. 8.
Quality Assurance in the Automotive Industry
2015. 3. 2.
How Brose improves the quality of its two-component production and automatically separates defective parts
2014. 12. 2.
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
2014. 12. 2.
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
2011. 8. 23.
HEWI and its Customers Benefit from Cavity Pressure Technology
2011. 2. 15.
End-to-end process monitoring for critical medical moldings
2011. 2. 7.
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
연락처
Max 25 MB