A torque sensor guarantees the functionality of mixing nozzles at Jonas & Redmann

Special-purpose machinery manufacturer Jonas & Redmann puts its trust in integrated process monitoring by Kistler to guarantee the functionality of mixing nozzles for dental applications. A friction coefficient test – performed with the help of a torque sensor from Kistler – ensures automatic segregation of good and bad parts. The necessary measurement technology is also integrated into the solution, so the signal is transmitted directly to the machine control. 

A young company that has already built up a tradition: mechanical engineering specialist Jonas & Redmann was founded in Berlin almost 30 years ago. Since then, the firm has built up an outstanding reputation with its high-caliber machines and systems for assembly and process automation; over 400 employees now work at JR's five sites spread across three continents. The Berlin-based engineers offer an extensive portfolio of innovative automation solutions, ranging from integrated standalone cells through to highly automated production lines. As well as factory automation in general, Jonas & Redmann has a special focus on sunrise industries such as medical engineering, photovoltaics and energy storage.

Frank Polak has been a key player in the company's success story for the last 22 years: he started out as a design engineer, and has since become JR's Head of Medical Engineering. He now leads a team of six design engineers who also benefit from the support of colleagues in other departments. "Most of our customers are large corporations with global reach, and several of them are DAX-listed. Standards in the medical technology sector are always high, but our customer base means that we have to meet even more demanding requirements – after all, the patients' wellbeing and safety are at stake," Polak points out. This is why every plant built by Jonas & Redmann must be appropriately qualified and validated – and that also applies to all sub-assemblies and add-on components.

Automated quality testing – including traceability

Many of the projects in the medical technology segment revolve around "disposables" – single-use medical products that must be disposed of after use, so they need to be produced in large quantities. High quality is an absolute necessity here, as Frank Polak confirms by offering some insights into a current project: "On behalf of a dental laboratory, we collaborated with a firm of consulting engineers to develop a highly automated production cell for mixing nozzles. To ensure quality in the live process, we use a Kistler torque sensor that communicates directly with the machine control." The dental laboratory uses the mixing nozzle to produce casting compounds for dental products such as those needed by dentists to prepare dental impressions.

To guarantee the functionality of the sub-assembly, a friction coefficient test (< 0.5 Nm) is carried out on the mixing mechanism of the assembled nozzle.

This product is a plastic sub-assembly consisting of four parts that are joined in the machine and then tested. Thanks to Kistler's solution, we can guarantee the quality of about five million units per year – and at the same time, we can ensure traceability,"

Frank Polak, Head of Medical Engineering at Jonas & Redmann

 

"Traceability is an essential requirement in today's medical sector – and responsibility for it is increasingly passed on to the special-purpose machinery manufacturer," Polak continues.

End-to-end inline process monitoring

The combination of Kistler's 4502A torque sensor and the maXYmos BL evaluation system ensures end-to-end inline process monitoring: the torque curve for each individual product can be tracked accurately on the monitor of the maXYmos system. 

But no highly-automated plant from Jonas & Redmann would be complete without a pre-integrated mechanism for segregating bad parts: the measurement value produced by the torque sensor is used to generate an OK/NOK signal that is then transmitted directly to the control  - so any parts joined with insufficient torque can be segregated immediately. Polak notes: "With a production rate of 40 parts per minute – equivalent to a cycle time of one and a half seconds – this poses an enormous challenge. And that's why we're so highly satisfied with Kistler's solution – because it does exactly what we need for the application! Before we use any third-party components, we carefully check whether we could meet the requirement by designing the solution ourselves. But in this case, Kistler's system was quite simply the better alternative for integrated process monitoring."

Tried-and-tested technology – fast integration

Polak's attention was drawn to Kistler by his colleague Andreas Nowak, Head of Mechanical Engineering and Operational Technology at Jonas & Redmann, who is thoroughly familiar with the components and systems available on the market. Nowak has opted for solutions from Kistler in the past, and he is highly satisfied with them: "In our joining processes, we already make use of Kistler's electromechanical joining systems: they ensure effective automation because they feature high efficiency and precise control. But there could also be further applications for medical engineering in the future, especially as regards process monitoring."

The prototype of the new plant to produce the mixing nozzles, with integrated Kistler components, was showcased on Jonas & Redmann's stand at the 2018 Automatica trade fair. One important factor in the successful outcome was Kistler's collaboration with the consulting engineers who were executing the project: together, the two teams quickly devised a test rig to verify the solution's feasibility. At the very first attempt, the test confirmed that the transducer shaft is suitable for this application case. The assumed theoretical values for frictional torque were almost entirely identical to the actual torques measured on the test rig. Jörg Nimz, a Sales Engineer at Kistler, is naturally delighted with the results: "The transducer shaft used here has already proven its excellence on the market many times over – especially in applications such as this one for measuring frictional coefficients. So we're pleased that Jonas & Redmann placed their trust in us, and now we're eager to hear about the end user's experience."

2022. 4. 11.
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
2022. 1. 14.
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
2021. 11. 18.
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
2021. 10. 12.
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
2021. 9. 14.
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
2021. 9. 9.
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
2021. 9. 3.
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
2021. 7. 2.
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
2021. 6. 22.
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
2021. 6. 2.
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
2021. 4. 26.
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
2021. 4. 13.
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
2021. 3. 22.
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
2021. 2. 8.
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
2020. 10. 5.
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
2020. 9. 18.
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
2020. 8. 20.
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
2020. 7. 22.
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
2020. 6. 9.
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
2019. 11. 15.
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
2019. 10. 23.
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
2019. 8. 15.
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
2019. 7. 17.
Turkey opts for weight enforcement with WIM technology from Kistler
2019. 6. 24.
For the next manned flight to the moon: safety that can be measured
2019. 6. 20.
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
2019. 5. 14.
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
2019. 4. 18.
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
2019. 4. 2.
NFL's Jaguars boost their fitness levels with Kistler.
2019. 3. 25.
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
2019. 3. 18.
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
2018. 12. 17.
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
2018. 11. 27.
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
2018. 10. 10.
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
2018. 10. 8.
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
2018. 8. 31.
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
2018. 8. 14.
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
2018. 7. 16.
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
2018. 4. 11.
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
2017. 11. 14.
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
2017. 8. 11.
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
2017. 1. 4.
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
2016. 12. 22.
Kistler makes progress in vehicle development possible
2016. 12. 22.
Kistler Sensor Correvit® SFII measures world record
2016. 12. 20.
Kistler sensors deliver a maximum in data quality under any conditions.
2016. 11. 7.
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
2016. 10. 5.
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
2016. 8. 17.
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2016. 2. 19.
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
2015. 11. 4.
Piezoelectric Measurements with CompactRIO™
2015. 6. 15.
Measurement Solutions for Automotive Test Systems
2015. 5. 8.
Quality Assurance in the Automotive Industry
2015. 3. 2.
How Brose improves the quality of its two-component production and automatically separates defective parts
2014. 12. 2.
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
2014. 12. 2.
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
2011. 8. 23.
HEWI and its Customers Benefit from Cavity Pressure Technology
2011. 2. 15.
End-to-end process monitoring for critical medical moldings
2011. 2. 7.
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
연락처
Max 25 MB