Using digital X-rays for quality control in measuring wheels

Winterthur, October 2020 – As well as calibration, the Kistler Group now also offers RoaDyn Structural Integrity Inspection by certified experts in accordance with ISO 9712. This digital X-ray inspection reveals even the tiniest volume defects in the measuring wheel. These are caused by the high stresses involved in vehicle testing and can potentially falsify the measurement result. Combined with fluorescent dye penetrant inspection, which visualizes micro-fissures in the surface, this reliable inspection method enables manufacturers in the automotive industry to achieve flawless measurement quality and saves them from having to invest in their own quality assurance processes.

Measuring wheels are the preferred means of carrying out measurements during driving dynamics campaigns or operational loads, for example when designing new components. The loads that measuring wheels are exposed to during these tests are sometimes equivalent to several vehicle lives – consequently, they are among the most heavily stressed metrological components. To ensure that they continue to function reliably and safely, it is essential to check the measuring wheels at an early stage and at regular intervals.

Component testing from a single source

Measuring wheels are regularly calibrated to detect deviations in sensor behavior at an early stage. In parallel with the necessary calibration, Kistler offers non-destructive component testing using two methods: digital X-ray and fluorescent dye penetrant testing. In the case of X-ray testing, components are exposed to short-wave electromagnetic radiation, in which gamma radiation excites the electrons in the detector’s crystal array. Scintillation converts the X-ray photons directly into electricity. The resulting data is then digitally recorded. Depending on the degree of blackening, the X-ray image reveals the different thickness or density of the material and consequently also shows any fissures or pores that may be present.

The second test method, a fluorescent dye penetrant test according to DIN EN ISO 3452-1, is more complex. In this process, a liquid is applied to the surface of the component, which penetrates into the surface defects of the material. A subsequent developer layer creates a counter-capillarity, drawing out the liquid that has penetrated into the cracks and making even micro-fissures visible with the aid of UV-A illumination. This intensive control of the measuring wheels after calibration not only ensures the safety of the components, but also helps employees involved in vehicle testing to avoid potential accidents.

Expertise saves time and money

Bringing calibration and quality control under one roof saves manufacturers time and money. The short throughput time of Kistler’s digital X-ray inspection is a particular advantage in series production testing. Rather than having to do without their measuring wheel for several weeks, as is usually the case, manufacturers who have their measurements carried out by Kistler get their measuring wheel back within just a few working days. In special cases, as little as a few hours. Our certified experts at Kistler are responsible for non-destructive materials testing and can reliably confirm the functionality of the tested measuring wheels, provided that the tests do not produce any findings.

“By combining calibration and RoaDyn Structural Integrity Inspection, we achieve a high quality of measuring wheel verification without our customers having to invest in their own control procedures at the factory – we take care of measuring wheel validation from start to finish and guarantee our customers the best possible results”, explained Ibrahim Naji, who supervises digital X-ray and fluorescent dye penetrant inspection at Kistler.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.