The NCFE Joining Module from Kistler

Winterthur, 10 October 2016 – Kistler is unveiling a new addition to its portfolio of electromechanical joining modules. The NCFE joining module is specifically designed for simple joining processes – so plant manufacturers and power pack operators now have a cost-effective alternative to conventional pneumatic or hydraulic systems.

Kistler is launching its new NCFE joining module, developed especially for plant manufacturers who nowadays build their own joining units and also for operators of conventional power packs. This innovation unlocks entirely new possibilities for all those customers who previously found it unprofitable to use Kistler's electromechanical joining systems. The new joining module is specifi-cally intended for simple joining processes that feature low requirements as regards cycle times, design and measuring ranges. As compared to hydraulic or pneumatic units, the NCFE module (the 'E' stands for Economy) offers convincing advantages such as low energy consumption, simple handling and fast commissioning. The new NCFE joining module is designed for applications in the 10 – 80 kN measuring range.

A New Era Dawns for Plant Manufacturers and Power Pack Operators

Every day, customers all over the world benefit from Kistler's enormous stock of know-how in the field of electromechanical joining systems. Kistler set out to identify additional markets where its flexible, energy-saving joining units could be used. The Swiss sensor manufacturer singled out two particularly important target groups: operators of conventional pneumatically driven power packs, and plant manufacturers.

Alexander Müller, Product Manager for NC Joining Systems, explains that Kistler's existing portfolio of joining systems does not fully cover the highly specific requirements of these users. This prompted Kistler's product management team to develop a new joining module for this target group.

Alexander Müller adds that the new module opens up entirely new prospects for all plant manufac-turers who previously developed their own joining systems. The NCFE module offers them a cost-effective alternative to developing their own systems. All the systems are pre-tested, so fast com-missioning is guaranteed. Thanks to the advantage of integrated sensor technology, this module provides plant manufacturers and power pack operators with complete, end-to-end monitoring and control of the entire joining process. Installation as well as handling are made far simpler, so plant manufacturers can present convincing arguments to their customers on points such as energy savings, short delivery times and flexibility.

Comprehensive Control Thanks to the maXYmos NC Monitoring System

The joining process is monitored by the maXYmos NC monitoring system, which evaluates and documents XY curves for joining and press-fit processes in conjunction with the NC joining mod-ules and the IndraDrive servo amplifier that is included in the system. The patterns of measure-ment curves can be used to monitor the quality of a single production step, a sub-assembly or an entire product, with control in real time via SERCOS III. The benefits: optimal cycle times can be achieved with maximum repeat accuracy, downtime is minimized and machine availability is in-creased – adding up to a boost in productivity for the entire manufacturing process.

Thanks to integrated sequence control (sequencer mode), processes can be mapped with no need to rely on costly external PLC programming. The programs can be set up quickly and easily with the help of the intuitive user interface on the touch display. A total of up to 128 programs can be saved and for each program, an independent sequence with as many as 255 objects can be defined. Processes are evaluated with the help of profiles for two interrelated measurands that are assessed as good (OK) or bad (NOK). Ten Evaluation Objects (EOs) are available for each program, so process deviations can be detected and complex process sequences can be regulated and controlled.

The Right Joining System for Every Application

Alexander Müller sums up the benefits for new users in a nutshell:

"As compared to pneumatic or hydraulic processes, the NCFE module offers substantially higher efficiency – like all Kistler's joining systems. Savings potential with the electrical process is up to 77% as compared to the hydraulic process, and about 90% in relation to the pneumatic process. Maintenance outlay for these systems is minimal – so users can save even more on their already low production costs. What's more, scrap is reduced because 100% quality control is achieved with this module."

As the product manager responsible for joining systems, Müller is especially proud that Kistler can now offer its highly advanced NC joining technology to a broader market thanks to this cost-effective new development:

"With this new bandwidth of products – from compact high-end joining modules (NCFH) through to simple joining units (NCFE) – Kistler now offers the right system to meet every requirement. Another plus: seamless integration into an overarching production envi-ronment is possible thanks to the flexible interfaces that are included in maXYmos NC as standard. This means that we have passed another milestone in our success story as a global provider of joining systems: with the NCFE module, we can now offer our customers even more specific support as they endeavor to cut costs, save time and strengthen their competitive edge on the market!"

Download Press Release (PDF)
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.