Simply carry-on tightening – with the INSPECTOR torque wrench!

Winterthur, October 2020 – Kistler is expanding its range of inspection systems for fastening technology by introducing the new INSPECTOR torque wrench. Thanks to this easy-to-handle device with its display/measuring unit, users can carry out process capability tests on bolted joints for evaluation and documentation of fastening process under series production conditions in a matter of seconds. The INSPECTOR meets a requirement that is especially important in the automotive and vehicle manufacturing industry: quality assurance compliant with the VDI/VDE guideline after the fastening process is completed. The new torque wrench also offers an advantage that was never available on the market until now: an interface with the CEUS and testXpert software applications for evaluation and archiving.

Bolted joints, which come in a wide variety of designs, play an essential part in industrial production as a safe and verifiable method of connecting components. In the automotive industry, for instance, bolted joints are used for all important connections on wheels, axles, airbags, safety belts and brakes, to name only a few examples – and most of these joints are relevant to safety, so they require special attention as regards documentation.

This sets high reliability requirements for the inspection systems that are used in research, production and – above all – quality assurance. Further tightening has become firmly established as a testing method in recent years. Shorter cycle times are making it increasingly difficult to perform tests directly after assembly. But with the further (or carry-on) tightening test method, a torque wrench is used to continue tightening the joint by a defined further rotation angle after it has already been fastened, and the resultant torque is then measured. Thanks to recording and statistical evaluation of the fastening curve, suitable methods can be used to determine whether the bolted joint was produced in a controlled and capable process.

Handheld electronic tool

"The new INSPECTOR electronic torque wrench from Kistler provides users with a high-performance tool for process capability tests," according to Wilfried Blechmann, Head of the Fastening Technology Business Field at Kistler. "This is a compact, easy-to-operate tool that combines precise measurement technology with a very comfortable high-quality user interface. It will help users to assemble bolted joints reliably and provide proof of process capability in compliance with VDI/VDE 2645 Part 3," Blechmann continues. Another benefit: the digital measurement signals acquired from the INSPECTOR during testing can be evaluated and archived with the CEUS and testXpert software applications.

Connectivity allows evaluation and archiving

For this purpose, the database-supported CEUS software from Kistler handles all the tasks required for documented inspections of the fastening process: parameterization via CEUS allows operators to define tests according to customer-specific, standardized or guideline-based requirements, with free configuration of the fastening points. For more extensive documentation and evaluations, the measurement data can be transferred to the CEUS software with its varied range of options for statistical evaluation. CEUS also makes it easier to plan the testing schedule, and users benefit from software support as they process their workload with the help of stored testing tasks (known as "routes") that are transferred to the INSPECTOR. Inspection reports and data export provide plenty of flexibility, too: an editor allows users to integrate results, tables and graphics as well as freely definable parameters into an inspection report according to their individual requirements. All data obtained can also be forwarded automatically to higher-level software platforms via an export interface. And in addition, the testXpert software used by Kistler makes it possible to transfer the measurement data from the new torque wrench to the evaluation software so that advanced evaluations can be performed. 

"Kistler's portfolio of inspection systems for bolted joints is already extensive, and now the addition of the INSPECTOR gives customers an even wider choice of fastening technology solutions," Blechmann notes. "A varied range of inspection systems, the unique interface offered by the new torque wrench for connection to CEUS and testXpert software, and specific services: factors that add up to a comprehensive offering, precisely in line with customers' requirements for quality assurance in fastening technology. Users can take advantage of benefits that will help them to meet the growing requirements for process capability, traceability, product liability and efficiency."
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.