New cooperation between Vehico and Kistler Group

Winterthur, May 2020 - The Kistler Group, known for its market leadership in dynamic pressure, force, torque and acceleration measurement technology, has entered into a cooperation with Vehico, located in Braunschweig (Germany), a manufacturer of driving robots and vehicle control systems for vehicle testing. As a result, an extensive package of sensor technologies and driving robots will now be available from a single source.

The number of vehicle tests continues to rise, partly due to changing legal regulations and consumer test requirements. With the progress made with Advanced Drivers Assistance Systems (ADAS), the number of system verification tests is growing exponentially. It is therefore vital for manufacturers to carry out all testing as efficiently and economically as possible. 

To guarantee smooth driving dynamics and the functionality of ADAS systems, vehicles are tested and evaluated using driving robots in combination with sensors from Kistler. Kistler’s sensors measure different forces affecting the vehicle and the driver, for example on brakes, the steering wheel and on the wheels themselves. Vehico’s driving robots provide objective vehicle testing, precise and reproducible tests up to driverless testing by automatic steering, gas, and brake robots. In addition, Vehico platforms can simulate other road users, from walking pedestrians to fast-moving vehicles.

Making the testing processes easier is at the heart of the new cooperation. Rather than choosing sensors and robots individually, customers can now obtain an extensive portfolio from a single source. All individual components can be perfectly matched, reducing time and effort at the point of installation and improving reliability and reproducibility.

Evaluating vehicle dynamics and active safety

The driving robots are used for development of vehicle control and ADAS systems, and for the evaluation of production vehicles. The sensors provide data that allows rating the quality and reliability of the installed dynamic control and ADAS technologies. Kistler also offers solutions to evaluate the huge volume of data that is being generated. The measurement data management system MaDaM and the post-processing software jBEAM together help to gather, analyze and visualize virtually any set of data.

“Kistler’s and Vehico’s expertise in the field of vehicle dynamics and ADAS complement each other. All customers will be able to benefit directly for classic vehicle testing, the development of new types of assistance systems and autonomous vehicles,” says Dr. Lothar Ganzelmeier, Managing Director of Vehico.

“By combining our long-standing expertise in dynamic vehicle testing and vehicle safety with Vehico’s innovative technologies in driving robots, we are now able to extend our portfolio and services for vehicle development and testing. Now we can measure, evaluate and improve the quality of dynamic control and ADAS systems from start to finish. We help to accelerate and simplify testing processes for our customers”, says Alexander Putz, Project leader ADAS testing systems at Kistler.

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

2022. 7. 28.
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.