maXYmos from Kistler: making quality assurance easier for medical device manufacturers

Winterthur, May 2020 - maXYmos TL ML from Kistler is the first process monitoring system that meets the strict regulatory requirements for quality assurance in the medtech sector. A monitoring system that can deliver 100 percent testing: this is a critical requirement for producers of medical devices as well as plant and machinery manufacturers operating in environments where pharmaceutical goods and medtech equipment are produced. Kistler now meets this need with the latest version of its tried-and-tested maXYmos system. maXYmos TL ML can easily be qualified and validated for integration into existing quality management systems.

Process monitoring systems play an increasingly important part in quality assurance on automated production lines for medtech devices. Medical device manufacturers not only have to prove that they have a quality management system in place: they must also demonstrate that the medical devices they produce meet the requirements for safety and quality. Their further obligations include providing proof of quality assurance for all their machines, tools and the entire manufacturing process. And as yet another requirement, medical device manufacturers have to verify their suppliers' quality management systems.

Excluding liability – a critical objective for medical device manufacturers

In extreme cases, inadequate quality assurance during the production of medical devices can put people in harm's way or even lead to loss of life. Companies that place medical devices on the market are fully liable in the event that their products fail to function perfectly. This is partly why the industry is subject to such strict regulation. Producers of medical devices as well as plant and machinery manufacturers operating in the medtech and pharmaceutical sectors are confronted with huge challenges – especially when it comes to integrating process monitoring systems into automated production and packing processes.

To help customers overcome the obstacles they face, Kistler has joined forces with partners in the mechanical engineering and plant construction industry to develop the maXYmos TL ML process monitoring system, in strict compliance with the guidelines of the FDA (U.S. Food and Drug Administration) and its Medical Device Reporting (MDR) regulations.

A process monitoring system with FDA- and MDR-compliant functionalities 

Kistler has developed this new solution on the basis of its maXYmos TL (Top Level) system. Like all the systems in the maXYmos family, maXYmos TL visualizes process profiles and offers an extensive range of interfaces for connecting sensors. The system is integrated directly into the production line to monitor and evaluate the quality of any given manufacturing step – and therefore of the whole product – on the basis of a curve. With the help of evaluation objects (EOs), users can adapt the curve evaluation to the specific monitoring task. For instance, the tolerances defined in the process validation can be used for this purpose. Based on this specification, the system then decides whether each workpiece is good or bad.

The functions integrated in maXYmos TL ML comply with the regulatory requirements for applications in the medtech industry. The system hardware also meets the specific requirements for measurement equipment that apply in the medtech industry, including:

  • Design to accommodate exceptionally small measuring ranges (force-displacement monitoring, torque sensor technology)
  • Integrated user management compliant with FDA regulatory requirements
  • Audit trail: recording and monitoring of all changes to testing processes, with time and user indexing for end-to-end traceability of each individual product
  • Optional blocking of ports for secure integration into the customer's data structure
  • Direct printer connection so that test records can also be documented as hard copies

Optimized production processes give medical device manufacturers a competitive edge

Thanks to the new maXYmos TL ML process monitoring system from Kistler, producers of medical devices as well as machinery and plant manufacturers operating in the medtech and pharmaceutical sectors will now find it much easier to validate their production processes. In the best-case scenario, 100 percent inspection of a manufacturing step can completely eliminate the need for mandatory process validation in production. Qualification of the production equipment is the first requirement for proof of the system's safety. For this purpose, Kistler supplies ready-to-use checklists for Installation Qualification (IQ) and Operational Qualification (OQ). An in-plant calibration can then be performed to validate the measurement system at any time – a service that Kistler offers for its customers throughout the world. This also makes requalification of assembly plants much simpler, because the entire measuring chain is calibrated. The key benefit: manufacturers can bring their product developments and innovations to market much more quickly – giving them the competitive edge that is such a critical factor in this industry.

Into the future with intelligent networking and control

maXYmos TL ML supports OPC UA, so it can easily be connected to machine controls and can communicate with higher-level control and management systems.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.