Making roads and bridges safer

Winterthur, 21 March 2019 - Dilapidated roads and bridges cost taxpayers billions every year, and they cause traffic jams stretching for kilometers. In the worst-case scenario, continuous stress gives rise to real risks. Bridges in particular are severely impacted by increasing traffic volumes. Heavy vehicles are the main cause of damage, because vehicle weight is one of the critical parameters that determine an infrastructure's lifetime. Cutting-edge technology now makes it possible to monitor traffic loads on roads and bridges more accurately than ever before. Weigh In Motion systems can weigh vehicles while they are actually traveling: this means they can supply precise information about loads on heavily used routes, so overweight vehicles can be directly excluded from traffic. 

The number of heavy semitrailers on Swiss roads has almost quadrupled since 1980: growth in this vehicle category alone is placing undue demands on the infrastructure. Experts identify heavy truck traffic as the decisive factor that causes wear on roads and bridges. The "fourth power law" explains why this is so. According to this law, the increase in the force acting on the road is not linear, but exponential  - an increase to the fourth power, in fact. Load per axle is the critical parameter here. A comparison between a truck with a weight of ten tonnes per axle and a passenger car with an axle load of one tonne makes this clear. According to the fourth power law, the impact of the truck's axle on the asphalt and bridge materials is not ten times greater than the impact caused by the car  - but no less than ten thousand times (10x10x10x10) greater! In other words, one 30-tonne truck causes just as much damage to the road as 7 500 cars.

Numerical recording of traffic is one method that helps operators keep track of infrastructure damage inflicted on bridges and roads by growing traffic volumes. Roadside count stations or detection loops embedded in the asphalt can transmit the numbers of trucks that drive past (or over) the equipment. However, these methods cannot answer the most critical question: how much do the trucks actually weigh? According to the fourth power law, unladen trucks have a much lower impact on road surfaces and bridge statics than fully loaded vehicles. Weigh In Motion systems  - such as those offered by Kistler  - provide the ideal solution for collecting data that is genuinely meaningful. As well as recording the numbers of vehicles, systems from this Swiss company capture reliable data about axle and axle-group loads  - as the vehicles travel past, with no need for drivers to interrupt their journeys, and with no other adverse effects on traffic whatsoever. The statistics acquired from this comprehensive data collection process can then be used to predict and schedule the actions needed to refurbish roads and bridges.

Switzerland's Federal Roads Office (FEDRO) already operates a number of Weigh In Motion measuring points with special Kistler force sensors that weigh vehicles while they are traveling. The results are alarming: up to 4.5% of trucks passing these measuring points exceed the permitted 40-tonne limit. That adds up to 75 000 overweight vehicles every year! In other countries, too, Kistler's system is already in widespread use as a practical measure to prevent overloading. On the El Carrizo highway bridge in Mexico, for example, trucks are weighed before they drive onto the bridge; if they exceed the defined weight limits, they are prohibited from crossing. Hungary and the Czech Republic make similar use of this technology for speed monitoring, to ensure that those responsible for overloaded trucks have to pay the price. Measures such as these deliver dual benefits: they protect the infrastructure, and they also improve safety on the roads. Other European countries are likely to waste no time in learning from these examples, so Weigh In Motion systems will contribute even more directly to the safety of bridges and roads in the near future.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.