Leading-edge biofidelic dummy now available worldwide

Winterthur/Münster, December 2020 – CTS and Kistler decide to collaborate on realistic substitutes for the human body: thanks to the combination of a biofidelic dummy and high-precision measurement technology, customers now benefit from greater scope for crash tests, product development, operational training and modeling or reconstruction of dynamic processes. The solution from CTS is now available through the Kistler Group's global sales network, and it can be equipped with individual in-dummy measurement technology from Kistler and additional sensor instrumentation. 

As well as significantly enhancing vehicle safety, ongoing advances in the development of crash test dummies are opening up new application areas. The PRIMUS biofidelic dummy from CTS offers an ideal solution for these purposes because it has bones, ligaments and joints that are largely modeled on those of humans; weight distribution, skin and skeletal structure are also very close approximations of the biological original.

To take one example: PRIMUS can be used for highly accurate reconstructions of accidents ‒ not only in the automotive sector but also in other application areas such as the aviation industry, safety engineering, product tests, and recovery exercises for rescue services. In the military sector, PRIMUS is suitable for use in applications such as tests of bulletproof vests. During operation, PRIMUS behaves like an unconscious human being; it can used in both standing and sitting positions with no need for further modifications. On request, PRIMUS can also be equipped with in-dummy measurement technology from Kistler, the Swiss market leader: combined evaluation of precise measurements and real damage supplies highly accurate and dependable test results for purposes such as expert reports and insurance cases, or to obtain certifications.

Thanks to the collaboration between CTS and Kistler, customers across the globe now gain access to a holistic high-end system for crash tests – and that's not all. This solution is highly versatile, and it meets the most demanding requirements.”

Jens Wolking, Business Driver Vehicle Safety at Kistler

 

 

Integrated data acquisition ‒ made to measure

Digital sensor technology from Kistler is fully integrated into PRIMUS to allow autonomous data acquisition without influencing the dummy. Implementation is efficient, with just one cable for the data logger that is installed in the chest area.

PRIMUS was developed by CTS in cooperation with the Dresden University of Applied Sciences. The developers focused particular attention on the structural design and the materials used in order to reproduce the effects of shock and pressure loads on the human body as realistically as possible. CTS operates its own in-house production facility at Münster in the Westphalia region of Germany, so each dummy can be individually equipped and flexibly adapted to customers' requirements: for example, individually designed measurement technology can be supplied, sections of tissue and bone can be specially adapted, and other functions can also be customized.

Customized design to suit the purpose of use

Dr. Mirko Dobberstein, Managing Director of CTS, sums up: "Our collaboration with Kistler gives us the opportunity to market our biofidelic dummy throughout the world ‒ and it also opens the way for us to develop new applications. Flexibility in the production of the dummies and also in equipping them with high-end measurement technology means that we can offer custom solutions to meet the very highest standards ‒ adding up to an enormous step forward in the field of crash testing and even beyond!"
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.