Latvia grants homologation for OIML-certified KiTraffic Basic from Kistler

Winterthur, May 2021 – The KiTraffic Basic Weigh In Motion (WIM) system from Kistler gained a best-in-class OIML certificate in 2020. This opens up access to new markets for WIM: thanks to its compliance with OIML standards, KiTraffic Basic is now successfully homologated in Latvia, so the solution from Kistler is ready for use in direct enforcement applications there. KiTraffic Basic has also obtained a local type approval in the Czech Republic.

Keeping control of increasing traffic volumes is no easy task: overloaded trucks are more likely to damage road infrastructure, and they also present a greater risk of accidents. Bridges of all ages also need protection against excessively heavy traffic and stress caused by passing vehicles. To address these challenges, growing numbers of operators, road owners and authorities are seeking reliable automated monitoring solutions, especially for truck traffic. Kistler has over 20 years of experience with Weigh In Motion, and its WIM systems are installed in more than 50 countries worldwide. As a leading provider of automatic traffic solutions, the Kistler Group works continuously to optimize its WIM technology.

Now ready for direct enforcement in Latvia: blazing the trail for other countries 

The KiTraffic Basic WIM system (Type 9835A) was awarded another certificate by the International Organization of Metrology (OIML) in 2020. On this occasion, the OIML officially confirmed that the system from Kistler can accurately and reliably measure the gross vehicle weight and axle loads of trucks moving at speeds up to 120 km/h – and even 140 km/h for vans. Tomas Pospisek, Regional Manager Eastern Europe Traffic Solutions at Kistler, explains why this is so important: “Even in the EU, every country has its own rules and regulations for the operation of Weigh In Motion systems. That’s why every homologation process is different and always complex. But the international OIML standard is a common starting point, making it easier for us as well as system integrators to get the approvals needed to install WIM systems.”

This was exactly the approach taken in both Latvia and the Czech Republic and – with the help of the recently acquired OIML certificate – homologation for KiTraffic Basic was completed comparably quickly in both countries. “Now, system integrators in other countries can include our certified system in their WIM solutions; then they can apply for official approval from authorities and go on to compete for tenders,” Pospisek points out: 

Now, system integrators in other countries can include our certified system in their WIM solutions; then they can apply for official approval from authorities and go on to compete for tenders.”

Tomas Pospisek, Regional Manager Eastern Europe Traffic Solutions at Kistler

 

The certification in Latvia opens up a new market for WIM technology from Kistler: KiTraffic Basic is now fully available for monitoring, pre-selection and direct enforcement of overloaded vehicles.

WIM with certified performance – ready to conquer the globe

At the heart of the KiTraffic Basic system are tried-and-tested Lineas piezoelectric quartz sensors from Kistler. As well as accurately measuring vehicle weight at high speeds, this WIM solution delivers a whole series of attractive advantages: it can seamlessly handle high axle loads (of up to 30 tonnes each), and there is no overall limitation on the maximum measurable weight. With a temperature range from –40 to +80°C, reliable operation is guaranteed in almost any climate.

As Pospisek concludes: “We’re proud to have reached this milestone for operational readiness and even direct enforcement in Latvia. This opens up new business opportunities – in the other Baltic countries, for instance. I’m convinced that the OIML certification of proven accuracy at high speeds will help us gain ground in other markets too.”

Learn more about Weigh In Motion systems from Kistler at www.kistler.com/wim
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.