Kistler's custom sensors can cope with every measurement challenge – no matter how extreme

Winterthur, February 2019 - With a measuring range of up to 450kN in the Z axis and 100kN in the X and Y axes, Kistler's Type 9397C 3-component force sensor offers unique measuring capacity. This, the largest sensor of its type in the world, is the ideal choice for large-scale measurement tasks such as capturing impact forces in crash tests. The Swiss pioneer of piezoelectric measurement technology specializes in ready-to-use custom solutions that can also cope with extremely high measurement ranges.

"The 3-component force sensor is at the heart of every application that involves measuring very high dynamic forces with the utmost precision," according to Martin Betschart, Product Manager at Kistler. He continues: "Our customer-focused, application-oriented approach is backed by over 60 years of experience in piezoelectric measurement technology. That combination gives us a very precise knowledge of the requirements in different sectors and industries. The new Type 9397C 3-component force sensor shows that there are literally no limits to the scale of the measurement tasks that we can accomplish."

Piezoelectric 3-component force sensors are used in industry to measure dynamic and quasistatic tensile and compression forces. Because these sensors are very rigid, their natural frequencies are high: this enables them to measure the smallest dynamic changes to very large forces in all three directions with high precision and excellent reliability. The sensors are already calibrated and pre-loaded on delivery, so they can be used as soon as they have been installed correctly. 

Reliably measuring huge impact forces

One typical application area is measuring the impact of an aircraft's landing gear on the runway. The Landing Gear Drop Test simulates the forces that act on the landing gear as the aircraft touches down. To perform the test, the entire landing gear is raised in a drop tower, the wheel is accelerated and is then dropped onto the sensor equipment. Four sensors are installed in one dynamometer for simultaneous measurements of the forces of 900kN Fz and 400kN Fx/y. Another application: the groundbreaking crash wall for high-speed trains – the world's first – that has been operating in China since late July 2017. Its measuring range is 20 times greater than the usual ranges for crash tests in the automotive industry. 

Load tests on space rockets 

Spacecraft payloads such as telescopes and electronic instruments are subjected to strong quasistatic and mechanical-dynamic forces during the test phases of space flight programs. To qualify the structures for space flight, vibration and shock test rigs are used to simulate the vibration levels during the load tests. The Force-Limited Vibration Testing method is used to restrict the force applied and prevent damage to payloads because of excessive forces. To achieve this, 3-component force sensors are integrated on the interface between the shaker and the payload.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.