Kistler unveils optimized digital charge amplifier

Winterthur, November 2020 — Charge amplifiers have a crucial part to play in the piezoelectric measuring chain. Kistler offers charge amplifiers that are tailored to users' needs, with innovative solutions that match customers' specific requirements and digitalization levels. And now, Kistler is launching a new version of its 5074A digital charge amplifier: designated as type 5074B, it incorporates improvements that will enable users to benefit from enhanced flexibility and simpler integration.

Back in 2018, Kistler achieved a breakthrough in industrial charge amplifier technology by introducing its 5074A digital charge amplifier. Launched on the market as the world's first digital charge amplifier, the 5074A is the ideal solution for control and monitoring of industrial processes such as press-fit, assembly and joining operations. It was the only amplifier on the market with communication consistently based on Industrial Ethernet (IE): for the first time ever, it gave plant and machinery manufacturers the possibility of integrating any desired piezoelectric sensors directly into their real time-capable Ethernet systems. Users could comfortably make settings on the measurement amplifier via the control – something that was never possible in the past. Maximum flexibility was ensured by an extremely wide measuring range – from 20 to 1,000,000 pC – coupled with an extensive range of measurement functions for diverse applications, opening up virtually unlimited operational possibilities. All these advantages made the 5074A amplifier the perfect product for applications requiring dynamic and quasistatic measurements via Industrial Ethernet. Another key benefit: high performance by today's standards, allowing acquisition rates of up to 50 kSps per channel and real-time transmission of measurement data with cycle times as low as 100 μs.

"The new 5074B digital charge amplifier, available as of now, supersedes the 5074A – and it retains the range of tried-and-tested benefits offered by its predecessor," says Stefan Affeltranger, Product Manager for Production Monitoring at Kistler. But the 5074B also comes with two features that deliver major operational improvements. The new amplifier is ready to operate within around six seconds, as compared to the previous time of 30 seconds for each startup procedure – so users save valuable time. This improvement has a direct impact on plant availability, especially for modular plants with swappable hot-plug modules. Another innovation: the two energy paths in the M8 connectors are now separated so that additional standard devices can be connected as per the industry standard without extra considerations. This also makes it possible to switch off the peripheral power. "With the new 5074B, additional devices can be installed in the machine very easily and reliably – and what's more, this doesn't result in any further functional restrictions," Affeltranger explains.

Simple implementation at low cost

Like the 5074A predecessor model, the 5074B can also be implemented simply and at low cost. Integration into an existing Ethernet does not require any additional software. Complex and costly cabling for analog and control signals is also eliminated. Configuration via the control means that industrial processes benefit from excellent data security. "The newly available 5074B is a major addition to the family of charge amplifiers from Kistler, which includes analog and digital models as well as a miniature charge amplifier with IO-Link technology," Affeltranger points out. "We're continuously developing our portfolio so that we can respond to users' widely varying requirements by offering innovations and cutting-edge technologies. And this also opens the way for digitalization of the measuring chain in many areas where such a step did not seem technically or economically viable until now."
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.