Kistler Showcases Solutions for Dependable Bolted Joints

Winterthur, 27 October 2016 – At this year's SPS IPC Drives in Nuremberg from 22 to 24 November, Kistler will premiere laboratory systems to analyze bolted joints, calibration equipment and test systems for torque tools, as well as measuring systems for random sample testing. Among the products on show at the stand, the spotlight is on INSPECTpro – the new monitoring system to measure torque and rotation angle – along with cutting-edge products from Kistler's joining and torque portfolio.

In automated production, everything revolves around accurate, reliable process monitoring. Especially in the automotive industry, monitoring and control of bolted joints is hugely important for quality assurance. That's because all the influences that find their way into this process converge at the end of the process chain. Even the smallest errors in the development or assembly process can cause costs running into millions. By integrating Schatz GmbH into the Kistler Group, Kistler is deepening its application know-how in bolted joint technology – so for the first time, customers across the globe have access to bolted joint expertise from one single source.

INSPECTpro for More Transparent Testing Processes

INSPECTpro, the portable measuring device for torque and rotation angle, opens up new possibilities in terms of hardware as well as software: now, process capability checks and random sample inspections during assembly are even easier to perform. Graphic analyses of assembly processes ensure optimal quality in bolted joint assembly. Customers always need testing to be faster and more effective, so new software modules are constantly being developed to ensure easier handling for users and greater transparency in test processes. One new feature is the Tool Management license. Tools to be tested can be stored here ahead of time so they can be conveniently called up later on in Tool Testing mode. The Tolerance Classes software module handles the use of stored tolerance classes in the parameter sets for tool testing/management or bolted joint management.

NCFR – Dynamic Drive Technology and High-Precision Sensors

The latest products from Kistler's range of joining modules will also be on show at the stand: Kistler is presenting its NCFR Joining Module – as well as the classical linear joining process, this system can perform a controlled rotary movement of the ram, either sequentially or even simultaneously. Like the entire family of NC joining systems, the NCFR joining module features a variety of additional benefits: users will appreciate its enormous flexibility and excellent dynamics combined with intuitive operation – so joining processes ranging from simple to highly complex can be handled rapidly and efficiently. Thanks to the servo amplifiers used, all traverse movements that are performed can be controlled with high precision.

Torque Sensor 4503B and KiTorq 4550A: Sensor Technology for Maximum Precision

The cutting-edge sensor technology showcased by Kistler at the SPS IPC Drives in Nuremberg will convince visitors that our company also represents the state-of-the-art when it comes to the development of high-precision torque sensors. The 4503B torque sensor offers a host of extended functionalities, bringing it into line with the very latest market requirements. For instance, optical speed and angle sensing has now been replaced by magnetic technology. This gives the sensor the advantage of added resilience for reliable operation in heavily contaminated industrial environments (e.g. where oil mist is present) – thereby saving valuable time on maintenance. The torque sensor's electronics have also been optimized, and the 4503B now has a cut-off frequency of 10 kHz for highly dynamic measurements.

Another technological milestone on Kistler's stand is the KiTorq 4550A with angle sensing – to enable determination of torque, speed or rotation angle with exceptionally high resolution (up to 8192 pulses per revolution). The number of pulses can be freely adjusted to the requirements as appropriate.

The torque measuring flange system consists of a measuring element, the KiTorq rotor and a torque evaluation unit (the KiTorq stator). With a suitable selection of components for the specific test bench, this system offers excellent flexibility for manufacturers of electrical motors and combustion engines, transmissions, pumps and compressors: this is because the ringless stator makes it possible to use different measuring elements without having to rebuild the entire test setup.

maXYmos TL 1.2 and maXYmos BL 2.3: the Latest Generation of Monitoring Systems

Kistler's stand also highlights the latest generation of maXYmos monitoring systems. Their purpose: to deliver consistent, process-integrated quality assurance. The patterns of measurement curves can be used to monitor and control the quality of a single production step, a sub-assembly or an entire product. Because this control is integrated in the process, the system provides the basis for enhanced transparency in assembly and testing systems – paving the way for increased costefficiencythroughout the production facility. 

Don't miss the trade show date!

If you want to see Kistler's diverse range of solutions for interconnected quality monitoring at first hand, save the dates for the SPS IPC Drives trade show now: it runs from 22 to 24 November 2016 in Nuremberg.



Media Contact:
Simone Koch
Divisional Marketing Manager IPC
Phone: +41 52 224 18 02
Email: simone.koch@kistler.com

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
2017. 10. 9.
Kistler's Type 5074A industrial charge amplifier breaks new ground in industrial charge amplifier technology
2017. 10. 6.
Whether hybrid drives or electric vehicles: anyone who wants to make a change needs to measure and understand
2017. 9. 27.
Our experts will present you Kistler measuring technologies for demanding space applications.
2017. 9. 5.
At Fakuma 2017, we will demonstrate how you can benefit from new ComoNeo functionalities
2017. 8. 31.
Kistler Group showcases the entire spectrum of its integrated quality assurance solutions
2017. 8. 25.
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
2017. 8. 11.
Jaguar Land Rover uses Kistler RoaDyn® Wheel Force Transducers for accurate tyre modelling
2017. 7. 11.
Kistler is taking over IOS GmbH (Germany), provider of Manufacturing Execution Systems (MES).
2017. 7. 6.
Tettnang-based firm eso GmbH was acquired by the Kistler Group on July 5.
2017. 5. 2.
Kistler presents innovative measurement equipment for demanding vehicle testing applications
2017. 4. 25.
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
2017. 4. 12.
Kistler will be present at Control, the world's leading quality assurance trade fair.
2017. 4. 12.
Advanced features for LabAmp family maximize flexibility for cutting force users.
2017. 4. 11.
Measuring equipment for sophisticated T&M applications
2017. 2. 1.
The Kistler Group is constantly growing and recruiting specialist staff worldwide.
2017. 1. 17.
Olympic champion Anthony Ervin and Kistler create a Success Story together.
2016. 12. 2.
Kistler seeks more than 40 specialists in what is likely Switzerland's largest job advertisement.
2016. 10. 27.
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...
2016. 2. 12.
Kistler Lorch GmbH Honored for Outstanding Qualities as Employer
2016. 2. 2.
The Kistler Group has overcome currency-related challenges at its Swiss site to achieve continued growth.
2016. 1. 28.
Accurate Wheel Force Measurement with Minimum Configuration Effort
2015. 11. 26.
Increased Flexibility for High-Speed Combustion Analysis
2015. 11. 2.
New Piezoresistive Sensor with Temperature Probe and Integrated Signal Conditioning.
2015. 10. 27.
Kistler Provides Maximum Flexibility for Product Testing and Development
2015. 10. 16.
Kistler's NCFR Joining Module honored in the handling and assembly category
2015. 10. 5.
Setting the Standard for 100% Control of Linear Joining Processes with Partial Rotation
2015. 9. 18.
Kistler Group: safeguarding the firm's competitive edge.
2015. 9. 15.
Quick evaluation of performance and force with Kistler MARS 2.1.
2015. 9. 3.
Major update for Kistler’s mobile engine indication system.
2015. 9. 1.
Setting New Standards in Automated Process Monitoring for Injection Molding.
2015. 8. 25.
Kistler Showcases Three Latest Product Innovations at Motek 2015
2015. 6. 29.
Kistler Automotive GmbH honored as one of Germany's most innovative companies
2015. 6. 26.
Kistler honored with ASCO Award Gold for best corporate transformation in Switzerland.
2015. 6. 26.
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...