Kistler showcases digital innovations, expands services

Winterthur, 12 October 2017 – At the SPS IPC Drives from 28 to 30 November 2017 in Nuremberg, Germany, the Kistler Group will unveil a new calibration system for torques of up to 100 kNm. Kistler's stand will also feature more milestones in electrical automation: the high-performance torque sensors in the KiTorq series (with real-time capability) and the world's first digital charge amplifier.

Sensors and systems from Kistler help customers get the most from their machinery and plant. For example, they help with inspection and calibration of drives and tools; they are used to monitor and optimize individual production steps and to analyze and automate entire production processes. Now that the era of digitization has dawned, one of the major challenges facing engineers is to continue developing products such as piezoelectric sensors towards the goal of Industry 4.0, ensuring maximum connectivity for automated environments. With one overriding aim: to generate real added value for customers.

Motion control in real time with KiTorq

Kistler has yet again enhanced the potential of its high-performance sensors in the KiTorq series. A transmission rate of 4 kHz now makes the evaluation unit (stator) of this modular series four times as fast when the Profinet or EtherCat interface is used for the connection. For Profinet, this allows the use of IRT mode, enabling real-time communication for isynchronous motion control applications – for instance, this makes torque control possible on the test bench.

The new stator can be combined as desired with the various rotors in the KiTorq system such as KiTorq 4550A (presented at the SPS IPC Drives 2016), delivering measurements of torque, speed or rotation angle with exceptionally high resolution of up to 8192 pulses per rotation.

Calibration for big challenges: high-end testing system available as a service

The new calibration system at the Kistler Group's Lorch facility now offers an exceptional service for customers in the drive technology sector. This system has a usable measurement range of 1 to 100 kNm and is one of the very few plants in this performance class to hold accreditation from DAkkS, the German accreditation body. Thanks to the new system, designers of heavy-duty machinery, ship engines and wind power turbines as well as manufacturers of special-purpose machinery now have the option of intensive testing and optimization for their solutions. This new plant (which ensures traceability) marks another significant expansion of the Kistler Group's range of calibration services.

First in the world: the new digital charge amplifier

Kistler has achieved a breakthrough in industrial sensor technology with its new Type 5074A data acquisition unit. The charge amplifier Type 5074A is currently the only amplifier on the market for piezoelectric sensors with communication consistently based on Industrial Ethernet (IE). For the first time, plant and machinery manufacturers can now integrate any desired piezoelectric sensors directly into a real time-capable Ethernet system, so they can easily make settings on the measurement amplifier via the control.

Stefan Affeltranger, Product Manager in Kistler's Production Monitoring section, is full of enthusiasm about this new product:

The charge amplifier 5074A is the world's only amplifier for quasi-static measurement processes with piezoelectric sensors that offers communication based on real time-capable Industrial Ethernet."

Stefan Affeltranger, Product Manager in Kistler's Production Monitoring section

 

It is also extremely secure, he adds: "Access to the unit is only possible with the appropriate industrial communication protocol; changes to measurement parameters can only be made with access via the master."

Discover the new possibilities at SPS IPC Drives 2017!

If you'd like to get first-hand experience of Kistler's digital innovations and our expanded service offering for test benches and calibration, you're warmly invited to visit us at the trade fair in Nuremberg from 28 to 30 November 2017 on stand 526 in hall 4A!
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.