Kistler showcases cutting-edge testing technology

Winterthur, 11 April 2017 – Kistler will be present at Control, the world's leading quality assurance trade fair from 9 to 12 May 2017 in Stuttgart. The Group will be showcasing Schatz mobile testing systems for bolted joint analysis and tool testing. Other highlights demonstrated at Kistler's fair stand will include the highly dynamic 4503B torque sensor, the latest generation of maXYmos monitoring systems and a wide-ranging portfolio of sensor technology.

By integrating Schatz GmbH into the Group, Kistler has added new depth to its application know-how in bolted joint technology, giving customers across the globe access to expertise on bolted joint testing. Even the smallest errors in the development or assembly process can cause costs running into millions.

Calibration and certification – all in one

Schatz-combiTEST is a mobile system that features dual capabilities: it combines calibration of manual torque wrenches with testing of automated bolting systems. Convenient, on-the-spot testing of all the tools on an assembly line is now possible thanks to this compact device, powered by a rechargeable battery. By ensuring the process ability of their tools, customers can substantially cut their outlay on tool sampling tests that must be carried out regularly, accurately and in compliance with the standards. Visitors to Kistler's trade fair stand can also try out the latest version of the integrated CEUS software: as well as evaluation and documentation of all testing processes, it can be used for certification purposes.

INSPECTpro for transparent testing processes

INSPECTpro, the portable measurement and evaluation instrument from Schatz, offers a convenient way to test torque and rotation angle on bolted joints. This system provides graphic analyses of assembly processes to ensure that bolted joint assemblies meet optimum quality standards.

Testing always has to be faster and more effective, so we are constantly developing new custom software modules that will ensure easier handling and improve the transparency of test processes. One new feature is the Tool Management license: tools to be tested can be stored ahead of time so that later on, they can be called up directly in Tool Testing mode. Kistler will show visitors to the trade fair how easy it is to implement efficient testing processes with INSPECTpro.

Latest-generation monitoring systems: maXYmos 1.4

Kistler's maXYmos product line: the byword for process monitoring systems that deliver integrated quality control of production steps. For the first time, Kistler has now created continuity between maXYmos TL (Top Level) and maXYmos NC (Numeric Control), the system specially designed to monitor electromechanical joining processes. Thanks to the Split View and Multi View features, the XY curves from both systems can be juxtaposed for comparative evaluation. Another innovation: maXYmos 1.4 records changes to the device setup as required. Through process-integrated quality testing, Kistler's solutions deliver process transparency – the basis for boosting cost-effectiveness across the entire production chain.

4503B torque sensor: rugged design with excellent dynamic characteristics

Time and again, Kistler's advanced sensor solutions attest the Group's technological leadership. Yet another example: the 4503B torque sensor with expanded functionality to accommodate the latest market requirements. Optical speed and angle sensing on this rugged sensor has now been replaced by magnetic technology – so it can be used safely in industrial environments with no additional maintenance outlay. Another plus: the torque sensor's electronics have also been optimized, and the 4503B now has a cut-off frequency of 10 kHz for highly dynamic measurements.

Mighty midgets: piezo-based low-force sensors

Thanks to their rugged design, piezoelectric sensors from Kistler keep precise track of quasi-static and highly dynamic force processes, even when conditions are difficult. They offer many advantages over other technologies: proportionality, low measuring deflections and long service lifetimes.

Another advantage: even very small forces can be measured with the quartz elements. For applications of this sort, Kistler offers a wide-ranging portfolio of small force sensors. Miniaturization means that they can also be used when installation space is severely limited. This trend is especially noticeable in the electronics sector, where manufacturers are calling for technical devices and control elements in ever-smaller formats. This poses major challenges for production, because it is essential to guarantee that all manufactured parts have constant quality in terms of functionality as well as haptics.

Experience testing technology in action!

Would you like to see a live demonstration of the Kistler Group's diverse range of solutions for efficient quality assurance – solutions that can meet the challenges of the future? If so, you're warmly invited to visit us on stand 7313 in hall 7 at the trade fair in Stuttgart, from 9 to 12 May 2017.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.