Kistler relaunches its KiBox as a comprehensive powertrain diagnostics system

Winterthur, May 2021 – Ever since Kistler launched its KiBox in 2009, this measurement system for combustion engine development has held a leading position on the market. And now, Kistler is unveiling the KiBox2: a new and completely remodeled version of the KiBox featuring the latest advances in connectivity, usability and software together with capability for conventional, electric and hybrid powertrain analysis. Designed as a modular and extendable platform, the KiBox2 opens the way for development engineers to attain unprecedented levels of efficiency in powertrain optimization.

Automotive design is undergoing a radical transformation: electric and fuel-cell vehicles are gaining ground on global markets – but internal combustion engines will continue to play a key part, with plenty of scope for ongoing optimization. To meet the challenges of this new era in the evolution of the automobile, development engineers need measurement technology that is flexible and easy to use. Kistler's response: the all-new KiBox2, a comprehensive powertrain diagnostics system for engine development. Based on innovative open architecture, this is a complete solution for electric as well as non-electric powertrains – a powerful analytical tool that will help customers minimize their time to market and stay one step ahead of the competition:

  • Versatile in-vehicle and test bench testing, irrespective of electrification level
  • Verified real-time performance for both closed-loop and in-cycle engine control
  • State-of-the-art user interface with active user guidance
  • Maximum connectivity including WLAN, hotspot capability and GPS
  • Full backward compatibility with KiBox, extendable with software upgrades
  • Future-proof system architecture based on flexible hardware and software modules

New modular system architecture featuring state-of-the-art technologies

Modularity is a key advantage of the KiBox2, with both hardware and software designed according to the modular principle. The new solution from Kistler also includes the KiBox Cockpit software: an open ecosystem for parametrization, visualization and analysis that ensures seamless connection to third-party devices. Thanks to the advanced data management functions included, testing efficiency is significantly higher. The user experience is now enhanced by active-intuitive guidance with voice control and audio feedback to guarantee safe and efficient operation while driving. The list of new benefits goes on: an improved signal conditioning for the crank angle sensor, a bidirectional CAN-FD interface, and the option of cascading up to four KiBox2 units including PTP (Precision Time Protocol). 

The key to maximum efficiency in engine development

By integrating measurement and analysis capability for both electric and combustion-based powertrains in the KiBox2, Kistler has developed one of the most versatile and comprehensive powertrain diagnostics systems available on today's market. Outstanding usability, advanced data management features and modular expandability make this solution even more attractive. 

And as an added benefit, customers can enhance their engine development capabilities by using metrics for electric machine efficiency characterization, as well as in-cylinder pressure metrics for “normal” and “abnormal” combustion, including new synthetic fuels. Janko Meier, Product Manager Systems at Kistler, concludes: „The new KiBox2 is a paradigm shift for propulsion system measurement, leveraging the competences of the Kistler Group, to provide a complete, efficient powertrain diagnostic and optimization solution.”

 

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

2022. 7. 28.
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.