Kistler presents first wireless dynamometer (RCD) equipped with a piezoelectric sensor

Winterthur, August 2022 – Kistler brings to market the first wireless RCD (rotary cutting dynamometer) with a piezoelectric sensor. It allows for highly accurate measurements of cutting forces in various machining applications. Part of the measurement system is a new platform (software and hardware) which performs automated analyses that help to increase the efficiency of working processes. Test series, for instance, can be analyzed automatically by using a predefined analysis configuration for each channel. The analogue outputs and digital I/O will enable direct communication with machines and robots not only to monitor but also control processes in the future.

RCDs are used by universities, research centers and in tool and machine development but also for production monitoring to measure cutting forces – specifically in milling, drilling, grinding and super-finishing operations. In machining, part quality, tool life and production time depend on different factors: Dynamometers provide data which give valuable insights into wear mechanisms, material characteristics, or any machine or process abnormalities. The knowledge obtained from these measurements helps to improve product quality as well as the cost-effectiveness of cutting processes. 

Especially in production monitoring, wireless solutions are often preferred since space in machines is limited and the installation of cables to connect the sensor can be difficult or may not be allowed. The wireless RCD from Kistler is the first of its kind equipped with a piezoelectric sensor and connected via wireless technology to the data acquisition device. It comes with four channel piezo crystals to measure torque as well as forces in all three directions (Fx, Fy and Fz). The low energy wireless technology connection has a range up to five meters to the receiver box depending on the conditions on site. 

Higher accuracy with piezoelectric sensor

Piezoelectric sensors feature a large measuring range up to 20 kN with high resolution (<1N) and a high sensitivity. This allows users to employ the same sensor in a wide variety of applications from roughing down to finishing processes. The wireless RCD from Kistler has a 10 kHz sampling rate that allows to capture highly dynamic foot-prints of the measurement in applications with up to 16 000 RPM. Overall, piezoelectric sensors ensure more accurate measurements than other technologies, such as strain-gauge sensors, which have significant limitations especially when measuring small forces and high dynamic processes. Highly accurate measurements are not only important for research but also for production monitoring. The piezoelectric measurement technology can capture very small changes and deviations before they have a significant effect on product quality.

Automated process analysis thanks to new software & hardware platform PTS

The new PTS (Piezo Tool System) software accompanying the wireless RCD automatically acquires and analyzes machining data while the machine is running. Users gain optimal insights into the condition of the cutting tool as the software provides automatic signal trend analysis. In the future, the system will also be able to communicate directly with the machine’s control unit to initiate, for instance, automated tool changes at just the right moment. This leads to less machine downtime, better cost effectiveness and reduced maintenance efforts. Additionally, the PTS platform automates data acquisition, analysis and registration. This will especially improve the efficiency of testing in laboratories and research centers.   

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

2022. 9. 27.
The new SlimLine Sensor 9132CD is nine times more sensitive than comparable SlimLine sensors.
2022. 9. 16.
At K 2022, Kistler will showcase its solutions for injection molding that make plastics processing more intelligent and sustainable.
2022. 9. 6.
With ComoScout, Kistler offers a simple and cost-effective process monitoring system for injection molding processes.
2022. 8. 31.
High-end measurement systems for rolling stock – from brake testing to traffic monitoring.
2022. 8. 22.
Artificial intelligence in punching: AI helps manufacturers improve product quality and step up their quality assurance.
2022. 8. 12.
New wireless dynamometer allows for highly accurate measurements of cutting forces.
2022. 7. 28.
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.