Kistler is setting new standards for electromechanical NC joining systems with the maXYmos NC

Munich, 3 June 2014 – At Automatica 2014 from 3-6 June, Kistler will be showcasing a new joining system comprising maXYmos NC, the IndraDrive servo amplifier and established and proven NC joining modules. The newly developed maXYmos NC monitors and controls the joining process. Equipped with an intuitive touch display, the new system is particularly easy to use, while the integrated sequence control offers a high level of flexibility for straightforward to highly complex joining processes.


Process control made easy
The XY monitors from Kistler's maXYmos series enable customers to visualize and evaluate production processes – allowing them to operate in a consistent, process-integrated manner and to maximize quality assurance. In doing so, they monitor XY curves, where two measured variables must be in a certain relation to each other. Force-displacement curves are a good example of this, which arise from bearings being press-fitted. A further development to the maXYmos product range, the maXYmos NC (Numeric Control) enables NC joining systems to now also be monitored and controlled. Such NC joining systems are predominantly used in the automotive and supply industry in the widest range of manufacturing processes, such as gearbox, motor, chassis or pump installation. The maXYmos NC evaluates and documents the XY curves of joining and press-fitting operations in combination with NC joining modules and the associated IndraDrive servo amplifier. Due to the form of measurement curves, each stage of the production and assembly line – and even the entire product – can be monitored and operated via SERCOS III all in real time. In this way, optimum cycle times can be achieved with the highest degree of repeat accuracy. Unplanned downtimes are minimized as machine availability increases, in turn allowing the productivity of the manufacturing process to be accelerated.


Increased flexibility for users
The integrated sequence control (Sequencer Mode) enables processes to be illustrated without the need for expensive, external PLC programming. Indeed, the programs are set up in a swift, straightforward manner using the intuitive user interface of the touch display. In total, up to 128 programs can be stored, with the option of defining each one with an independent sequence of up to 255 elements. As a result, even highly complex processes can be illustrated simply and effectively. Such processes are evaluated by means of the curve patterns of two measured variables in relation to one another, which are then rated as good (OK) or bad (NOK). For that purpose, ten evaluation objectives are available in each program. Process deviations are reliably detected, while complex process sequences are regulated and controlled. Moreover, the new Multi-View function can be used to simultaneously visualize and compare various processes on the same monitor.


Easily integrated and intuitively operated
The flexible housing concept of maXYmos monitors allows easy integration into existing or newly developed systems. The maXYmos NC comprises two components, the measuring and evaluation module (MEM) and the display module (DIM). These two components can either be installed separately or as a compact unit. Moreover, up to eight joining processes can be visualized on the same display. As such, this guarantees maximum flexibility during installation, whilst saving space and contributing towards an optimum cost-benefit ratio. Furthermore, the measuring and evaluation module (MEM) ticks all the boxes in terms of its variety of interfaces. The most common interfaces such as PROFIBUS, PROFINET, EtherNet/IP and EtherCAT are integrated and can be selected via a menu on the touch display. This allows users to respond to changing requirements in relation to sensor or fieldbus types. In addition, the standardization of MEM development keeps costs for spare part handling to a minimum.


Kistler is presenting the maXYmos NC at Automatica in Munich, Germany from 3-6 June 2014 at stand 425, hall A6.

Press Release (PDF/EN)

Captions
Image 1: The uniform operating philosophy of the maXYmos product range offers users an intuitive and easy-to-use system. This supports straightforward, swift startup of electromechanical NC joining systems.

Image 2: The measuring and evaluation module (MEM) ticks all the boxes in terms of its variety of interfaces. All the standard interfaces are continuously available, ensuring flexibility in the event that the requirements placed on sensor or fieldbus types change, as well as offering considerable advantages in terms of spare parts stocking.

Image 3: The maXYmos NC controls the NC joining module via the servo amplifier through the integrated sequence control. An independent sequence can be defined for each of the 128 programs.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.