Kistler Instrumente GmbH has new German headquarters

Ostfildern, April 27, 2016 – In Sindelfingen, the former Ostfildern and Schönaich sites are being brought together under one roof. The new headquarters are very close to several customers and have plenty of space for future expansion.

Kistler's new German headquarters are on Umberto-Nobile-Straße, named after the Italian aviation pioneer. The pioneering spirit is rooted deep in Kistler's DNA and can be seen not only in the company's many innovations but also the new site, which it is finally unveiling after a planning and construction phase lasting almost 3 years.

Finger on the pulse 

In recent years Kistler has achieved significant global growth. Firstly, the new site provides the space it needs to prepare for the challenges of the future and drive forward further expansion. Secondly, the new, central location also brings Kistler closer to its customers, guaranteeing faster support and even closer contact.

Rolf Sonderegger, CEO of the Kistler Group, is delighted with the new site in Böblingen/Sindelfingen: "The airfield location offers huge potential for development. It was selected mainly due to its proximity to our most important automotive customers and the innovative surroundings in the airfield."

Everything under one roof

The priority in Sindelfingen is to combine the former Ostfildern and Schönaich sites under one roof and therefore bring together all expertise in one location. The one central location is home to elements of production, the tech center, development, sales, human resources, marketing, and finance. The new shared site allows distances to be cut, workflows to be optimized, and processes to be made more efficient.

The modern building with its open-plan concept is also designed as a central point of contact for customers. The entrance area features an atrium, joining the three upper floors by means of a common air space. As well as the reception area, the foyer in the entrance area on the ground floor is also where you will find exhibition spaces, meeting rooms, and two training rooms, which can be linked with the foyer to produce one large room by removing the mobile partitions. When opened up, the new training rooms form part of the reception hall and, depending on the number of people in the training session, can be separated individually. Right next to the training area and reception hall is the production area, where Kistler's products are manufactured, tested, calibrated, and delivered. Production can be viewed through a wide glass front and can of course be visited on prearranged tours.

Focus on lean elements

The new infrastructure is a big step forward for Kistler in terms of production too. Since 2014 and the transition to lean production, the focus in production has been on the environment and simple and quick sequences of processes. All the processes undertaken at Kistler Germany are coordinated for smooth interaction between production, logistics, calibration, and service to guarantee as efficient a production workflow as possible.

Efficient building

Efficiency is also important for the building itself. For example, the offices and production areas are mainly heated and cooled by means of concrete core activation. Ventilation, air extraction, and air conditioning of the various areas take place as required and the relevant systems use highly efficient heat recovery. Individual extraction units, with direct links to the outside, are also used sporadically in the test hall and workshop. An air-water heat pump with a COP >4 cools the building and it is heated using waste heat from the refrigeration machines and district heating. The building's electricity is provided by its own in-built transformer station. The building has a low voltage main distribution board and one electric distribution room on each loor. The server room also has a redundant fiber-optic network and cooling system.

Kistler as an attractive employer

Kistler's new German headquarters are large enough for the current workforce of around 180 from the Ostfildern and Schönaich sites and forms the basis for a large future. The company operates in a growing sector so expansion needs to be driven forward and the new Sindelfingen site is already set up to accommodate up to 300 members of staff. Once this level is reached, another floor can be added to the current production area.

It goes without saying that the Kistler Group is always looking for qualified people and, as an attractive employer, wants to do its bit for the Böblingen/Sindelfingen region and establish itself as an important part of the community. 

Download Press Release (PDF)
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.