Kistler and BIG KAISER partner for precise measurement of cutting forces

Stuttgart, 18th September 2018 - At the International Exhibition for Metal Processing (AMB) in Stuttgart, Hall 1, Booth 1A61, Kistler and BIG KAISER are showcasing how their collaboration will help customers. The two companies are exhibiting a new system, where Kistler’s Type 9171A rotating dynamometer and BIG KAISER’s MEGA New Baby Chuck are combined to deliver high levels of accuracy in cutting force measurement.

The BIG KAISER MEGA New Baby Chuck offers higher precision than traditional ER clamping systems, delivering superior runout accuracy. BIG KAISER has specially adapted the interface on the MEGA New Baby Chuck to ensure it connects securely and accurately to the Type 9171A. As a result, Kistler’s customers can now achieve noticeably lower total radial runout errors by using this dynamometer. 

This means that they benefit from improved cutting force measurement accuracy, enabling them to increase the lifetime of cutting edges. For customers using the dynamometer in their own production processes, its high precision enables them to develop machining strategies that increase tool lifetimes and thereby reduce overall cost. In manufacturing, it enables tools to be replaced before they break, as increased forces at the cutting edge indicate that a failure is imminent.

The Type 9171A is a piezoelectric dynamometer for use in high-performance cutting applications. It measures forces and torques even under very high loads at speeds up to 12,000 rpm, allowing machining processes to be analyzed and optimized while obtaining information on tool wear. Compared to previous dynamometer models, the Type 9171A delivers a much wider range of spindle speeds with improved dynamic properties and a significant weight reduction. It is particularly suited to multi-component force and torque measurements on rotating tools during milling and drilling.

BIG KAISER's collet chucks offer high accuracy for any machine spindle, with a guaranteed runout of 0.001 mm at the collet nose and less than 0.003mm at 4xD. The MEGA New Baby Chuck is the company’s most popular collet chuck for diameters up to 25 mm. All MEGA collet chucks have a notch-free MEGA nut that prevents vibration and reduces noise levels. These chucks are tightened using a unique MEGA wrench that can safely and evenly apply force along the entire nut periphery.

Innovative design and high precision

Gunnar Keitzel, Head of Cutting Force, Kistler, said, “Tool holders from BIG Kaiser are characterized by an innovative design, which has been optimized for high-speed machining. Kistler is pleased to now also be able to offer rotating cutting force systems with these high-precision interfaces, including the innovative MEGA New Baby Chuck."

Stefan Appenzeller, Head of Product Marketing, BIG KAISER, said, “Kistler’s 9171A is a market-leading dynamometer that provides the highest levels of precision. Together, BIG KAISER and Kistler can now help customers develop and improve their cutting processes.”


The International Exhibition for Metal Processing (AMB) is held in Stuttgart, Germany from 18th to 22nd September 2018. 1,500 exhibitors from more than 30 countries will present the latest machine and precision tool developments as well as other machining solutions. In 2016, approximately 90,000 visitors attended the AMB, and this year an extra exhibition hall has been added.


The Type 9171A dynamometer and MEGA New Baby Chuck, with the adapted interface to fit the Type 9171A, are available from Kistler now.

Image material (please name the Kistler group as picture source)

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

2022. 7. 28.
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.