KiRoad Wireless HDR: the new cable-free solution for vehicle developers

Winterthur, June 2021 – The Kistler Group is launching the world's first wireless wheel force measurement system – an innovation that will massively reduce the effort involved in vehicle dynamics, durability and tire testing. The new KiRoad Wireless HDR features far-field telemetry compliant with the 2.4 GHz WLAN standard, and it can be used with existing RoaDyn wheel force transducers.

Vehicle developers use high-precision wheel force transducers (WFTs) to measure wheel forces and moments directly on the hub, yielding data that is especially critical for durability tests. These measurements are also used to evaluate vehicle dynamics and characterize tire performance. Wheel force transducers in the RoaDyn series were the first systems that used near-field telemetry to transmit data to the vehicle – and now, the measurement technology experts at Kistler have broken new ground yet again.

KiRoad Wireless HDR (High Data Rate) features remote wireless transmission for wheel force measurements – eliminating the need for time-consuming adaptations and cabling both inside and outside the vehicle. Automobile and tire manufacturers, suppliers to the automotive industry, research institutions and motorsport teams are among the many users who will benefit from reduced installation effort and easy operation – freeing up valuable time for over-the-road and on-track testing.

Cable-free measurements – with no protruding parts on the vehicle

This modular system consists of three components that are compatible with the 6-component wheel force transducers from Kistler, already established as the industry standard: the onboard unit (electronics), the wheel unit and the rotary encoder. Key features and benefits of KiRoad Wireless HDR:

  • Data transmission via WLAN (wireless standard: IEEE 802.11n)
  • No protruding parts – so vehicle contours are unchanged
  • Replaceable battery pack with minimum capacity of 4 hours at –20°C (e.g. for winter tests)
  • Digital data output for all channels via CAN, DTI and Ethernet
  • System configuration and visualization of measurement results in KiCenter software or browser

A new rotary encoder concept used with the KiRoad Wireless HDR eliminates the need to attach any equipment to the outside of the vehicle. The wheel unit, with its integrated calculation and transmitter unit, is designed to be waterproof and is easy to install and remove, thus minimizing setup time for the test engineer.

KiRoad Wireless is easy to retrofit on Kistler RoaDyn WFTs

All RoaDyn WFTs that are currently in operation can be equipped with KiRoad Wireless HDR. This gives Kistler's customers the benefits of a cable-free measuring system for all 6-component WFTs: they can measure all forces and moments on the wheel in each of the three spatial directions, as well as wheel angle and angular speed. The new system met every expectation throughout intensive practical testing with pilot customers, and KiRoad Wireless HDR is available as of now.

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

2022. 9. 27.
The new SlimLine Sensor 9132CD is nine times more sensitive than comparable SlimLine sensors.
2022. 9. 16.
At K 2022, Kistler will showcase its solutions for injection molding that make plastics processing more intelligent and sustainable.
2022. 9. 6.
With ComoScout, Kistler offers a simple and cost-effective process monitoring system for injection molding processes.
2022. 8. 31.
High-end measurement systems for rolling stock – from brake testing to traffic monitoring.
2022. 8. 22.
Artificial intelligence in punching: AI helps manufacturers improve product quality and step up their quality assurance.
2022. 8. 12.
New wireless dynamometer allows for highly accurate measurements of cutting forces.
2022. 7. 28.
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.