It pays to take a closer look

Straubenhardt, September 2018 - Vester – a Kistler Group company – will demonstrate its all-round expertise in test automation for plastic and hybrid parts at the Fakuma 2018 trade fair from 16 to 20 October in Friedrichshafen . At stand 6112 in hall A6, visitors can see how 100% process control for series parts is implemented efficiently with Vester's latest-generation VVC 821 and VVC 620 automatic test systems, which can be integrated into automated production lines as required.

There can be no doubt that injection molding has become more complex and challenging: multi-cavity molds and innovative processes now make it possible to produce complex geometries and exceptionally intricate plastic or hybrid parts. But these advances also create more demanding standards for quality assurance and product testing: 100% control of manufactured parts and end-to-end documentation of the production process are increasingly specified as requirements. To meet these challenges, Kistler offers appropriate components, systems and solutions from one single source.

For plastics processors and service providers, automatic testing and sorting systems from Vester – a Kistler Group Company – are the solution of choice: they combine process reliability with efficient quality monitoring, including automated segregation of good and bad parts. Modular test cells equipped with appropriate camera and illumination technology allow end-to-end testing of dimensions, geometries and other component attributes – combined with high throughput rates and outstanding precision.

End-to-end quality testing with high throughput rates

The VVC 620 is an automated testing system equipped with up to six cameras, used for integrated testing of continuously manufactured parts. It can be flexibly integrated into production lines, and it allows dimensional inspection, contour tracing and detection of surface defects at high processing speeds of up to several hundred parts per minute. Users enjoy maximum comfort thanks to a touchscreen, and they can make individual settings to handle faulty parts.

Vester is also showcasing the VVC 821, the latest version of its successful automated rotary plate tester that meets the most advanced requirements. Yet another highlight on display at the Fakuma: the VVC 821/C with integrated feed, which can achieve testing and sorting rates of up to 700 parts per minute. The VVC 821 is ideal for dimensional inspections of single parts and attributive surface testing; a module for hardness testing can also be integrated as an option.

Successful integration ensures continuity

Test automation solutions are essential whenever the objective is to ensure quality-conscious, reliable production while safeguarding business interests. Vester test cells play a key part in achieving these goals – not only by helping to achieve near-perfect part quality, but also by delivering results that provide users with a basis for optimizing their own production.

After a little more than a year, Vester Elektronik GmbH of Straubenhardt (Baden, Germany) has been successfully integrated into the Kistler Group – as is clear, for instance, from the continuous growth of its workforce. All Kistler's existing and new customers can rely on tried-and-tested processes – and they also benefit from access to a proven test automation portfolio backed by comprehensive advice and services. Thus, Kistler is successfully focusing expertise in multiple fields to offer one single source for industrial manufacturers across a variety of sectors.

Experience test automation – live!

Your personal advisors at Vester – a Kistler Group Company – are looking forward to welcoming you warmly to stand 6112 in hall A6 at the Fakuma in Stuttgart from 16 to 20 October 2018.

Visuals (Reproduction is free of charge provided that the Kistler Group is credited as the source of the image)
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.