Integral powertrain analysis of a plug-in hybrid

Winterthur, October 2019 – Kistler is collaborating with the University of Bath (UK) on a joint research and development project that focuses on comprehensive characterization of the powertrain in a vehicle with a plug-in hybrid drive concept. A combination of different measuring systems supplies a full and accurate picture of the vehicle's dynamics and driving behavior. 

Reducing emissions and cutting fuel consumption: these are two of the main requirements that are driving advances ahead in the automotive industry. Attention is constantly focused on electrification, and electrified powertrains are increasingly becoming established as the standard on the European market and beyond. The term "electrification" now includes the whole spectrum from start-stop technology for combustion engines to fully battery-driven electric powertrains. But this transformation also involves greater complexity for developers and additional challenges for manufacturers  –  with added pressure due to the need for short development cycles.

How does measurement technology from Kistler help to meet these requirements and generate added value for vehicle manufacturers? To take one example: by delivering reliable, high-quality measurement data that makes it easier to arrive at design-related decisions in the early phases of development. Let us take a detailed look at an assignment of this sort with the help of a specific example: a plug-in hybrid vehicle.

Interaction between various Kistler technologies

Kistler is collaborating with the University of Bath (UK) on a joint project to investigate the requirements for measurement technology that will be set by the powertrains of the future. For this purpose, a state-of-the-art vehicle from a renowned manufacturer in southern Germany has been made available to Andrew Lewis of Bath University and Simon Regitz, Head of Development at Kistler. The vehicle is equipped with a drive concept (plug-in hybrid) that presents various challenges in terms of development. The research forms part of a larger government-sponsored project that aims to define future development processes as combinations of vehicle simulation and distributed over-the-air measurement data (for more details, see: vchuv.uk).

One of the main challenges facing the researchers was to characterize the overall performance of the powertrain: this would enable a precise combination of laboratory conditions and on-road driving situations, leading to in-depth understanding of the powertrain's behavior in real time. This requires an accurate analysis of the powertrain's inputs, outputs and control strategies  –  including the torque and energy flows throughout the entire system.

To accomplish this task, various Kistler technologies were used in interaction with one another: the KiBox indicating system (for parameters related to the combustion engine and torque), the RoaDyn P106 wheel force transducer system on all driven wheels (for drive torque and braking forces), and torque measurement technology on the drive shafts (for torque distribution and recuperation). In addition, the control unit data was recorded and the current to the belt-driven starter generator was measured. A complete description of the vehicle's drive system becomes possible when this wealth of information is combined with integral analysis.

In-depth understanding of the powertrain is the key to optimization

The research produced some surprising discoveries: the estimated battery capacity, for instance, proved to be significantly lower than expected. It was also possible to determine strategies for rapid response behavior with a dynamic accelerator. Information of this sort is essential for manufacturers who want to understand the performance of their powertrains under real driving conditions while minimizing interventions in the operation of the powertrain. First and foremost, however, this application shows just how much can be achieved with measurement technology solutions from Kistler – especially when they are combined for the purpose of integral analysis.

Initial results from this collaboration were set out in a joint paper that was presented at the 13th International Symposium on Propulsion Diagnostics in Baden-Baden. This work points the way for the development of Kistler's vehicle measurement technology in the near future. It is also an excellent example of our activities in the powertrain segment that aim to help manufacturers accomplish their development assignments. As the next step in our cooperation with the University of Bath, we intend to collect more measurement data during actual driving. The focus is on one question in particular: how does the drive system manage energy and torque flows in order to support vehicle dynamics and improve drivability?
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.