How artificial intelligence is changing quality assurance in punching

Winterthur, August 2022 – Information about progress of production and assured quality down to component level: even for the very smallest parts, requirements for traceability and quality are increasing in every industry – and the punching and stamping sector is no exception. To meet these growing expectations, punched part manufacturers need to vastly step up their quality control. How can a combination of an optical inspection system equipped with AI software and a laser marking process help them achieve this goal? In this interview, the answers are explained by three Kistler experts: Dr.-Ing. Oliver Schnerr, Head of Global Sales – Integrated Solutions, Stephan Bellem, Head of Test Automation and Head of Engineering, and Ferenc Toth, Head of Vision Systems. 

What do the increasing requirements for quality and traceability mean for punched part manufacturers? 

Schnerr: These requirements really do present a major challenge for the punching and stamping industry. Alongside high part quality, efficiency is an essential requirement – and the aim is to ensure production with the minimum possible scrap rate. Another challenging requirement is accurate and detailed documentation throughout the production chain, so manufacturers can protect themselves against recourse claims: it should be possible to implement this with maximum efficiency. 

Bellem: The solution we’ve developed at Kistler makes us the first provider to launch a complete package on the market. The individual parts are checked with the "shape-from-shading" optical inspection process, which uses software equipped with artificial intelligence (AI) to detect any quality-relevant defects. An additional feature is an integrated laser marking process which then adds an identification number to the individual parts. By networking the system with the surrounding machines, we also make it easier to implement comprehensive process monitoring. As well as marking the individually inspected parts and storing the relevant documents in a database, the system saves information about the upstream and downstream steps of the process. What's more, the inspection system itself analyzes its own functionality before each batch or shift and generates a corresponding functional capability record: this is part of the Measurement System Analysis.

Toth: Thanks to comprehensive documentation for the production chain, we’re evolving from the random sample databases of the past towards complete inspection and traceability of the manufactured parts. This opens the way for users to take a major step towards digitalizing their production and process monitoring. 

What is special about the "shape-from-shading" optical inspection method?

Toth: This process makes use of special illumination and imaging technology to separate information about the texture of an inspected part from its topological characteristics. To achieve this, the part to be inspected is illuminated from several directions and captured by a camera. This results in images where light and shade are distributed differently. We can then use these (real) individual images as the basis for calculating various topographical images which only show the 3D information about the surface of the inspected part. This makes the process independent of changes in the surface of the inspected part, such as color or brightness differences that would show up clearly in the texture image and thus prevent stable evaluation. In this way, even scratches, cracks or indentations with heights or depths of only a few micrometers can be detected reliably with conventional image processing methods.

Schnerr: This process makes it possible to identify minimal defects in the surface of an individual inspected part. But that's not all: the method also ensures detection of surface defects that are actually relevant to quality – and that's another crucial advantage for manufacturers. It allows them to vastly reduce their pseudo scrap rates.

How is AI used for optical quality assurance?

Toth: Artificial intelligence makes quality assurance easier throughout the production chain. To start with, the deep neural network is fed with images of OK parts, so it "learns" their characteristics. Since our customers specialize in producing OK parts, a vast quantity of data is available to us. If the image of a part deviates from these characteristics, the AI software recognizes this and triggers separation of the part as appropriate. After a few production batches, we can then feed the software with more images of OK parts that may have different characteristics than the parts inspected in the first round. In this way, we continue to refine the AI – and we can also minimize the percentage of pseudo scrap even further.

Schnerr: By deploying artificial intelligence in quality assurance, we can achieve some major advances – especially as regards unusual defects, or those that only occur sporadically. The parameters defined in advance for conventional rule-based inspection methods often fail to identify these defects, so parts with faults of this sort remain undetected and are not separated out. 

Will AI-supported quality inspection supersede conventional optical inspection methods?

Schnerr: I think that's rather unlikely. Going forward, manufacturers will in all probability use a combination of the two methods – because one of these processes cannot replace the other one. The conventional processes will continue to be used for defect characteristics that we can describe in adequate detail with rule-based mathematical methods. AI-based inspection is the more obvious choice for detecting unusual faults, or those which only occur rarely.

Let’s dare to take a look into the future: in which areas will AI become the technology of choice?

Schnerr: In the future, we will mainly be using AI in cases where we want to make statements about the quality of parts, but where it’s very difficult to describe the defects with mathematical methods. Here at Kistler, we’re already making use of artificial intelligence in several areas: one example is plastic injection molding technology for the manufacture of medical devices, where quality calculations are based on cavity pressure data. Users always need to consider which method is most suitable for their requirements in each individual case. To assist with this, we are standing by to advise our customers right from the start. We check out the places where it doesn't make sense to use AI, and we also work out where – and how – quality control can be implemented optimally with the help of AI.

Read our Technical Paper

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

2022. 9. 27.
The new SlimLine Sensor 9132CD is nine times more sensitive than comparable SlimLine sensors.
2022. 9. 16.
At K 2022, Kistler will showcase its solutions for injection molding that make plastics processing more intelligent and sustainable.
2022. 9. 6.
With ComoScout, Kistler offers a simple and cost-effective process monitoring system for injection molding processes.
2022. 8. 31.
High-end measurement systems for rolling stock – from brake testing to traffic monitoring.
2022. 8. 22.
Artificial intelligence in punching: AI helps manufacturers improve product quality and step up their quality assurance.
2022. 8. 12.
New wireless dynamometer allows for highly accurate measurements of cutting forces.
2022. 7. 28.
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.