High-precision measurement data for the optimization of cooling lubricants

Blaser Swisslube AG, located in Hasle-Rüegsau, is a leading manufacturer of lubricants for metal parts manufacturing. In the development of new cooling lubricants, the Swiss company relies on Kistler's measurement expertise. High-precision measurement data ensures that the cooling lubricants are adapted exactly to the application requirements and that they function reliably in practical use.

More than Eighty specialists, research and experiment engineers at Blaser Swisslube are located in the Development and Technology center, with the goal to solve present and future challenges. The development of new machines, materials and processes leads to new application areas for cooling lubricants and, thus, to new challenges. To address these challenges, the properties of newly developed cooling lubricants are tested and optimized. Blaser Swisslube generates measurement data under industrial operating conditions with the goal of recording a wide range of parameters for analysis of cooling and lubricating behavior.

Because cutting force components are directly related to the tribological ratios in the cutting zone, recording these components is very important in assessing new lubricant recipes. This information can be used to gain detailed knowledge of the lubricating properties of a cooling lubricant and its constituent parts as well as to analyze the influences of the cooling lubricant with increasing tool wear. The demands on the dynamics and accuracy of the measuring system are likewise correspondingly high. It is important that the stability in the cutting process not be negatively influenced. The conditions of industrial production can thereby be maintained and valid measurement results obtained. For measurements in this extreme range, a very rigid and compact measuring system must be used.

The Kistler 3-component measuring system 9129A is used in the measurements performed by Blaser Swisslube. The instrument satisfies all requirements with respect to accuracy, dynamics and very high rigidity. Furthermore, it is compact and can be installed directly in the machine without significant effort. The system is used in all cutting tests on the lathe and delivers reliable data on cutting force, feed force and passive force. Thanks to the piezo technology that is used, the measuring range and the resolution can easily be adapted to the respective application without changing the stability of the system.

By constantly recording the force, Blaser Swisslube is able to compare cooling lubricants and their constituent parts.

Depending on the cooling lubricant technology, the force distributions vary greatly. Together with other modern measurement tools, we are thereby able to exactly record the mechanisms of action of the cooling lubricant in the cutting process."

Manfred Schneeberger, process engineering manager at Blaser Swisslube AG

 

The Development department benefits from the knowledge gained: future cooling lubricant solutions can be even more precisely tailored to the respective requirements.

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
2017. 10. 9.
Kistler's Type 5074A industrial charge amplifier breaks new ground in industrial charge amplifier technology
2017. 10. 6.
Whether hybrid drives or electric vehicles: anyone who wants to make a change needs to measure and understand
2017. 9. 27.
Our experts will present you Kistler measuring technologies for demanding space applications.
2017. 9. 5.
At Fakuma 2017, we will demonstrate how you can benefit from new ComoNeo functionalities
2017. 8. 31.
Kistler Group showcases the entire spectrum of its integrated quality assurance solutions
2017. 8. 25.
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
2017. 8. 11.
Jaguar Land Rover uses Kistler RoaDyn® Wheel Force Transducers for accurate tyre modelling
2017. 7. 11.
Kistler is taking over IOS GmbH (Germany), provider of Manufacturing Execution Systems (MES).
2017. 7. 6.
Tettnang-based firm eso GmbH was acquired by the Kistler Group on July 5.
2017. 5. 2.
Kistler presents innovative measurement equipment for demanding vehicle testing applications
2017. 4. 25.
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
2017. 4. 12.
Kistler will be present at Control, the world's leading quality assurance trade fair.
2017. 4. 12.
Advanced features for LabAmp family maximize flexibility for cutting force users.
2017. 4. 11.
Measuring equipment for sophisticated T&M applications
2017. 2. 1.
The Kistler Group is constantly growing and recruiting specialist staff worldwide.
2017. 1. 17.
Olympic champion Anthony Ervin and Kistler create a Success Story together.
2016. 12. 2.
Kistler seeks more than 40 specialists in what is likely Switzerland's largest job advertisement.
2016. 10. 27.
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...
2016. 2. 12.
Kistler Lorch GmbH Honored for Outstanding Qualities as Employer
2016. 2. 2.
The Kistler Group has overcome currency-related challenges at its Swiss site to achieve continued growth.
2016. 1. 28.
Accurate Wheel Force Measurement with Minimum Configuration Effort
2015. 11. 26.
Increased Flexibility for High-Speed Combustion Analysis
2015. 11. 2.
New Piezoresistive Sensor with Temperature Probe and Integrated Signal Conditioning.
2015. 10. 27.
Kistler Provides Maximum Flexibility for Product Testing and Development
2015. 10. 16.
Kistler's NCFR Joining Module honored in the handling and assembly category
2015. 10. 5.
Setting the Standard for 100% Control of Linear Joining Processes with Partial Rotation
2015. 9. 18.
Kistler Group: safeguarding the firm's competitive edge.
2015. 9. 15.
Quick evaluation of performance and force with Kistler MARS 2.1.
2015. 9. 3.
Major update for Kistler’s mobile engine indication system.
2015. 9. 1.
Setting New Standards in Automated Process Monitoring for Injection Molding.
2015. 8. 25.
Kistler Showcases Three Latest Product Innovations at Motek 2015
2015. 6. 29.
Kistler Automotive GmbH honored as one of Germany's most innovative companies
2015. 6. 26.
Kistler honored with ASCO Award Gold for best corporate transformation in Switzerland.
2015. 6. 26.
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...