First-ever use of RoaDyn for microcar road testing in Japan

Winterthur, July 2021 – Thanks to a new approval from the Japanese government, Kistler can now meet the requirements for testing on public roads with the RoaDyn S635, its six-component wheel force transducer (WFT). The RoaDyn passed comprehensive tests to prove compliance with the local JWL (Japan Light Wheel Alloy) standard. For the first time ever, the WFT can now be used for tests in local road traffic on microcars from a Japanese manufacturer.

RoaDyn wheel force transducers from Kistler are used for test drives on public roads and test tracks, off-road testing, and also on vehicle test benches. They detect the load applied to the wheel by connecting each of the load cells to the wheel rim and hub, with the help of a vehicle-specific adapter. The signals are amplified directly in the load cells, and then they are filtered, digitized and coded by the hub electronics.

Next, the data is transmitted by telemetry (inboard transmission), via a rotor/stator pair mounted on the inner side of the wheel (rotor) and wheel suspension (stator); this is followed by processing with the onboard electronics, and output to a data acquisition device. In this way, the RoaDyn S635 delivers precise measurement results that provide a valuable basis for vehicle development work. 

Inboard transmission eliminates the need for external components

In the RoaDyn S635, the telemetry is located on the inner side of the wheel to minimize projection over the wheel contour. This allows the WFT to be used on public roads. All structural parts and wheel rims are designed and manufactured by Kistler. An FEM strength simulation analysis ensures that the six-component WFT can handle the loads stated on the data sheet.

Thanks to its modular structure based on individual load cells, this WFT has the flexibility needed to meet varying requirements for hub and rim geometries, load, and measurement range. All the signals are digital, ensuring that high data integrity is maintained during transmission.

RoaDyn S635 passes extensive series of JWL tests

The JWL (Japan Light Wheel Alloy) norm was introduced by the Japanese Ministry of Land, Infrastructure, Transport and Tourism as a standard to improve the safety of light alloy wheels. Use on public roads is permitted only if the requirements set by this standard are met. To comply with the JWL standard, the RoaDyn S635 from Kistler had to undergo three extensive tests. After successfully meeting the criteria, the six-component WFT from Kistler was granted JWL certification.

The first stage of the approval process was a rotary bending test, focusing on the rotational loads and moments that act on the wheel during driving. A clamping device on the rim flange was used to clamp the wheel force transducer – comprising load cells, structural elements, and the aluminum rim – onto the test equipment. The transducer was then exposed to a rotary bending moment over the mounting surface of the wheel hub. 120,000 cycles were completed. Next came a radial load endurance test, using a machine equipped with a drum: in this case, over 600,000 cycles were performed. The final hurdle was the impact test, when the wheel was placed on a mounting plate, fixed, and inclined by 13 degrees. A free-falling weight was dropped onto the edge of the rim flange, and the wheel was then examined for cracks, deformations, and air leaks.

After each of the three tests, a dye penetrant inspection was carried out to check for cracks. The RoaDyn S635 six-component wheel force transducer from Kistler successfully met the high requirements in all the test phases. And as additional proof of excellence, an electromagnetic compatibility examination of the telemetry yielded equally successful results.

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

2022. 8. 12.
New wireless dynamometer allows for highly accurate measurements of cutting forces.
2022. 7. 28.
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.