Torque Sensors and maXYmos

Winterthur, October 27, 2015 – At this year's SPS IPC Drives (November 24-26,2015), Kistler will be presenting its latest torque sensor portfolio in combination with the extended maXYmos family, as well as the latest applications in the field of product testing and development.

In the industrial production sector, more and more manufacturers rely on Kistler sensor technology to monitor each stage of the assembly process when manufacturing safety-related components. As a leader in the field of measuring and system technology with a wide range of torque sensors, Kistler provides the ideal solution for every application – whether in testing couplings, testing torque to determine screw quality, or testing the push-and-turn caps on nasal sprays. In addition, Kistler's high-precision torque sensors are also used in the field of development; for example, to determine the efficiency of electric motors or friction coefficients at test benches.

Product Testing with maXYmos TL: Higher Quality and Lower Costs
By gradually expanding its product portfolio, Kistler has secured its reputation worldwide as a leading supplier of sensor systems. Thanks to the innovative development of the maXYmos family in particular, the uniformity of the systems and their simple, intuitive handling are now part of day-today industrial manufacturing operations. When testing products, users can access a simple system that enables them to perform various tests quickly and accurately – not only by force-displacement monitoring, but now also by monitoring the torque over time or angle of rotation.

With its wide range of interfaces, the system provides an ideal platform for recording a large number of measurands and their evaluation. Thanks to the user-friendly ‘Sequencer Mode’, test sequences can be programmed in the device and analyzed online in real-time. These sequences can easily be parameterized on the device and perform simple control tasks.

The maXYmos TL detects defective parts or deviations early in the production process and displays them transparently. This leads to minimized downtimes, optimized test sequences, and improved plant availability. Thus, the integrated process control enables higher quality and lower costs in assembly and testing.

Torque Sensors: Central Role in Product Development
Kistler’s sensor technology is not only used in direct product testing in the production process, but also in the test bench field for quality monitoring. The accuracy and flexibility requirements for test systems, i.e. evaluating the efficiency of power train components, continue to grow. Robust, highly accurate torque sensors are particularly in demand for determining friction coefficients and performance factors.

Latest Torque Portfolio for Maximum Accuracy
Visitors to this year's SPS IPC Drives can be convinced that Kistler is leading in the development of high-precision torque sensors. Kistler will be presenting the KiTorq Type 4550A with angle measurement for the first time. Compared to the KiTorq Type 4551A, this newly developed sensor now enables the measurement of torque, speed, and rotation of angle with an unprecedented resolutionof up to 8 192 pulses per revolution. The number of pulses can be freely adjusted to meet the user’s requirements. The torque measuring flange system consists of a measurement body, the KiTorq rotor, and an evaluation unit (the KiTorq stator). For manufacturers of electric and combustion engines, drives, pumps and compactors, the system provides wide flexibility thanks to the guideless stator in that measurement bodies can be used without having to completely rebuild the test facility.

Type 4503B, also being presented at this year’s SPS IPC Drives, offers a number of enhanced functions to satisfy current industry standards. For example, optical speed and angle measurement have been replaced by a magnetic one. This means the sensor is now safe and robust enough for use in contaminated industrial environments (e.g., oil mist), which saves valuable maintenance time. Furthermore, the electronics of the torque sensor have been improved. For highly dynamic measurements, Type 4503B also has a cut-off frequency of 10 kHz. Users can customize it individually via an integrated digital low-pass filter, while the second measuring range can be flexibly scaled up to a spread of 1:10. In addition, the Type 4503B is characterized by large measuring ranges of 0.2 … 5 000 Nm, as well as an integrated rotational speed/angle measurement up to 8 192 pulses/revolution and a high-speed version with up to 50 000 rpm.

Innovative Products for a Dynamic Market
With the KiTorq Type 4551A and 4503B torque sensors, as well as the new KiTorq Type 4550A with angle measurement, Kistler's torque sensor portfolio fulfills all market requirements as these sensors offer maximum dynamics and accuracy for industrial manufacturers. Compatible with previous
versions, the new torque sensors can also be integrated in existing systems with minimal effort. The key benefits of the maXYmos monitoring system also apply to the torque sensors presented at the SPS IPC Drives: They improve transparency in the testing process, and therefore boost quality and reduce production costs.

Kistler is presenting its newest sensors and systems at SPS IPC Drives in Nuremberg from 24 to 26 November 2015, booth 526 in hall 4A.


Download Press Release (PDF)

User Contact
Stephan Vogel
Business Development Manager
Phone: +49 7172 184 187
Email: stephan.vogel@kistler.com

 

Media Contact
Simone Koch
Divisional Marketing Manager IPC
Phone +41 52 2241 802
Email: simone.koch@kistler.com

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
2018. 7. 25.
On her way to Olympia 2020 she relies on Kistler Group measurement experts.
2018. 7. 18.
Effective monitoring with strain sensors protects machines and tools
2018. 7. 3.
The Top 100 Competition has again singled out the most innovative German small and medium-sized enterprises (SMEs) for the 10th time.
2018. 6. 25.
Kistler is pleased to introduce MicroDyn, the world's smallest series-produced cutting force meter.
2018. 6. 19.
Kistler introduces the world’s first high temperature accelerometer for the monitoring of gas turbines.
2018. 6. 11.
Kistler is earmarking the highest investment budget for research and development in the company`s history.
2018. 5. 11.
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
2017. 10. 9.
Kistler's Type 5074A industrial charge amplifier breaks new ground in industrial charge amplifier technology
2017. 10. 6.
Whether hybrid drives or electric vehicles: anyone who wants to make a change needs to measure and understand
2017. 9. 27.
Our experts will present you Kistler measuring technologies for demanding space applications.
2017. 9. 5.
At Fakuma 2017, we will demonstrate how you can benefit from new ComoNeo functionalities
2017. 8. 31.
Kistler Group showcases the entire spectrum of its integrated quality assurance solutions
2017. 8. 25.
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor technology and test automation.
2017. 8. 11.
Jaguar Land Rover uses Kistler RoaDyn® Wheel Force Transducers for accurate tyre modelling
2017. 7. 11.
Kistler is taking over IOS GmbH (Germany), provider of Manufacturing Execution Systems (MES).
2017. 7. 6.
Tettnang-based firm eso GmbH was acquired by the Kistler Group on July 5.
2017. 6. 20.
Perfect production data synchronization through direct MES system integration.
2017. 5. 2.
Kistler presents innovative measurement equipment for demanding vehicle testing applications
2017. 4. 25.
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality assurance in injection molds.
2017. 4. 12.
Kistler will be present at Control, the world's leading quality assurance trade fair.
2017. 4. 12.
Advanced features for LabAmp family maximize flexibility for cutting force users.
2017. 4. 11.
Measuring equipment for sophisticated T&M applications
2017. 2. 1.
The Kistler Group is constantly growing and recruiting specialist staff worldwide.
2017. 1. 17.
Olympic champion Anthony Ervin and Kistler create a Success Story together.
2016. 12. 2.
Kistler seeks more than 40 specialists in what is likely Switzerland's largest job advertisement.
2016. 10. 27.
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints, calibration equipment, torque tools test systems and more.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
2016. 2. 12.
Kistler Lorch GmbH Honored for Outstanding Qualities as Employer
2016. 2. 2.
The Kistler Group has overcome currency-related challenges at its Swiss site to achieve continued growth.
2016. 1. 28.
Accurate Wheel Force Measurement with Minimum Configuration Effort
2015. 11. 26.
Increased Flexibility for High-Speed Combustion Analysis
2015. 11. 2.
New Piezoresistive Sensor with Temperature Probe and Integrated Signal Conditioning.
2015. 10. 27.
Kistler Provides Maximum Flexibility for Product Testing and Development
2015. 10. 16.
Kistler's NCFR Joining Module honored in the handling and assembly category
2015. 10. 5.
Setting the Standard for 100% Control of Linear Joining Processes with Partial Rotation
2015. 9. 18.
Kistler Group: safeguarding the firm's competitive edge.
2015. 9. 15.
Quick evaluation of performance and force with Kistler MARS 2.1.
2015. 9. 3.
Major update for Kistler’s mobile engine indication system.
2015. 9. 1.
Setting New Standards in Automated Process Monitoring for Injection Molding.
2015. 8. 25.
Kistler Showcases Three Latest Product Innovations at Motek 2015
2015. 6. 29.
Kistler Automotive GmbH honored as one of Germany's most innovative companies
2015. 6. 26.
Kistler honored with ASCO Award Gold for best corporate transformation in Switzerland.
2015. 6. 26.
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and rehabilitation.
2015. 4. 22.
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
2014. 11. 10.
New product developments for dynamic measuring technology at the Kistler booth at SPS IPC Drives 2014
2014. 10. 14.
Wide range of options for optimizing the quality assurance through documenting and evaluating production data of CoMo Injection Systems
2014. 9. 29.
Users obtain a full range of force–displacement measurement systems from one source
2014. 6. 3.
Extending the maXYmos product range to control and monitor production processes and quality assurance
2014. 5. 26.
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.
2013. 11. 11.
From flexible torque sensors to complete test stands for highly-efficient electric drives
연락처
Cara-Isabell Maercklin
Cara-Isabell Maercklin
Media Contact
연락처