Direct Enforcement: KiTraffic Digital from Kistler defines a new level for Weigh In Motion

Winterthur, December 2019 – With KiTraffic Digital, measurement technology expert Kistler is bringing to market the most accurate Weigh In Motion system yet available. The new system promises an accuracy of up to two percent GVW – independent of almost all external factors, such as driving maneuvers or road conditions. In this way, Kistler has created the conditions for automatically imposing fines for overloaded vehicles.

Weigh In Motion technology is already being used for various purposes – for example, to protect bridges and roads or to collect data for statistics. Sensors in the road surface record the weight of vehicles while driving without impairing the flow of traffic. However, the technology has not so far been capable of capturing overloaded vehicles directly after weighing in the same way as we are used to with speed controls. In the vast majority of countries, ‘direct enforcement’ – i.e. automated recording of vehicle data with subsequent notification of charges – requires vehicles to be weighed using certified, static scales. The authorities also need to be able to rely on the measurement results if, for example, the road quality is sub-optimal or a vehicle drives diagonally across the sensor. At most measuring stations where fines are imposed for overloaded vehicles, Weigh In Motion technology is therefore primarily used for pre-selection. Officers are then subsequently required to verify the measurement result with the aid of a static weighbridge and can only then order the driver to pay a fine.

Multiple individually measuring sensors

With KiTraffic Digital, the Swiss company Kistler has now succeeded in bringing a solution onto the market that significantly improves measurement accuracy and thus enables direct enforcement in accordance with legal requirements. The entirely new sensor incorporates multiple quartz crystals that independently deliver data via a digital interface. The digital measuring signal permits individual calibration of each quartz crystal and prevents signal interference on the transmission path. Working from the measurement signals, sophisticated algorithms calculate the wheel, axle and total weight of each vehicle. Thanks to open standard interfaces, the system can be easily integrated into third-party traffic monitoring systems.

The new digital system also enables other potential sources of error to be ignored. For example, the sensor delivers reliable results even when the vehicle being measured is about to overtake and is driving diagonally over the Weigh In Motion sensor arrangement. At the same time, monitoring can be carried out on any number of lanes. The sensors also provide information on whether a vehicle is equipped with single or dual tires and can draw conclusions about the condition of the tires. The new system automatically records this information without the need for additional hardware. On the contrary, KiTraffic Digital even eliminates the need for the previously necessary induction loops for vehicle detection.

KiTraffic Digital will be presented to the public for the first time in April next year at Intertraffic Amsterdam.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.