ComoNeo from Kistler features new functions and enhanced connectivity

Winterthur, June 2021 – Kistler has added a whole series of new features to its ComoNeo process monitoring system – taking integrated injection molding production to new levels of quality and efficiency. For example: monitoring of the pressure curve in all cavities is now much more precise, with the help of an envelope curve adapted to the process. The ComoNeo 4.1 is WLAN-compatible for the first time, and users will appreciate even more improvements such as additional interfaces and comfortable user management.

For many years now, customers in the plastics processing industry have been able to rely on ComoNeo from Kistler: high-precision cavity pressure monitoring turns injection molding into a transparent process with vastly improved quality and optimum use of resources. Users can choose from a whole series of monitoring and control functions to improve their specific injection molding processes – even including model-based prediction of part quality, assisted by artificial intelligence (ComoNeoPREDICT).

Everything's under control – because the envelope curve is adapted to the process

And now, monitoring of the pressure curves in all cavities is even more accurate: thanks to a new function integrated into ComoNeo 4.1, profiles can be checked for deviations with outstanding precision. This function calculates an "envelope curve" on the basis of any desired number of curves, providing a reference for stable injection molding processes. This is especially helpful when users need to evaluate individual events or even (almost) the entire profile for compliance with critical tolerances – and they can also set the quality criteria manually.

Proactive response to challenges in the medtech sector

ComoNeo 4.1 also includes two new software modules that respond to increased requirements for electronic production records in the medtech industry: With ComoNeoLDAP, ComoNeo can use your company's existing Windows user management – the key to direct, automated management of existing user guidelines. Another innovation is ComoNeoLOG: this feature ensures secure, time-indexed electronic storage of all user activities that involve changing or deleting electronic records – the audit trail, as it is known.

Efficiency boost from wireless communication

To ensure an even more comfortable user experience, ComoNeo from Kistler now includes WLAN functionality: a normal commercial USB stick with Wi-Fi capability is all that's needed to integrate the system into a company's existing network via WLAN. (It should be noted that Kistler only issues hardware recommendations but does not sell the sticks itself.) The benefit: users can now connect the process monitoring system to the production environment via wireless.

To raise connectivity and usability to even higher levels, ComoNeo's user interface (UI) has been expanded in both directions: with the "External UI" function, users can now view external data (such as production data from ComoDataCenter or an MES) on ComoNeo's display. And the ComoNeo UI can also be viewed on the machine control (or elsewhere) via VNC (Virtual Network Computing). This means that customers can now assemble their individual HMI on a variety of devices.

The best ComoNeo of all time – upgrade now!

Improved monitoring capability, simplified and expanded user guidance, and enhanced connectivity: these assets make ComoNeo 4.1 an excellent choice for new customers or as an upgrade for existing customers. The new version also includes many improvements to details such as high maximum resolution for the cavity pressure curves, while tried-and-tested features such as precise measurement of cavity pressure and a wide range of functions for highly advanced injection molding are already part of the ComoNeo standard. A series of benefits that add up to optimum quality assurance and maximum flexibility for every user.

Dossier de press

Portrait de Kistler avec logo pour un aperçu rapide: Kistler Press Kit.zip

2022. 9. 27.
The new SlimLine Sensor 9132CD is nine times more sensitive than comparable SlimLine sensors.
2022. 9. 16.
At K 2022, Kistler will showcase its solutions for injection molding that make plastics processing more intelligent and sustainable.
2022. 9. 6.
With ComoScout, Kistler offers a simple and cost-effective process monitoring system for injection molding processes.
2022. 8. 31.
High-end measurement systems for rolling stock – from brake testing to traffic monitoring.
2022. 8. 22.
Artificial intelligence in punching: AI helps manufacturers improve product quality and step up their quality assurance.
2022. 8. 12.
New wireless dynamometer allows for highly accurate measurements of cutting forces.
2022. 7. 28.
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.