Blechexpo: Kistler showcases automated test systems for quality assurance

Winterthur, October 2019 - Kistler, the measurement technology expert, is presenting a varied range of test systems for punched and series parts as well as joining and forming processes at the Blechexpo in Stuttgart from 5 to 8 November 2019. Visitors to stand 6418 in hall 6 can learn about the benefits of automated process monitoring: improved quality, reduced tool breakages and more efficient production. This year's Blechexpo marks a "first" for Kistler. The company's diverse test automation portfolio includes products from Vester Elektronik GmbH of Straubenhardt, a member of the Kistler Group since mid-2017.

Efficiency is the most critical factor in testing mass-produced parts – closely followed by accuracy. Kistler, the optical measurement technology specialist, offers solutions that score high on both counts – with tangible user benefits from test automation such as high sorting performance, reduced pseudoscrap, and process reliability. Backed by 25 years of advisory expertise and in-depth test automation know-how, Kistler caters to its customers' needs with a comprehensive and varied portfolio of tailor-made solutions from one single source.

High-speed testing and sorting of mass-produced parts

To take just one example: the Shape from Shading process integrated into the high-efficiency KVC 821 sorting system gives users a reliable solution for inspection and control of workpiece surfaces in the µm range. This is a precise method of determining part contours by casting shadows from different illumination angles. The benefit: relevant height deviations in the parts can be accurately differentiated from other deviations (e.g. in color) that have no relevance. With a sorting rate of up to 500 parts per minute, the KVC 821 system quickly and reliably distributes the parts into different containers; faulty parts are separated out completely. On the other hand, pseudoscrap can be reduced and costs can be cut thanks to the process that is integrated into the sorting system.

Another highlight at Kistler's stand: the KVC 621 punched part test cell to measure and inspect complex geometries and grid designs. The Laser Mark KLM 621 laser marking cell codes or marks even the smallest parts at high production speeds of over 1,000 workpieces per minute. A key advantage: all the systems are compatible with hardware from third-party providers.

Boosting quality and preventing tool breakages

The SPP 630 tool monitoring system features a modular structure, so it can be configured to match customers' needs and their existing technology. Depending on requirements, the system delivers information about pressing force and insertion depth, and it can also evaluate structure-borne sound with high precision. The system stores any desired amount of tool data, and the sensors offer exceptionally high resolution: even very small parts with dimensions of less than 0.2 millimeters are captured. Deviations are less than 0.02 millimeters. On request, all the sensors can be equipped with their own cleaning nozzle to ensure that accuracy is unimpaired even under difficult conditions.

Joining modules save energy and cut costs

Kistler offers a complete range of electromechanical joining systems. As compared to hydraulic or pneumatic systems, they offer up to 90 percent more efficiency – and thanks to electronic control, they can be regulated with far greater precision. Kistler is showcasing the NCFE module on its stand at the Blechexpo trade fair. This is an outstandingly cost-efficient solution for simple joining processes in the force range from 10 to 80 kN – so it plays an effective part in permanently reducing overall operating costs.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.