A bridge to digitalization

Winterthur, 15 April 2020 - A flexible new amplifier for today's industrial applications: Kistler introduces the miniature charge amplifier with IO-Link – suitable for use in a wide range of applications including robotics, the packaging industry and the food and beverage sector, as well as being ideal for OEMs. This intelligent amplifier combines analog and digital communication technology to pave the way for Industry 4.0.

Kistler is launching its 5028A charge amplifier – the first device of its type on the market that can use IO-Link technology to output analog signals from piezoelectric sensors as digital measurement data. Benefits for users include highly rigid and dynamic piezoelectric measurement technology, digital data that is resistant to interference from disturbance variables, and end-to-end communication all the way through to sensor level. IO-Link technology supplies users with real-time data to monitor the condition of their plants and measurement chains. This opens the way to predictive maintenance: for example, users can initiate maintenance tasks on a plant if data is regularly outside of the setpoint range. When the IO-Link component is replaced, the new parameters are transferred automatically.

By incorporating a digital interface into the 5028A charge amplifier, Kistler is taking another step towards the fully networked factory in keeping with the goals of Industry 4.0. Users receive reliable data for process evaluation – and they can start work on processing the data immediately. With the 5028A, the raw analog signal is already digitized in the amplifier. The disturbance variables that occur in conventional analog systems due to inductive or capacitive couplings can therefore be avoided from the outset. Likewise, complex and costly individual cabling for analog and control signals is eliminated. However, the 5028A is also suitable for alternative use as an analog charge amplifier with reset/operate input. It delivers proven performance for controlling fast processes with low latency and jitter. Stefan Affeltranger, Product Manager in Kistler's Production Monitoring section, is firmly convinced of the new product's potential: "The 5028A charge amplifier is the world's first amplifier for measurement data from piezoelectric sensors with communication based on IO-Link. This device will fit easily into almost any industrial application that calls for lightweight components and simple solutions."

Standard interfaces ensure flexible use

As well as its extended functional scope, the 5028A charge amplifier offers customers another decisive benefit: the interfaces with the upstream sensor as well as the customer's downstream system are compliant with industrial standards. This means that the charge amplifier can be integrated into any existing network that supports IO-Link. This advantage guarantees easy, cost-efficient installation – and users can be sure that data is transmitted reliably and securely. Kistler is thus taking another step towards the harmonization of proprietary connector types according to commonly used standards. This will make the products easier to use. Even on the smallest of Kistler's amplifiers, customers themselves can now adjust the settings in line with their own requirements. This innovation is Kistler's response to an industry-wide trend: growing demand for more flexible use of components in different systems.

Much valuable space can be saved thanks to the compact dimensions of the 5028A charge amplifier, which can easily be positioned on robot heads or other moving parts. The new device can be used generally in mechanical engineering applications and is also suitable for sectors such as medical technology, because it allows verification of changes to settings at any time. This product's favorable cost-to-benefit ratio underscores the economic advantages of IO-Link technology – an aspect that is also highlighted by the IO-Link Consortium.

Free Webinar on May 14th, 2020 on charge amplifier with IO-Link technology

Dipl. Ing. FH Stefan Affeltranger, Product Manager at Kistler, will present the new charge amplifier with IO-Link technology in a free webinar on Thursday, 14th May 2020 at 10:00 (CET). Participants will get to know the product and the benefits of IO-Link technology, learn for which industrial applications the amplifier is outmost suitable and understand the added value on the way to a Smart Factory.

Click here to register.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
2018. 11. 20.
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
2018. 10. 16.
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 10. 8.
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
2018. 9. 24.
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
2018. 8. 21.
A new Center of Competence for production control and management systems will be opened in Aachen.
2018. 7. 31.
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
2018. 5. 9.
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
2018. 5. 8.
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
2018. 5. 3.
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
2018. 4. 24.
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
2018. 4. 12.
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
2018. 3. 6.
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
2018. 2. 16.
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
2018. 2. 15.
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
2018. 1. 31.
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
2018. 1. 24.
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018. 1. 23.
Overcoming the complexities of RTM – with Kistler
2017. 10. 12.
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
2016. 10. 21.
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
2016. 10. 19.
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016. 10. 10.
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016. 9. 30.
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
2016. 9. 7.
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
2016. 7. 24.
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
2016. 7. 12.
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016. 5. 12.
Screw technology complements the range of applications.
2016. 4. 27.
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.