Cost-efficiency of injection molding, mass production of lightweight components as well as documentation and evaluation of production data are the focus for Internation-al Plastics Fair 2014

Tokyo, 30 September 2014 - At the International Plastics Fair (IPF) from 28 October to 01 November 2014, Kistler is presenting systems which significantly reduce the 'cost of poor quality' (COPQ). In addition, Kistler will showcase fresh innovative sensor technology for reliable mass production of lightweight components for the automotive industry. A new tool for data management and - analysis of injection molding processes will also be shown at Kistler booth.


Maximum Quality Assurance ensures minimum COPQ

Kistler will be presenting the COPQ tool for the first time at IPF 2014, which will help to contrast the 'costs of poor quality ' (COPQ) with the cost of investing in Kistler products. For each project, the tool calculates a Return-on-Investment (ROI) of the Kistler systems. It can be tested at the Kistler stand during the show and will subsequently be available to Kistler customers on its website, free of charge.

Kistler assures 100% quality and zero defect production in all injection molding processes. Kistler sensors and systems can measure and analyze cavity pressure during molding, monitor the process and reduce rejects or separate them immediately upon production. By integrating quality assurance in the actual injection molding process, the costs associated with poor quality can be significantly reduced.

The future of mass production of lightweight components

Reproducible mass production of lightweight structures is a key technology for the future advancement of mobility in various industries – with specific focus on automobile, aeronautical and space technologies. These structural components are manufactured with a thermoplastic or thermosetting matrix in various processes. This includes forming and back injection molding of organic sheets, injection molding (or pressing of long glass fiber-reinforced thermoplastics), as well as resin transfer molding (RTM) and sheet molding compound (SMC). The production of lightweight and composite components place special requirements on process monitoring and quality assurance. The key to these processes is reproducible mass production of molded parts.

For the last forty years, Kistler has been a sought-after partner in the development of new processes and applications with its sensors and systems for measuring and analyzing cavity pressure. With a portfolio of world-leading products, Kistler offers optimum sensor technology for every process, from compact injection molding, to special procedures in injection molding technology, through to RTM.

The new RTM sensor ensures that filling errors and deviations from the optimum process sequence can be identified and also that cascaded filling operations can be managed for large molded parts. As well as measuring pressure, the new sensors facilitate measuring of the vacuum in an evacuated tool. They record all process states and provide an important contribution to increasing process transparency and ensuring molded part quality in the production of lightweight components.

Other pioneering technology at the trade show

Kistler will be presenting its new cavity pressure sensors at IPF 2014. Pioneering innovation in this field, Kistler has developed new sensors with a front diameter of 1 mm and 2.5 mm, which will be available in two variations – with an exchangeable cable and as a cable-less variety. This provides greater flexibility when using these sensors as well as easy repair of damaged cables. In addition, a miniature measurement pin for contact free measuring of cavity pressure is also provided, which can be used in the production of parts with high optical requirements and confined working environments.

The new strain transmitter for electrical injection molding machines is used for simultaneous clamping force measurement and protection. The new mold technology showcases Kistler’s continued evolution of sensors into high-speed injection molding machines and is an example of its commitment to innovation through R&D. Thanks to the particularly sensitive mold protection monitoring, optimum protection for all tool components is guaranteed.

Multi-machine production monitoring and process analysis

Furthermore, Kistler will be showcasing the new CoMo Data Center 2.0 (CDC) for data management and analysis of injection molding processes at IPF 2014. It links all the user's CoMo Injection Systems together, seamlessly combining process- and qualityrelated production data for both live and completed orders in one database. In addition to receiving at-a-glance information about the status of each injection molding machine, users are enabled to monitor their production and analyze processes across multiple machines. For example, they can see which machine is generating particularly good or poor performance values. All data can be accessed through a web browser, even from a mobile device – for complete transparency at any time and from everywhere in the world. As a result, users can meet the growing customer demand for documentation and traceability of production data.

Kistler is presenting its innovations at the International Plastics Fair in Tokyo, Japan from 28 October to 01 November 2014 at Stand 61811 in Hall 4.


Download Press Release (PDF/EN)


Media Contact

Simone Koch
Divisional Marketing Manager IPC
Phone +41 52 2241 802



Image 1: Cavity pressure sensor (Type 6161AA)

Image 2: Cavity pressure sensor (Type 6183C)

Image 3: Longitudinal measuring pin (Type 9239A)

Image 4: CoMo Data Center 2.0

2017. 2. 15.
Discover how Kistler contributes to face the great challenges of our times.
2016. 11. 11.
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis,...
2016. 10. 14.
Reliable measurement solutions are becoming ever more important in the globally networked economy.
2016. 6. 7.
Discover our latest Kistler News online.
2016. 5. 3.
The latest issue of Kistler News is now online.
2016. 2. 1.
Learn more about what motivates us and what we are striving for this year in the latest Kistler View.
2015. 12. 4.
Kistler Japan Celebrates its 30th Anniversary and Thanks Its Loyal Customers.
2015. 10. 15.
NCFR Joining Module Honored at Motek for Best Handling and Assembly
2015. 9. 22.
The latest issue of Kistler News is now online.
2015. 9. 3.
Download KiBox Cockpit V2.1 for free and discover new features.
2015. 8. 20.
Seminar zur Qualitätssicherung in der industriellen Fertigung – jetzt anmelden.
2015. 6. 29.
Kistler Automotive GmbH honored as one of Germany's most innovative companies
2015. 6. 26.
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...
2015. 6. 12.
A fascinating TV report on the trendy sport ‘Parkour’ – with Kistler force plates playing a hidden but...
2015. 4. 22.
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data...
2015. 3. 23.
Kistler partners with OEMs and keeps the finger on the pulse of Industry 4.0
2015. 2. 13.
At SIAF 2015 Kistler will be presenting advanced versions of its proven maXYmos product family
2014. 10. 14.
Wide range of options for optimizing the quality assurance through documenting and evaluating production data...
2014. 9. 29.
Users obtain a full range of force–displacement measurement systems from one source
2014. 9. 24.
At Motek 2014 Kistler will be presenting advanced versions of its proven maXYmos product family
2014. 6. 3.
Extending the maXYmos product range to control and monitor production processes and quality assurance
2014. 5. 26.
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in...
2014. 5. 19.
Users obtain a full range of force–displacement measurement systems from one source
2014. 2. 6.
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with...
2014. 1. 14.
Dr.-Ing. Oliver Schnerr, Head of Sales of the Industrial Process Control (IPC) division, hands over the...
2013. 11. 11.
From flexible torque sensors to complete test stands for highly-efficient electric drives
2013. 9. 16.
1 mm pressure sensor Type 6183C with a new design
2013. 8. 13.
Monitoring, open- and closed-loop control of RTM and SMC processes
2013. 7. 24.
New longitudinal measuring pin for non-contact cavity pressure measuring
2013. 5. 6.
Kistler Goes Beyond Limits: Acceleration sensors for heavy-duty applications at the SENSOR+TEST 2013
2013. 4. 8.
Kistler Goes Beyond Limits: High-tech sensors for heavy-duty applications at the SENSOR+TEST 2013
2013. 3. 20.
In 2012, the Kistler Group reached a record turnover of 279 million Swiss francs with an increase in turnover...
2013. 3. 19.
Kistler Group, a leading global provider of sensors for measuring pressure, force, torque and acceleration,...
2012. 11. 15.
Kistler präsentiert auf der Fachmesse SPS/IPC/DRIVES in Nürnberg (24. bis 26. November 2012) am Stand 4A-451...
2012. 10. 8.
At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012), Kistler will present a...
2012. 10. 8.
At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012) Kistler will present its...
2012. 10. 8.
The new firmware upgrade V2.4 for Kistler's CoMo Injection process monitoring system offers better...
2012. 9. 10.
Kistler Group continues to expand: revenues up 20 %, strengthening of customer-specific development capacities...
2012. 9. 10.
Kistler Gruppe weiterhin auf Expansionskurs: Umsatzsteigerung um 20 %, Stärkung der kundenspezifischen...
2012. 6. 29.
With the acquisition of the DTI Technology ("Digital Transducer Interface") from Hentschel System GmbH,...
2012. 6. 29.
Mit dem Erwerb der DTI-Technologie ("Digital Transducer Interface") von der Hentschel System GmbH, Hannover,...
2012. 5. 8.
At the Automatica Trade Fair, which will take place from 22 through 24 May, 2012 in Munich/Germany, Kistler...
2012. 5. 7.
Kistler sensors and systems deliver an impressive performance where products from other suppliers come to...
2012. 3. 15.
CIRP focuses on cutting because this method of machining components is one of the key production processes.
2012. 2. 17.
In-process quality assurance solutions made by Kistler Group have proven their high efficiency for...
2012. 2. 1.
Despite difficult conditions, with sales growth over 11 % Kistler still achieved a sound result in 2011.
2011. 11. 2.
On Stand 4A-451 in Hall 4A of the SPS/IPC/DRIVES exhibition from 22 to 24 November 2011 in Nuremberg, Kistler...
2011. 11. 2.
By designing a measuring unit and an evaluation unit as separate assemblies, and introducing modular...
2011. 10. 20.
This year's Fakuma sees Kistler showing a system for online prediction of the quality of injection molded...
2011. 10. 19.
Kistler brings the quality-minded injection molder another substantial step closer to zero-defect production.
2011. 9. 28.
As an XY monitor for process monitoring and product testing, the maXYmos BL Type 5867A… from Kistler has...
2011. 9. 28.
Telemetric transmission of the force signal without having to rely on a cable, and suitability for use in...
2011. 9. 28.
Kistler is expanding its selection of electromechanical NC joining modules NCFB Type 2160A… with versions...
2011. 2. 3.
The Kistler Group based in Winterthur, Switzerland, looks back on a successful 2010 financial year with sales...
2010. 12. 10.
Kistler, worldwide supplier of precision sensors, systems and instrumentation for the dynamic measurement of...
2010. 11. 24.
Kistler, worldwide supplier of precision sensors, systems and instrumentation for the dynamic measurement of...
2010. 11. 10.
Kistler's new generation of triaxial PiezoBeam® accelerometer Type 8688A(x) offers best-in-class sensitivity...
2010. 10. 29.
Swiss company Kistler Instrumente AG of Winterthur is the leading international supplier of sensors and...
2010. 9. 10.
The new press force sensor Type 9393A… extends the successful Press Force series of sensors to a measuring...
2010. 9. 6.
With the new combined pressure and temperature sensor Type 6188A… Kistler establishes another milestone in the...
2010. 7. 21.
Kistler has developed its new data acquisition (DAQ) system Type 5697A… for recording data in R&D laboratory...
2010. 7. 9.
Kistler has commissioned an additional calibration unit for torque sensors on its Lorch production site.
2010. 6. 8.
As a development partner of the automobile industry the Kistler Group aims to provide vehicle manufacturers...
2010. 4. 19.
The Kistler Group has been awarded the contract for instrumentation of three crash centers for the Indian...
2010. 4. 7.
In order to optimise processes inside an engine, it is extremely important to have a true picture of the...
2010. 1. 13.
New Type 4520A... Basic Line provides a cost-effective torque sensor based upon strain gage technology.
2009. 12. 10.
The well established Kistler press force sensors are based on the piezoelectric measuring principle.
2009. 11. 18.
Successful automation of joining processes where room is at a premium and joining stations closely spaced...
2009. 10. 23.
The Kistler Group acquired KT Automotive GmbH based in Munich, Germany, in an all-stock transaction on 22...
2009. 9. 14.
The curve of cavity pressure during injection molding is the critical process variable for evaluating part...
2009. 7. 1.
To allow direct incorporation of Kistler products into CAD designs, the Kistler CAD Download Service offers...
2009. 4. 30.
The Kistler Group has acquired Corrsys-Datron Sensorsysteme GmbH based in Wetzlar, Germany, in an all-stock...
2009. 3. 9.
The roll-out of the world's first measuring tram took place in Dresden, Germany, on 5 March with the handover...
2009. 1. 15.
The Kistler Group took over MSC Automotive GmbH based in Schwieberdingen, Germany, in an all-stock transaction...