- GPS-exchange format GPX
- Garmin database files in formats CRS, HST, TCX
- Garmin FIT, a binary format used (for example) by VIRB cameras
- Google KML
- NMEA (National Marine Electronics Association); multiple common datasets are supported
- FAI-IGC, format defined by FAI, specifically designed for gliding competitions
- Other data formats used in the automotive industry (such as MDF4), containing GPS data, etc.
- Photo importer that can export GPS data from the photo metadata
- 적용 분야
- 연구 개발 시험
- 산업 공정 제어
- Modular assembly and testing systems for automation
- Industrial signal conditioning for smart factory
- 산업용 테스트 시스템
- 사출 성형 공정의 공동(cavity) 압력 측정
- 서보 프레스 | 전자기계식 접합 시스템
- 품질 보증을 위한 접합 공정 모니터링
- 품질 보증을 위한 성형 공정 모니터링
- Fastening Technology (볼트 / 너트 분석 장비)
- 측정 기술 – 맞춤형 솔루션
- Medtech(의료 공학) – 제조 품질 보증
- 공정 모니터링을 통한 최적화된 반도체 제조
- 테스트 자동화
- 교통량 솔루션
- 제품
- 서비스
- 채용 정보
- 회사 정보
- 회사
- 역량
- Added value through software: new solutions from sensor to cloud
- Quality assurance for medical technology: what is important?
- Electromechanical joining: making production more cost-effective and transparent
- Optimizing vehicle dynamics: sensors and systems for mobility and motorsport
- Focus on patient's well being: production optimization for medical technology
- Solutions and expertise for spaceflight programs across the globe
- Achieving more with the right measurement technology: practical examples, from aircraft engines to NVH
- The evolution of the piezoelectric measuring chain: added value for industrial manufacturers
- At the forefront of technological development: measurement technology for the 21st century
- Focusing on resource efficiency: monitoring and optimizing large engines with cylinder pressure sensors
- Boost efficiency and conserve resources – intelligent plastics processing with Kistler
- How solutions from Kistler deliver optimized, reliable cutting processes
- Measurement technology generates added value: how Kistler supports vehicle development
- Making sure that if it belongs together, it stays together: fastening technology expertise from Kistler
- Systematic Weigh In Motion: focusing on automated weighing technology
- DTI can do more – and advances towards autonomous driving
- Kistler measurement technology enhances patient safety
- Effective production monitoring and quality assurance with Kistler
- Data acquisition of the next generation
- With piezoelectric measurement to success
- Reliable, safe and efficient vehicle tests – with Kistler
- Plastics technology: advancing towards Industry 4.0
- Electromechanical joining systems: an investment in the future
- On the path to success with efficient vehicle development
- Just in Time Production as Competitive Advantage
- 미디어 및 뉴스
- 행사 및 전시회