New KiRoad Performance

Winterthur, 28 January 2016 – The new KiRoad Performance on-board electronics is a compact, mobile control unit that enables users to configure Kistler RoaDyn® wheel force transducers quickly and reliably. As well as ensuring that measurement data is processed reliably, this unit also supports intuitive wireless operation of wheel force measurement systems on the vehicle and, in future on the test bench.

For over 25 years, Kistler’s wheel force transducers have been setting standards when it comes to measuring vehicle dynamics or durability and tire testing. Now, Kistler is launching the KiRoad Performance: a user-friendly control unit featuring smart configurations and operations that meet todays and future requirements for a flexible wheel force measurement solution.

Fast and Reliable Setup

During system start-up, the KiRoad Performance reads the individual characteristic data for each Kistler RoaDyn® wheel force transducer, automatically detecting the input to which each sensor is connected, ensuring that all sensors are identified and easily parameterized.

Convenient Wireless System Monitoring

The KiCenter software, used by the KiRoad Performance, provides operators with a user-friendly wireless control of all the settings accessible from a mobile device via an intuitive, web-based graphical user interface. The KiRoad Performance and all connected sensors can be controlled from remote, which allows for convenient support and service assistance.

Reliable Signal Processing for Dependable Measurement Data
KiRoad Performance provides the power supply for all RoaDyn® wheel force transducers, and also processes the raw signals from the load cells with crosstalk and lever-arm compensation. The system delivers data in digital and analog form to maximize the accuracy of measurement results.

Jakub Vidner, Kistler's Product Manager for Vehicle Dynamics and Durability, is convinced that measurement of vehicle dynamics as well as durability and tire tests will become far easier and more reliable with this new product: ‘The intuitive configuration and flexible interfaces of the compact KiRoad Performance meet all the requirements for a user-friendly, high-precision measuring platform that can deliver state-of-the-art wheel force measurements.’

Flexible for Use in Confined Spaces
The compact design (199 x 182 x 127 mm) makes the KiRoad Performance easy to install in the vehicle, even when space is at a premium. This cost-efficient solution offers flexible scalability and supports measurements from one to four RoaDyn® wheel force transducers, allowing wheel force transducers to be added or removed at any time. It is also possible to cascade several KiRoad Performance units synchronously. Multiple digital and analog interfaces are provided, offering flexible options for data output, ensuring maximum compatibility with existing systems. Extra analog sensor inputs are provided (two channels per wheel force transducer) enabling users to connect additional sensors (e.g. angle correction sensors or accelerometers) to allow synchronous recording of additional data.

For more information, visit: www.kistler.com/kiroad-performance

Download Press Release (PDF)

Contact for Users

Jakub Vidner
Product Manager Vehicle Dynamics and Durability
Tel.: +49 7031 41 817 820
Email: jakub.vidner@kistler.com

Media Contact

Lisa Glatz
Divisional Marketing Manager ART
Tel.: +41 52 224 12 31
Email: lisa.glatz@kistler.com

プレスキット

キスラー会社概要:キスラープレスキット

2018/05/09
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data...
2018/05/08
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its...
2018/05/03
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process...
2018/04/24
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality...
2018/04/12
The global leader in dynamic measurement technology supports the passion for innovation and technology with a...
2018/03/06
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the...
2018/02/16
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
2018/01/24
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018/01/23
Overcoming the complexities of RTM – with Kistler
2018/01/06
キスラー社の新しいスプリントシステム(KiSprint)は、競技条件下でのスタートダッシュを生体力学的に最適化する効率的な手段をトレーナーとアスリートに提供します。堅牢な可動式システムでは、ソフトウェアによる総合的な評価...
2017/10/12
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
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
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
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
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
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
2016/10/27
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
2016/10/21
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
2016/10/19
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016/10/10
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016/09/30
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
2016/09/07
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
2016/07/24
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
2016/07/12
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016/05/12
Screw technology complements the range of applications.
2016/04/27
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...