Kistler's Signal Conditioning Platform: Now on the Network

Winterthur, 26 November 2015 – Kistler is launching a new and improved Signal Conditioning Platform (SCP) that ensures process reliability and enables early detection of unsafe operating conditions in fixed or mobile combustion analysis applications.

For over 50 years, Kistler's innovative solutions for high-precision combustion analysis have ensured the firm's leading position in the global market. With new Ethernet options and an improved software interface, Kistler’s new SCP for high-speed combustion analysis centralizes equipment configuration and optimizes usability for maximum flexibility.

Flexible System with Centralized Control
Kistler’s network-compatible SCP can be equipped with application-specific measuring modules to accomplish various measuring tasks. The new platform allows virtual linkage of the systems deployed, so all SCPs can be operated from one centrally controlled PC. Thomas Kley, Kistler's Product Manager in the Engine R&D Strategic Business Field, emphasizes the high flexibility and usability of this newly developed product: ‘A host of user-friendly functions position the new SCP on the market as a powerfully attractive combustion analysis system.’

Intuitive GUI for Simple and Quick Data Handling
The SCP’s GUI provides an overview of all key data, such as measuring module configurations, sensor data and operating times, so that all changes can be made on a single screen. An ‘Export’ function converts the data into various formats to document all the measurement settings. Cylinder peak pressure histograms for each sensor can be created at the click of a button while users can immediately detect sensor load and strain, as well as any irregularities.

Real-Time Monitoring for Early Detection of Unsafe Operating Conditions
A CAN bus interface allows for the digital capture and real-time monitoring of cylinder peak pressures in addition to the operating temperature of low pressure piezoresistive sensors. This data allows users to immediately recognize engine or equipment damaging events and take corrective action, thereby avoiding unsafe operating conditions.

Kistler PiezoSmart® Sensors Ensure Process Reliability
PiezoSmart® guarantees the correct allocation of sensor data as errors caused by manual data handling can be eliminated and preparation effort is reduced to the minimum. PiezoSmart® allows historical monitoring and an assessment of an existing sensor portfolio.

Two versions of Kistler's new SCP are available. The Type 2853B model (8 slots or 16 channels) is suitable for engine indication on the test bench. SCP Slim Type 2852B (with 2 slots or 4 channels) is suitable for both mobile and test bench applications. For existing SCPs (Kistler Type 2853A), Kistler offers Type 5615BFK and 5615BRK Upgrade Kits for retrofit.

For an overview of all supported measurands and additional product information, visit our product page at www.kistler.com/scp.

Download Press Release (PDF)

User Contact
Thomas Kley
Product Manager Engine R&D
Phone +41 52 2241 364
Email: thomas.kley@kistler.com

Media Contact
Lisa Glatz
Divisional Marketing Manager ART
Phone +41 52 224 12 31
Email: lisa.glatz@kistler.com

プレスキット

キスラー会社概要:キスラープレスキット

2018/04/12
The global leader in dynamic measurement technology supports the passion for innovation and technology with a...
2018/03/06
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the...
2018/02/16
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM)...
2018/01/24
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
2018/01/23
Overcoming the complexities of RTM – with Kistler
2018/01/06
キスラー社の新しいスプリントシステム(KiSprint)は、競技条件下でのスタートダッシュを生体力学的に最適化する効率的な手段をトレーナーとアスリートに提供します。堅牢な可動式システムでは、ソフトウェアによる総合的な評価...
2017/10/12
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a...
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
Kistler Group took over near Karlsruhe-based Vester Elektronik GmbH on 25 August, a specialist in sensor...
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
At Moulding Expo 2017, we will show how easy it is to install the measurement technology needed for quality...
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
2016/10/27
At this year's SPS IPC Drives in Nuremberg Kistler will premiere laboratory systems to analyze bolted joints,...
2016/10/21
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and...
2016/10/19
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
2016/10/10
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
2016/09/30
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore...
2016/09/07
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new...
2016/07/24
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of...
2016/07/12
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
2016/05/12
Screw technology complements the range of applications.
2016/04/27
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home...