Kistler is setting new standards for electromechanical NC joining systems with the maXYmos NC

Munich, 3 June 2014 – At Automatica 2014 from 3-6 June, Kistler will be showcasing a new joining system comprising maXYmos NC, the IndraDrive servo amplifier and established and proven NC joining modules. The newly developed maXYmos NC monitors and controls the joining process. Equipped with an intuitive touch display, the new system is particularly easy to use, while the integrated sequence control offers a high level of flexibility for straightforward to highly complex joining processes.


Process control made easy
The XY monitors from Kistler's maXYmos series enable customers to visualize and evaluate production processes – allowing them to operate in a consistent, process-integrated manner and to maximize quality assurance. In doing so, they monitor XY curves, where two measured variables must be in a certain relation to each other. Force-displacement curves are a good example of this, which arise from bearings being press-fitted. A further development to the maXYmos product range, the maXYmos NC (Numeric Control) enables NC joining systems to now also be monitored and controlled. Such NC joining systems are predominantly used in the automotive and supply industry in the widest range of manufacturing processes, such as gearbox, motor, chassis or pump installation. The maXYmos NC evaluates and documents the XY curves of joining and press-fitting operations in combination with NC joining modules and the associated IndraDrive servo amplifier. Due to the form of measurement curves, each stage of the production and assembly line – and even the entire product – can be monitored and operated via SERCOS III all in real time. In this way, optimum cycle times can be achieved with the highest degree of repeat accuracy. Unplanned downtimes are minimized as machine availability increases, in turn allowing the productivity of the manufacturing process to be accelerated.


Increased flexibility for users
The integrated sequence control (Sequencer Mode) enables processes to be illustrated without the need for expensive, external PLC programming. Indeed, the programs are set up in a swift, straightforward manner using the intuitive user interface of the touch display. In total, up to 128 programs can be stored, with the option of defining each one with an independent sequence of up to 255 elements. As a result, even highly complex processes can be illustrated simply and effectively. Such processes are evaluated by means of the curve patterns of two measured variables in relation to one another, which are then rated as good (OK) or bad (NOK). For that purpose, ten evaluation objectives are available in each program. Process deviations are reliably detected, while complex process sequences are regulated and controlled. Moreover, the new Multi-View function can be used to simultaneously visualize and compare various processes on the same monitor.


Easily integrated and intuitively operated
The flexible housing concept of maXYmos monitors allows easy integration into existing or newly developed systems. The maXYmos NC comprises two components, the measuring and evaluation module (MEM) and the display module (DIM). These two components can either be installed separately or as a compact unit. Moreover, up to eight joining processes can be visualized on the same display. As such, this guarantees maximum flexibility during installation, whilst saving space and contributing towards an optimum cost-benefit ratio. Furthermore, the measuring and evaluation module (MEM) ticks all the boxes in terms of its variety of interfaces. The most common interfaces such as PROFIBUS, PROFINET, EtherNet/IP and EtherCAT are integrated and can be selected via a menu on the touch display. This allows users to respond to changing requirements in relation to sensor or fieldbus types. In addition, the standardization of MEM development keeps costs for spare part handling to a minimum.


Kistler is presenting the maXYmos NC at Automatica in Munich, Germany from 3-6 June 2014 at stand 425, hall A6.

Press Release (PDF/EN)

Media Contact
Simone Koch Divisional Marketing Manager IPC
Phone: +41 52 2241 802
E-Mail: simone.koch@kistler.com

 

Captions
Image 1: The uniform operating philosophy of the maXYmos product range offers users an intuitive and easy-to-use system. This supports straightforward, swift startup of electromechanical NC joining systems.

Image 2: The measuring and evaluation module (MEM) ticks all the boxes in terms of its variety of interfaces. All the standard interfaces are continuously available, ensuring flexibility in the event that the requirements placed on sensor or fieldbus types change, as well as offering considerable advantages in terms of spare parts stocking.

Image 3: The maXYmos NC controls the NC joining module via the servo amplifier through the integrated sequence control. An independent sequence can be defined for each of the 128 programs.

2017/10/16
型内圧モニタシステムComoNeoとインダストリ4.0への取り組みをご紹介します
2017/06/21
2017年 7月 21日(金)に愛知県産業労働センター(ウインクあいち)にて「切削加工技術セミナー2017」を開催します。
2017/02/15
Discover how Kistler contributes to face the great challenges of our times.
2016/12/13
2017年1月7日から9日の日程で、本社を東京都港区から新横浜へ移転することになりました。
2016/11/11
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis,...
2016/10/14
Reliable measurement solutions are becoming ever more important in the globally networked economy.
2016/06/07
Discover our latest Kistler News online.
2016/05/03
The latest issue of Kistler News is now online.
2016/02/01
Learn more about what motivates us and what we are striving for this year in the latest Kistler View.
2015/12/04
日本キスラー株式会社は2015年12月4日をもちまして、創立30周年を迎えることとなりました。これもひとえに皆様のご支援の賜物と心より感謝いたしております。この節目に際しまして、ウェブサイトも刷新し、より皆様のご期待に応...
2015/10/15
NCFR Joining Module Honored at Motek for Best Handling and Assembly
2015/09/22
The latest issue of Kistler News is now online.
2015/09/03
Download KiBox Cockpit V2.1 for free and discover new features.
2015/08/20
Seminar zur Qualitätssicherung in der industriellen Fertigung – jetzt anmelden.
2015/06/29
Kistler Automotive GmbH honored as one of Germany's most innovative companies
2015/06/26
Kistler's software for force plates offers a host of new features for performance diagnostics in sports and...
2015/06/12
A fascinating TV report on the trendy sport ‘Parkour’ – with Kistler force plates playing a hidden but...
2015/04/22
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data...
2015/03/23
Kistler partners with OEMs and keeps the finger on the pulse of Industry 4.0
2015/02/13
At SIAF 2015 Kistler will be presenting advanced versions of its proven maXYmos product family
2014/10/14
Wide range of options for optimizing the quality assurance through documenting and evaluating production data...
2014/09/29
Users obtain a full range of force–displacement measurement systems from one source
2014/09/24
At Motek 2014 Kistler will be presenting advanced versions of its proven maXYmos product family
2014/06/03
Extending the maXYmos product range to control and monitor production processes and quality assurance
2014/05/26
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in...
2014/05/19
Users obtain a full range of force–displacement measurement systems from one source
2014/02/06
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with...
2014/01/14
Dr.-Ing. Oliver Schnerr, Head of Sales of the Industrial Process Control (IPC) division, hands over the...
2013/11/11
From flexible torque sensors to complete test stands for highly-efficient electric drives
2013/09/16
1 mm pressure sensor Type 6183C with a new design
2013/08/13
Monitoring, open- and closed-loop control of RTM and SMC processes
2013/07/24
New longitudinal measuring pin for non-contact cavity pressure measuring
2013/05/06
Kistler Goes Beyond Limits: Acceleration sensors for heavy-duty applications at the SENSOR+TEST 2013
2013/04/08
Kistler Goes Beyond Limits: High-tech sensors for heavy-duty applications at the SENSOR+TEST 2013
2013/03/20
In 2012, the Kistler Group reached a record turnover of 279 million Swiss francs with an increase in turnover...
2013/03/19
Kistler Group, a leading global provider of sensors for measuring pressure, force, torque and acceleration,...
2012/11/15
Kistler präsentiert auf der Fachmesse SPS/IPC/DRIVES in Nürnberg (24. bis 26. November 2012) am Stand 4A-451...
2012/10/08
At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012), Kistler will present a...
2012/10/08
At the Fakuma trade show in Friedrichshafen/Germany (from 16 until 20 October, 2012) Kistler will present its...
2012/10/08
The new firmware upgrade V2.4 for Kistler's CoMo Injection process monitoring system offers better...
2012/09/10
Kistler Group continues to expand: revenues up 20 %, strengthening of customer-specific development capacities...
2012/09/10
Kistler Gruppe weiterhin auf Expansionskurs: Umsatzsteigerung um 20 %, Stärkung der kundenspezifischen...
2012/06/29
With the acquisition of the DTI Technology ("Digital Transducer Interface") from Hentschel System GmbH,...
2012/06/29
Mit dem Erwerb der DTI-Technologie ("Digital Transducer Interface") von der Hentschel System GmbH, Hannover,...
2012/05/08
At the Automatica Trade Fair, which will take place from 22 through 24 May, 2012 in Munich/Germany, Kistler...
2012/05/07
Kistler sensors and systems deliver an impressive performance where products from other suppliers come to...
2012/03/15
CIRP focuses on cutting because this method of machining components is one of the key production processes.
2012/02/17
In-process quality assurance solutions made by Kistler Group have proven their high efficiency for...
2012/02/01
Despite difficult conditions, with sales growth over 11 % Kistler still achieved a sound result in 2011.
2011/11/02
On Stand 4A-451 in Hall 4A of the SPS/IPC/DRIVES exhibition from 22 to 24 November 2011 in Nuremberg, Kistler...
2011/11/02
By designing a measuring unit and an evaluation unit as separate assemblies, and introducing modular...
2011/10/20
This year's Fakuma sees Kistler showing a system for online prediction of the quality of injection molded...
2011/10/19
Kistler brings the quality-minded injection molder another substantial step closer to zero-defect production.
2011/09/28
As an XY monitor for process monitoring and product testing, the maXYmos BL Type 5867A… from Kistler has...
2011/09/28
Telemetric transmission of the force signal without having to rely on a cable, and suitability for use in...
2011/09/28
Kistler is expanding its selection of electromechanical NC joining modules NCFB Type 2160A… with versions...
2011/02/03
The Kistler Group based in Winterthur, Switzerland, looks back on a successful 2010 financial year with sales...
2010/12/10
Kistler, worldwide supplier of precision sensors, systems and instrumentation for the dynamic measurement of...
2010/11/24
Kistler, worldwide supplier of precision sensors, systems and instrumentation for the dynamic measurement of...
2010/11/10
Kistler's new generation of triaxial PiezoBeam® accelerometer Type 8688A(x) offers best-in-class sensitivity...
2010/10/29
Swiss company Kistler Instrumente AG of Winterthur is the leading international supplier of sensors and...
2010/09/10
The new press force sensor Type 9393A… extends the successful Press Force series of sensors to a measuring...
2010/09/06
With the new combined pressure and temperature sensor Type 6188A… Kistler establishes another milestone in the...
2010/07/21
Kistler has developed its new data acquisition (DAQ) system Type 5697A… for recording data in R&D laboratory...
2010/07/09
Kistler has commissioned an additional calibration unit for torque sensors on its Lorch production site.
2010/06/08
As a development partner of the automobile industry the Kistler Group aims to provide vehicle manufacturers...
2010/04/19
The Kistler Group has been awarded the contract for instrumentation of three crash centers for the Indian...
2010/04/07
In order to optimise processes inside an engine, it is extremely important to have a true picture of the...
2010/01/13
New Type 4520A... Basic Line provides a cost-effective torque sensor based upon strain gage technology.
2009/12/10
The well established Kistler press force sensors are based on the piezoelectric measuring principle.
2009/11/18
Successful automation of joining processes where room is at a premium and joining stations closely spaced...
2009/10/23
The Kistler Group acquired KT Automotive GmbH based in Munich, Germany, in an all-stock transaction on 22...
2009/09/14
The curve of cavity pressure during injection molding is the critical process variable for evaluating part...
2009/07/01
To allow direct incorporation of Kistler products into CAD designs, the Kistler CAD Download Service offers...
2009/04/30
The Kistler Group has acquired Corrsys-Datron Sensorsysteme GmbH based in Wetzlar, Germany, in an all-stock...
2009/03/09
The roll-out of the world's first measuring tram took place in Dresden, Germany, on 5 March with the handover...
2009/01/15
The Kistler Group took over MSC Automotive GmbH based in Schwieberdingen, Germany, in an all-stock transaction...