The dimensions are exactly right

A renowned German manufacturer of small electrical appliances puts its trust in automatic testing and sorting systems by Vester, a Kistler Group company. This manufacturer tests several million plastic parts every year to ensure the quality of its electric shavers and epilators  - thus guaranteeing the brand's success. The company has carved out a reputation for itself through the design of its products, and has earned a significant place in the history of industrial design. The brand is now included in the portfolio of a leading U.S. consumer goods corporation.

Virtually no complaints

Electric shavers are complex products that can consist of 200 to 300 highly intricate individual parts, depending on the type. To ensure that quality is the defining aspect of the customer experience, every one of these parts has to be perfect. Thanks to automatic testing and sorting systems by Vester, the company can guarantee that the parts in its end products meet very high quality and functionality standards. Comprehensive quality monitoring during and after the production process has significantly reduced the internal complaint rate. End-to-end quality monitoring has had an equally positive impact on warranty cases: here too, the rate has fallen substantially.

Precision  - even with high throughput rates

Three Vester automatic testing and sorting systems are currently operating on the company's plastic production lines, and a feasibility study for a fourth unit is already in progress. Eight more Vester systems are installed in the automated turning shop. To ensure excellent product performance, these systems test numerous items including outsourced metal parts such as the pins built into shaver heads and electric toothbrushes.

The testing rates and speeds required for plastic part production are exceptionally high. Correct positioning of individual parts as they are fed into the test line is essential to guarantee the necessary precision and to ensure high throughput rates. The aim here is to exclude parallax errors that occur because the camera's angle of view is distorted.

Our testing systems meet the demanding requirements regarding the complex geometry and high volumes. They helped to improve the quality of each individual part as well as of the complete device. Therefore, the customer owns an efficient solution."

Samuel Ganzhorn, Application Specialist

 

Systems for universal use

At present, several million plastic parts are tested and automatically sorted in the plant each year. Two VVC 120 systems (based on the inclined-plane principle) and one VVC 811 system (with a continuously rotating glass plate) supply answers to questions such as these: Are the parts deformed? Is there any flash formation? Do dimensions adequately meet the specification? Testing focuses on particularly critical parts that are crucial for function and performance.

This electrical appliance manufacturer sees two factors as decisive: the flexibility of Vester's systems, and their high performance. With a suitable setup, multiple features can be tested on one part. But that is not all: different components can also be tested on one system with minimum effort. Customers benefit from Vester's support with application changes: they can choose to have their camera and feed systems reconfigured on their own site or, for major conversions and retrofits, the work can be carried out at Vester's plant.

Thanks to its close collaboration with Vester, the manufacturer is able to meet the demanding requirements set by its parent company. Standard automatic testing systems always need to be adapted for each and every application, so their suitability for testing highly intricate plastic parts is limited. Vester's solutions take account of complex geometry, advanced testing requirements and high volumes: as well as boosting cost efficiency, they help to enhance product quality. The successful results of quality assurance with test automation by Vester are clear: models from this high-quality German manufacturer regularly occupy the top places in independent consumer tests.

Test results: the basis for process optimization

This manufacturer of shavers and epilators can look back on many years' successful experience of using Vester's automated test systems for metal parts. Vester continuously develops its solutions, with the focus on individual customer requirements. For this customer, inhouse testing is another advantage that should not be underestimated. Because users acquire know-how about specific repeated deviations on the spot, they can draw conclusions about the injection molding process and initiate steps to optimize it. With the help of Vester's systems, the customer can (for example) easily check which cavity was used for a defective part. By reading out the relevant identification code, users can track down the specific problem points in the process.

High-performance process monitoring is a critical factor in ongoing optimization and automation: it ensures that products such as shavers and epilators will convince and inspire end customers, now and in the future  - and the manufacturer can continue to predict lifetimes of up to seven years. By partnering with Vester, this customer gains access to technologically mature solutions that deliver highly efficient quality testing for plastic and metal parts. Vester thus plays a key part in delivering a customer experience that will stand the test of time.

2022/05/04
Daimler Buses relies on MaDaM and jBEAM to further develop of its electric city buses.
2022/04/11
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
2022/01/14
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
2021/11/18
自動車業界や風力タービン業界において信頼性の高い亜鉛フレークコーティングを実現する、ANALYSEシステムによる高度な締結部品試験
2021/10/12
China VIに適合したエンジン生産のために、どのようにしてユチャイは精度、透明性、資源効率の改善をなし遂げたのか
2021/09/14
動力計、研究用チャージアンプおよびソフトウェアによる高精度な測定チェーンにより、客観的な比較試験が可能
2021/09/09
バレンシアのエストゥディオ・デ・ラ・ピサダの足病学エキスパートは、3Dフォースプレートを使って患者とアスリートのための治療法や装具を開発しています
2021/09/09
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
2021/07/02
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
2021/06/25
動力計で擾乱を正確に捉えることにより、人工衛星の開発技術を向上
2021/06/02
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
2021/04/26
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
2021/04/13
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
2021/03/22
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
2021/02/08
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
2020/10/05
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
2020/09/18
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
2020/08/20
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
2020/07/22
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
2020/06/09
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
2019/11/15
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
2019/10/23
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
2019/08/15
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
2019/07/17
Turkey opts for weight enforcement with WIM technology from Kistler
2019/06/24
For the next manned flight to the moon: safety that can be measured
2019/06/20
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
2019/05/14
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
2019/04/18
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
2019/04/02
NFL's Jaguars boost their fitness levels with Kistler.
2019/03/25
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
2019/03/18
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
2018/12/17
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
2018/11/27
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
2018/10/10
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
2018/10/08
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
2018/08/31
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
2018/08/14
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
2018/07/16
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
2018/04/11
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
2017/11/14
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
2017/08/11
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
2017/01/04
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
2016/12/22
Kistler makes progress in vehicle development possible
2016/12/22
Kistler Sensor Correvit® SFII measures world record
2016/12/20
Kistler sensors deliver a maximum in data quality under any conditions.
2016/11/07
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
2016/10/05
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
2016/08/17
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2016/02/19
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
2015/11/04
Piezoelectric Measurements with CompactRIO™
2015/06/15
Measurement Solutions for Automotive Test Systems
2015/05/08
Quality Assurance in the Automotive Industry
2015/03/02
How Brose improves the quality of its two-component production and automatically separates defective parts
2014/12/02
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
2014/12/02
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
2011/08/23
HEWI and its Customers Benefit from Cavity Pressure Technology
2011/02/15
End-to-end process monitoring for critical medical moldings
2011/02/07
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
お問合せ
Max 25 MB