Schurter backs on Kistler's process monitoring for highly automated electronics production

Swiss electronics manufacturer Schurter AG has to meet the demanding standards set by the automotive industry, so 100% control and traceability are essential requirements in its production process. Schurter's new fully automated plant to produce complex safety-critical parts incorporates four Kistler systems for process monitoring – including fast cycle times, automatic sorting and measuring instrument capability testing.

Schurter, the Lucerne-based Swiss electronics manufacturer, has ambitious plans for the future: with a workforce that already numbers over 2 000, 11 production facilities and companies in 17 countries, the stage is clearly set for growth to continue. Acquisitions are generating added impetus; turnover already amounted to CHF 259 million in 2017, and the trend is upwards. Schurter's portfolio has two cornerstones: electric/electronic components (connectors, switches and circuit breakers, etc.), and input systems such as HMIs, touch panels and membrane keypads. Recent years have seen the addition of custom solutions based on a high level of vertical integration: these are grouped together in the firm's Solutions division.

As the trend towards electromobility gathers pace, electric fuses are now taking on a key role – especially in the production of batteries for electric automobiles. Each battery cell requires individual fuse protection, so the total number of fuses in a vehicle can quickly reach four or five hundred. In 2017, an end customer in the automotive sector commissioned Schurter to produce large quantities of fuses for use in safety-critical areas. André Schürmann, Head of Automation & Maintenance at Schurter, explains the background: "We can draw on many years of experience in automating fuse production processes. And thanks to our technological edge, we're still able to carry out the development work here in Switzerland, as well as some of the production. That's something our customers really appreciate." The fuses consist of numerous small parts; large quantities have to be manufactured with maximum automation, in compliance with the standards and of course with high quality. To meet these exceptional challenges, Schurter invited a near neighbor to come on board: special-purpose machinery manufacturer ROBO • MAT AG. "ROBO • MAT presented us with a very detailed offer for the development of the plant, including a 3D layout and exact pricing. Combined with their physical proximity and the close working relationship that developed from day one, this added up to a highly convincing complete package," Schürmann recalls

High-precision testing in seconds

Markus Zimmermann, owner and CEO of ROBO • MAT, explains the project: "Two fuse variants are produced on this plant, at rates of about 3 000 parts per hour and with a cycle time of 2.7 seconds. The product passes through 16 different stations in that brief period of time. Designing the plant faced us with the challenge of coordinating the process steps so as to achieve the short cycle time. The beauty of it was that Schurter hadn't yet finalized the fuse design when we started work. This meant that special requirements could still be incorporated into the design. Of course, that's only possible if you're close enough to the customer," Zimmermann stresses.

The process monitoring systems from Kistler were chosen to meet the demanding requirements for traceability and quality in the automotive industry. A total of four Type 9217A piezoelectric small force sensors are deployed in the new plant, together with the matching maXYmos BL evaluation systems.

As well as our favorable experience in the past, the main factors that persuaded us to opt for Kistler were the small force range and the very low response threshold."

Markus Zimmermann, owner and CEO of ROBO • MAT AG

Markus Zimmermann, owner and CEO of ROBO • MAT AG

 

The measured key variables are recorded and visualized during the process; in addition, the defined criteria are used for automatic in-process segregation of good and bad parts. Testing includes the spring force as well as the force applied to position the covers on the fuses. The sensors themselves are also tested: "What's really special about this plant is that the measurement equipment itself is cross-checked during the actual process. The sensor technology is measured about once in every 100 parts – to verify whether the sensors are still capturing the data that they should," Zimmermann continues. "This development is driven by requirements in the automotive industry. According to the International Automotive Task Force's standard IATF 16949 for safety-critical parts, the capability of the measuring equipment has to be verified regularly during the production process. The end customer specifically audited this particular point here in our plant," Schürmann adds.

An unprecedented level of quality data acquisition was attained in response to this combination of demanding customer specifications, compliance with the standard and a highly complex plant: "For each fuse, 76 specific datasets are captured and stored in one central database – as well as force and displacement, the data covers many other variables such as furnace and air temperature. This is the most extensive acquisition of quality data that we have ever implemented on one plant," Zimmermann points out. Schurter and ROBO • MAT have thus met all the specified requirements for quality assurance and documentation, so now they can focus on optimizing the operation of the plant.

Intuitive measurement technology generates added value

There is still some way to go before series production can finally begin. Acceptance was already obtained from the end customer after about a year of development work, but that is not the same as the 24/7 volume production targeted by Schurter. Phase two is therefore focusing on intensive testing and optimization of critical factors such as materials, plant settings and other parameters. "The measurement technology didn't need very much effort because the systems can be operated intuitively," Schürmann notes. "We've already used Kistler products in the past, so we know we can rely on performance, service and value for money," Zimmermann adds. "But other parts of the plant are so complex that commissioning and optimization involve a substantial workload. The advantage is that once the target has been attained, the settings are transferred directly to a second plant so we can cover the planned high quantities," Zimmermann continues. maXYmos and the rest of the process monitoring technology from Kistler will be on board again at that stage, with double testing to ensure that the fuses keep their promises.

Zimmermann concludes: "We appreciate the excellent collaboration, the professional support and Kistler's close relationships with its customers – and we shall be glad to choose Kistler again in the future." Schürmann sketches out the prospects for the future: "Plants will have to become more and more intelligent to meet the challenges posed by e-mobility and Industry 4.0. Condition monitoring, predictive maintenance and batch-level traceability are increasingly becoming part of the standard. This calls for measurement technology that can be integrated easily and operated intuitively – and it has to deliver precise and reliable results. In-process quality monitoring definitely generates added productive value, which is why growing numbers of industrial manufacturers are integrating it into their production."

2022/05/04
Daimler Buses relies on MaDaM and jBEAM to further develop of its electric city buses.
2022/04/11
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
2022/01/14
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
2021/11/18
自動車業界や風力タービン業界において信頼性の高い亜鉛フレークコーティングを実現する、ANALYSEシステムによる高度な締結部品試験
2021/10/12
China VIに適合したエンジン生産のために、どのようにしてユチャイは精度、透明性、資源効率の改善をなし遂げたのか
2021/09/14
動力計、研究用チャージアンプおよびソフトウェアによる高精度な測定チェーンにより、客観的な比較試験が可能
2021/09/09
バレンシアのエストゥディオ・デ・ラ・ピサダの足病学エキスパートは、3Dフォースプレートを使って患者とアスリートのための治療法や装具を開発しています
2021/09/09
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
2021/07/02
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
2021/06/25
動力計で擾乱を正確に捉えることにより、人工衛星の開発技術を向上
2021/06/02
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
2021/04/26
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
2021/04/13
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
2021/03/22
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
2021/02/08
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
2020/10/05
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
2020/09/18
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
2020/08/20
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
2020/07/22
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
2020/06/09
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
2019/11/15
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
2019/10/23
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
2019/08/15
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
2019/07/17
Turkey opts for weight enforcement with WIM technology from Kistler
2019/06/24
For the next manned flight to the moon: safety that can be measured
2019/06/20
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
2019/05/14
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
2019/04/18
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
2019/04/02
NFL's Jaguars boost their fitness levels with Kistler.
2019/03/25
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
2019/03/18
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
2018/12/17
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
2018/11/27
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
2018/10/10
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
2018/10/08
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
2018/08/31
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
2018/08/14
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
2018/07/16
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
2018/04/11
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
2017/11/14
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
2017/08/11
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
2017/01/04
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
2016/12/22
Kistler makes progress in vehicle development possible
2016/12/22
Kistler Sensor Correvit® SFII measures world record
2016/12/20
Kistler sensors deliver a maximum in data quality under any conditions.
2016/11/07
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
2016/10/05
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
2016/08/17
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2016/02/19
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
2015/11/04
Piezoelectric Measurements with CompactRIO™
2015/06/15
Measurement Solutions for Automotive Test Systems
2015/05/08
Quality Assurance in the Automotive Industry
2015/03/02
How Brose improves the quality of its two-component production and automatically separates defective parts
2014/12/02
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
2014/12/02
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
2011/08/23
HEWI and its Customers Benefit from Cavity Pressure Technology
2011/02/15
End-to-end process monitoring for critical medical moldings
2011/02/07
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
お問合せ
Max 25 MB