In the Pole Position with Precision Sensors from Kistler

Modern motorsport vehicles and drivers operate at the absolute limit. Every bit of potential is drawn from core components, such as motors and chassis. To ensure that all individual parts function properly, access to exact measurement data is essential. The lightweight, compact, and long-lasting Kistler onboard sensors are, therefore, the perfect solution for use in motorsport.

Continuous optimization as a challenge

In modern motorsport, details are decisive for victory or defeat. The conditions are hard and demanding. The cars must meet high standards. To detect possible defects at an early stage and thereby be able to continuously optimize the performance, it is essential that high-precision measurement data be accessible at all times.

High-precision sensors for maximum data quality

Motorsport vehicles are constantly pushed to the limit. In these areas, it is a challenge to achieve reliable measurements. Not only do the sensors need to be extremely durable, they must also measure with high precision in the extreme range and, at the same time, be small enough to be installed in restricted spaces. Only in this way is it possible to achieve maximum data quality at all times and under all external influences.

Best performance with Kistler technology

Kistler offers innovative solutions for these application areas. With the durable, high-precision, and space-saving onboard sensors, problems can be detected early on and the motor performance thereby maximized. At the same time, monitoring systems from Kistler ensure continuous control and documentation of the dynamic processes. The sensors and systems supply the race teams with reliable, real-time data that allows them to keep an eye on the performance of the race cars and to make the necessary decisions that can be the difference between victory and defeat. This ensures that the race teams themselves can further optimize race performance at the highest level. You can find more information at our Motorsport pages.

Our highly qualified employees push the limits of what is possible and deliver answers with our customers – and for our customers – to the great questions posed by a connected world around the megatrends mobility, emission reduction, quality control and lightweight construction.
Do you want to play a part in shaping the future? If so, become part of our team.

2018/08/31
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
2018/08/14
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
2018/07/20
Enhanced safety for patients thanks to process monitoring during injection molding
2018/07/16
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
2018/04/11
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
2017/11/14
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
2017/08/11
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
2017/01/04
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
2016/12/22
Kistler makes progress in vehicle development possible
2016/12/22
Kistler Sensor Correvit® SFII measures world record
2016/12/20
Kistler sensors deliver a maximum in data quality under any conditions.
2016/11/07
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
2016/10/05
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
2016/08/17
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
2016/02/19
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
2015/11/04
Piezoelectric Measurements with CompactRIO™
2015/06/15
Measurement Solutions for Automotive Test Systems
2015/05/08
Quality Assurance in the Automotive Industry
2015/03/02
How Brose improves the quality of its two-component production and automatically separates defective parts
2014/12/02
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
2014/12/02
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
2011/08/23
HEWI and its Customers Benefit from Cavity Pressure Technology
2011/02/15
End-to-end process monitoring for critical medical moldings
2011/02/07
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
お問合せ
Cara-Isabell Maercklin
Cara-Isabell Maercklin
Media Contact
お問合せ
(max 25 Mb)