Solutions from Kistler Boost Efficiency in Automated Production

Winterthur, 30 August 2016 – At this year's Motek from 10 to 13 October in Stuttgart, Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems. These product innovations represent outstanding examples of the trade show's theme: interconnection in automated production.

 

Especially in sectors where technology is such a strong driving force – such as the automotive industry – the vision of Industry 4.0 is becoming more relevant as time goes on, thanks to increased digitization and the growth of machine and system networking. Even so, not all market players are equally aware of the diverse possibilities for networking that are now available in automated production; nor do they fully appreciate the economic benefits that more transparent production processes can also deliver. As a leading provider of process monitoring systems, Kistler has set itself a specific goal at this year's Motek: to focus attention on this highly relevant issue by showcasing prominent examples of the technologies involved. For joining, forming and testing processes alike: Kistler offers complete systems – from the sensor to the evaluation unit – that can map processes accurately, enabling comparisons and evaluations on a standardized basis across the globe thanks to a consistent operating philosophy. 

 

Electromechanical Joining Systems: Another Addition to Kistler's Portfolio

At this year's Motek, Kistler will premiere its new NCFE (Economy) electromechanical joining module. This new product has been specifically developed for plant manufacturers and operators of conventional power packs. The functionality and design of the NCFE are deliberately geared to simple joining tasks. Plant manufacturers and operators of power packs who opt for the NCFE will benefit from a pre-tested system with integrated process control. This saves time and money on the development of users' own systems – and, because all Kistler process monitoring systems are based on a uniform operating philosophy, seamless integration into the overarching production environment is guaranteed. The NCFE is available for applications in the 10-80 kN measuring range. Kistler is also presenting its NCFR joining module – as well as the classical linear joining process, this system can perform a controlled rotary movement of the ram, either sequentially or even simultaneously.

 

Like the entire family of NC joining systems, all three new products deliver a host of benefits for their users: they offer great flexibility and excellent dynamics combined with simple operation – so simple as well as highly complex joining processes can be implemented rapidly and efficiently with one and the same product family. Thanks to the servo amplifiers used in the products, all traverse movements that are performed can be controlled with high precision. Another example: users of NCFH joining systems can switch between measuring ranges, so completely different components can be manufactured on one and the same plant. Furthermore, end-to-end standardization of the systems means that users can easily obtain spare parts – anywhere in the world. But at the end of the day, future users will probably be convinced by one argument above all others: thanks to their excellent flexibility and low energy consumption, all the joining systems can help the automobile industry and the automotive supply sector to achieve lasting reductions in their series production costs.

 

maXYmos TL 1.2 and maXYmos BL 2.3: the Latest Generation of Monitoring Systems

Yet another highlight is in store for visitors to Kistler's stand: the latest generation of maXYmos monitoring systems. Their purpose: to deliver consistent process-integrated quality assurance. The patterns of measurement curves can be used to monitor and control the quality of a single production step, a sub-assembly or an entire product. Now, maXYmos users can also measure multi-stage production processes (i.e. those with consecutive staggered steps): this has been made possible by equipping the maXYmos TL 1.2 and BL 2.3 with a sequencer mode, in the same way as the successful maXYmos NC. The benefits for users are clear to see: thanks to integrated process control, test processes can now be mapped with no need for costly external PLC programming. The programs can be set up quickly and easily with the help of the intuitive user interface on the touch display. Even for multi-stage processes, optimal cycle times can be achieved with maximum repeat accuracy. Because this control is integrated in the process, the system provides the basis for enhanced transparency in assembly and testing lines – paving the way for increased cost-efficiency throughout the production facility.

 

4503B Torque Sensor: the Rugged Sensor for Maximum Accuracy

Kistler's stand at the Motek will also present the latest state-of-the-art in high-precision torque sensor technology: the Type 4503B torque sensor, which offers a wide range of additional functions. On this new sensor, for instance, optical speed and angle sensing has now been replaced by magnetic technology. This gives the sensor added resilience for reliable operation in heavily contaminated industrial environments – thereby saving valuable time on maintenance. The torque sensor's electronics have also been optimized, and the 4503B now has a cut-off frequency of 10 kHz for highly dynamic measurements. Users can adjust this value individually with the help of an integrated digital low-pass filter, and the second measuring range is freely scalable up to a spread of 1:10. Outstanding features of the Type 4503B also include wide measuring ranges (from 0.2 to 5,000 Nm), integrated speed/angle sensing of up to 8192 pulses/revolution and a high-speed version with up to 50,000 revolutions per minute (1 min/rpm).

 

Save the Trade Show Dates!

If you want to see Kistler's diverse range of solutions for interconnected quality monitoring at first hand, save the dates for the trade show now: it runs from 10 to 13 October 2016 at Motek in Stuttgart.

Press kit

Scarica subito il Media Kit inclusivo di file PDF, Word e immagini ad alta risoluzione: Kistler Press Kit.zip

16/09/2022
At K 2022, Kistler will showcase its solutions for injection molding that make plastics processing more intelligent and sustainable.
06/09/2022
With ComoScout, Kistler offers a simple and cost-effective process monitoring system for injection molding processes.
31/08/2022
High-end measurement systems for rolling stock – from brake testing to traffic monitoring.
22/08/2022
Artificial intelligence in punching: AI helps manufacturers improve product quality and step up their quality assurance.
12/08/2022
New wireless dynamometer allows for highly accurate measurements of cutting forces.
28/07/2022
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
31/05/2022
Kistler showcases needs-oriented solutions for the Smart Factory and presents the extensive software and service resources.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
E’ con grande piacere che Kistler annuncia l’ottenimento dell’approvazione come strumento metrologico (Type Approval) per la soluzione di pesatura dinamica dei veicoli Kistler WIM System 9835A (KiTraffic Basic) fino a 140 km/h per mezzi di peso fino a 4 tonnellate e 120 km/h per mezzi con peso di oltre 4 tonnellate.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Overcoming the complexities of RTM – with Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.