Piezoelectric accelerometer from Kistler measures micro-vibrations even more accurately

Winterthur, July 2022 - The most successful triaxial accelerometer 8763B from Kistler has been improved even further. Its noise thresholds are now significantly lower for all ranges: Thanks to improved testing procedures, thresholds are up to 58 percent lower which allows for more accurate measurements in micro-vibration monitoring. Process improvements additionally led to shorter manufacturing times and increased stock levels – resulting in reduced lead times. 

Measuring micro-vibrations is necessary in many engineering applications: accurate GPS data depends on stable space crafts and satellites, while automobile developers need NVH testing (noise, vibration and harshness) to optimize driving comfort, vehicle performance, durability and reliability. Because micro-vibrations occur in the micro-g range, a highly sensitive measuring chain with very low noise is required for such applications.

Reduced noise thresholds for measurements of micro-vibrations

The IEPE (Integrated Electronics Piezoelectric) triaxial accelerometer 8763B is the most common Kistler sensor used for these measurements and permits vibration monitoring in three mutually perpendicular axes. The measuring threshold determines the smallest possible level of vibrations that can be reliably picked up by the sensor. In 2021, Kistler already improved the noise threshold for the 50-g range. More efficient testing procedures and large investments into Kistler’s facilities have now led to further improvements. The 8763B now features a significantly lower noise threshold for all its ranges: a 58-percent lower noise threshold for its 100-g range, 37 percent for the 250-g range, 52 percent for the 500-g range, 54 percent for the 1000-g range and 51 percent for the sensor’s highest range of 2000 g. With these improvements sensor 8763B becomes even more suitable for common applications, like modal analysis, frequency response measurement and e-motor testing.

Improved availability of triaxial accelerometer

The improved procedures and operations at Kistler have also resulted in shorter lead times and reduced delivery times for the 8763B series on low- to mid-sized orders. With this new process, throughput time has been reduced significantly under optimal conditions. This in turn, also allows for increased safety stock levels to be maintained. At the same time, the availability of subcomponents has improved as well.

The 8763B sensors provide a wide frequency response in each orthogonal axis, making it well-suited for dynamic vibration measurements, especially on lightweight structures. Other features include the sensors’ lightweight hermetic titanium housing and high immunity to base strain thanks to shear element technology. An integral silicone cable variant is available for underwater vibration testing at up to 10 bars. Sensors of the 8763B family can be installed on test objects by either adhesive mounting or flexible studs thanks to three 5-40 threaded holes, making it possible to fully utilize each mounting side of the cube design, ensuring reliable mounting for the calibration of each axis.

Press kit

Scarica subito il Media Kit inclusivo di file PDF, Word e immagini ad alta risoluzione: Kistler Press Kit.zip

16/09/2022
At K 2022, Kistler will showcase its solutions for injection molding that make plastics processing more intelligent and sustainable.
06/09/2022
With ComoScout, Kistler offers a simple and cost-effective process monitoring system for injection molding processes.
31/08/2022
High-end measurement systems for rolling stock – from brake testing to traffic monitoring.
22/08/2022
Artificial intelligence in punching: AI helps manufacturers improve product quality and step up their quality assurance.
12/08/2022
New wireless dynamometer allows for highly accurate measurements of cutting forces.
28/07/2022
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
31/05/2022
Kistler showcases needs-oriented solutions for the Smart Factory and presents the extensive software and service resources.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
E’ con grande piacere che Kistler annuncia l’ottenimento dell’approvazione come strumento metrologico (Type Approval) per la soluzione di pesatura dinamica dei veicoli Kistler WIM System 9835A (KiTraffic Basic) fino a 140 km/h per mezzi di peso fino a 4 tonnellate e 120 km/h per mezzi con peso di oltre 4 tonnellate.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Overcoming the complexities of RTM – with Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.