Kistler adds artificial intelligence to plastics processing

Winterthur, September 2019 – Kistler will present at the K 2019 – the world's largest trade fair for the plastics processing industry – from 16 to 23 October in Düsseldorf. The company's measurement technology experts will welcome visitors to stand G81 in hall 10, where they can learn how artificial intelligence will smooth the path to the smart factories of the future. The Swiss solution provider will showcase intelligent, professional solutions and products for the entire measuring chain, from sensors through to software.

Smart production, networking and data consistency

The process monitoring system ComoNeoPREDICT from Kistler adds artificial intelligence to the injection molding process. The quality model generated by intelligent software is based on neural networks. This is the starting-point for extremely accurate and efficient plastics processing that must meet the very high standards required in the automotive and medtech sectors. Maximum quality can be achieved thanks to this method of calculating the properties of manufactured plastic parts in advance.

Kistler also focuses on end-to-end networking of systems to ensure suitably high levels of data availability. Quality-related process data is made available via OPC UA on a platform-independent basis so that – for example – long-duration analyses can be undertaken and the causes of faults can be identified. A virtual production network will visualize live data from partner companies that operate ComoNeo and are using it for their exhibits at the K 2019 fair.

ComoNeo: the launch-pad for your smart production

ComoNeo from Kistler is the leading system for process monitoring and control in the injection molding sector. It is the core module in the digital value chain, both at horizontal process level on the shop floor and at vertical level for overarching systems. At process level, ComoNeo offers features such as process monitoring based on cavity pressure for conventional and multicomponent injection molding (ComoNeoMERGE). The system also enables automated switchover of the injection molding machine based on cavity pressure (ComoNeoSWITCH) as well as balancing of hot runner control systems (ComoNeoMULTIFLOW). All quality-related process data generated with ComoNeo can be transmitted to higher-level systems such as MES or ERP. All of these advantages make ComoNeo the launch-pad for your smart production.

Cavity pressure measurement to meet the most demanding requirements

Kistler's stand at the fair will include the Innovation Walk, where customers and visitors can experience how cavity pressure measurement is already helping injection molders today – with some glimpses of where the future will take us. The measurement technology value chain begins with the sensor and its centerpiece, the piezoelectric crystal. Learn about the structure of a cavity pressure sensor, and understand the basis for the piezoelectric effect – and how it is utilized. And discover the answer to an important question: why does Kistler grow its own highly specialized crystals?

Cavity pressure sensor technology is fundamentally important for smart plastics processing because it supplies data about the process parameters that are critical for improving part quality. At Kistler's stand, visitors can see how cavity pressure is measured both directly and indirectly – or even contact-free, thanks to the ultra-compact 9239A measuring pin. This product was developed for parts that have to meet the highest standards of surface quality. Another demonstration will showcase Kistler's portfolio of sensors for combined pressure and temperature measurement.

High-efficiency injection molding with ComoNeo: from reproducibility to prediction

ComoNeo from Kistler, the leading process monitoring system, analyzes the measurement data generated by the sensors. The system's seven modular functions give users transparent guidance on optimizing their injection molding production lines:

  • ComoNeoGUARD helps users to define monitoring windows that allow even more reliable assessment of bad parts.
  • ComoNeoMERGE ensures control of the more complex processing requirements when as many as four components with different mold technologies are in use.
  • ComoNeoMULTIFLOW allows hot runner balancing through individual control of the nozzle temperature for molds with multiple cavities.
  • ComoNeoSWITCH ensures automated switchover from the injection phase to the holding pressure phase at the ideal time.
  • ComoNeoCOMPOSITE optimizes the processing of long-fiber composites in the RTM process – assisted by special RTM sensors from Kistler.
  • ComoNeoRECOVER makes it possible to reproduce a proven injection molding process on a different machine – with step-by-step support from the integrated Assistant.
  • ComoNeoPREDICT allows model-based prediction of the desired part quality based on the cavity pressure and temperature profiles.

Kistler's experts will be glad to show you how ComoNeo works in practice. They will demonstrate how the system can be set up and used in line with each customer's requirements – to enhance product quality, prevent scrap and boost overall plant efficiency.

Come and meet Kistler at the K 2019 – on stand G81 in hall 10!

Our experts are looking forward to welcoming you in Düsseldorf from 16 to 23 October. Get to know our intelligent solutions for plastics processors. Learn how Kistler creates added value for its customers throughout the entire measuring chain.

Press kit

Scarica subito il Media Kit inclusivo di file PDF, Word e immagini ad alta risoluzione: Kistler Press Kit.zip

12/08/2022
New wireless dynamometer allows for highly accurate measurements of cutting forces.
28/07/2022
The most successful triaxial accelerometer 8763B measures micro-vibrations even more accurately.
31/05/2022
Kistler showcases needs-oriented solutions for the Smart Factory and presents the extensive software and service resources.
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
The new joining module is highly suitable for clinching and riveting, and also for assembly processes that require force-displacement monitoring.
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
E’ con grande piacere che Kistler annuncia l’ottenimento dell’approvazione come strumento metrologico (Type Approval) per la soluzione di pesatura dinamica dei veicoli Kistler WIM System 9835A (KiTraffic Basic) fino a 140 km/h per mezzi di peso fino a 4 tonnellate e 120 km/h per mezzi con peso di oltre 4 tonnellate.
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
The Kistler Group will showcase its test and analysis systems for threaded joints at the 2019 Fastener Fair in Stuttgart from 19 to 21 March.
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
Accurate and insensitive to its mounting position: the new Type 6044A M8 sensor features an anti-strain design to ensure reliable, high-quality results.
20/11/2018
Motorsport: the new 4080B/BT absolute pressure sensors from Kistler – for real-time monitoring with maximum measurement accuracy and signal quality!
16/10/2018
At Fakuma 2018, the Kistler Group is showcasing its latest monitoring and control packages for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
08/10/2018
The SMETEC Gesellschaft für Sensor-, Motor- und Energietechnik mbH recently became part of the Kistler Group.
24/09/2018
The Kistler Group is adding another variant to what is already the world's most comprehensive portfolio of wheel force measurement systems: the new RoaDyn S6GT 6-component wheel force measurement system.
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
The Kistler Group is introducing a compact mobile measurement solution for enhanced rolling stock maintenance in international railway operations in the shape of its railway brake force measuring system Type 2899A.
21/08/2018
A new Center of Competence for production control and management systems will be opened in Aachen.
31/07/2018
Competent service just a call away has always been a key aspect of Kistler's cooperation with its customers. Now, in a move to address growing demand in North Germany, the measurement technology experts are opening a new office in Wolfsburg.
25/07/2018
On her way to Olympia 2020 she relies on Kistler Group measurement experts.
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
Digitization, Internet of Things and Industry 4.0 are presenting major challenges. Discover how Kistler responds to the great challenges of our times.
09/05/2018
At Sensor + Test 2018 Kistler will be introducing a milestone in measurement technology: its new KiDAQ data acquisition system.
08/05/2018
At NPE 2018, the Kistler Group is showcasing its latest custom monitoring package for ComoNeo, its high-quality process monitoring system that is designed to deliver efficiency and transparency for injection molding.
03/05/2018
At Automatica 2018, the Kistler Group will turn the spotlight on diverse options for using sensors and process monitoring systems to support industrial production and enhance digitalization in test and assembly technology.
24/04/2018
The Kistler Group will showcase its expanded portfolio of industrial test and inspection systems for quality assurance at the 2018 Control trade show.
12/04/2018
The global leader in dynamic measurement technology supports the passion for innovation and technology with a three-year partnership.
06/03/2018
Kistler will be showcasing at Control 2018 its portfolio of industrial testing and inspection systems with the spotlight on the very latest additions.
16/02/2018
At Intertraffic 2018 the Kistler Group is showcasing its comprehensive KiTraffic Weigh In Motion (WIM) solutions, which support road owners and authorities in road and traffic monitoring, weight enforcement and weight-based tolling.
15/02/2018
At NPE 2018 in Orlando, Florida, the Kistler Group will demonstrate a wide range of modular functionalities for ComoNeo: the process monitoring system that takes injection molding to a higher level with integrated quality monitoring geared to meet customers’ needs and requirements.
31/01/2018
The new KiSprint provides coaches and athletes with an efficient means of biomechanically optimizing sprint starts under competitive conditions. The robust and mobile solution has comprehensive software assessment options and can be individually adapted and expanded.
24/01/2018
Kistler achieved a growth rate of 18 % in 2017. Digital transformation has top priority in 2018.
23/01/2018
Overcoming the complexities of RTM – with Kistler
12/10/2017
At the SPS IPC Drives Kistler Group will unveil the world's first digital charge amplifier Type 5974A, a milestone more in electrical automation.
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
With MARS software version 3.0, Kistler presents an extensive update of the proprietary measurement, analysis, and evaluation software for Kistler force plates.
21/10/2016
Kistler boosts the efficiency and reliability of large marine and stationary engines through monitoring and control of the combustion process
19/10/2016
Kistler is presenting the new versions of its ComoNeo and ComoDataCenter.
10/10/2016
Kistler is unveiling a new addition to its portfolio of electromechanical joining modules.
30/09/2016
The Kistler Group reported incoming orders worth CHF 233.3 million at the end of August 2016 and has therefore seen growth of 8.4 % compared to the same period in the previous year, or 5.6 % when adjusted for currency effects.
07/09/2016
At this year's K Trade Fair from 19 to 26 October in Düsseldorf, Kistler will be showcasing its latest new products and features with the focus on Industry 4.0.
24/07/2016
Kistler will be showcasing its new NCFE and NCFR joining modules, together with the latest generation of maXYmos monitoring systems on Motek 2016
12/07/2016
Kistler's Correvit® SFII sensor measures world record in 1.513 seconds
12/05/2016
Screw technology complements the range of applications.
27/04/2016
Following a long phase of planning, preparations, and conversion work, Kistler Instrumente GmbH has a new home for its German headquarters at the Böblingen/Sindelfingen airfield.
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
At Chinaplas 2015 Kistler will be presenting solutions for zero-defect production, process monitoring and data evaluation in injection molding
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
At Sensor + Test 2014 Kistler is presenting many new features from the field of measurement electronics in addition to its already proven sensor technology.
19/05/2014
Users obtain a full range of force–displacement measurement systems from one source
06/02/2014
The Kistler Group achieved sales of 285 million CHF in 2013, thus marking a slight growth in comparison with the figures for the prior year.