Measurement equipment from Kistler plays its part in the development of ultramodern gas turbines

Fuel-flexible gas turbines from MAN Energy Solutions combine high efficiency with low emissions: these pioneering energy supply solutions are an ideal choice for municipal utilities and industrial applications. During the development phase and also in the end product, high-temperature pressure sensors from Kistler deliver valuable real-time data to optimize the combustion process.

The changeover to energy supply solutions that deliver maximum efficiency while protecting the environment is one of the greatest challenges facing humanity in the 21st century. Resources have to be developed and emissions must be reduced against a background of continuously rising demand for energy. Gas turbines play a key part in tackling this challenge: they offer the ideal solution, especially in situations where both power and heat are required – as is often the case in municipal utilities or industrial settings. And in the future, it will become increasingly possible to operate gas turbines with hydrogen instead of natural gas, giving them a better environmental footprint and more compatibility with the desired energy mix.

More sustainable gas turbines of this sort with very low emission values are developed and manufactured at MAN Energy Solutions (MAN ES) in Oberhausen, Germany. The company's Turbomachinery Division, which is based here, traces its origins to the “Gute Hoffnungshütte” (or GHH) which at one time was Europe's largest machinery and plant construction enterprise: GHH began its iron smelting activities as long ago as 1758. Nowadays, some 1,800 employees at Oberhausen work in the competence centers for gas turbine development and production, and in the firm's extensive testing and service operations. On-site facilities include testing of complete gas turbine-compressor trains – the use of gas turbines to drive compressors (on gas pipelines, for example) is another key application area for this technology.

Integrated sensor technology monitors the combustion process

Dr. Bernhard Ćosić, who has been working at MAN Energy Solutions since 2015, leads the company's Gas Turbine Combustion Group and is a key player in the development of the MGT6000 series as well as the new MGT8000 series. Commenting on market trends, he says: “Our gas turbines, which deliver electrical power of between six and twelve megawatts, offer a far more sustainable solution for electricity and heat production than power plants that operate with diesel, coal or heavy fuel oil. Especially in situations that require not only power but also high-temperature heat – in paper production, for instance, or in the food industry – gas turbines achieve very high levels of efficiency. But they can also be used for decentralized power generation, particularly in remote areas where access is difficult, because commissioning costs for gas turbines are many times lower than for large engines.”

To monitor the combustion process and implement other advantages such as fuel flexibility and real-time monitoring, MAN ES opted for Kistler as a development partner. Piezoelectric high-temperature pressure sensors (6021A) from Kistler are connected directly to the gas turbine control; they operate in continuous mode to supply a data feed about the combustion process. “As well as being very compact, these sensors can withstand extremely high temperatures. That means we can position them close to the flame and obtain precise and highly informative data – available to us and our customers 24/7 via the MAN CEON Cloud. In this way, the requirements for condition monitoring and predictive maintenance are met.”

Sensors from Kistler play a major part in controlling and monitoring the combustion process. Alongside emission reduction, fuel flexibility is a key factor here. The MGT6000 series, for example, features dual fuel capability: this means that operation with liquid fuels such as diesel is also possible in the event that no natural gas is available. As Ćosić points out, it is also possible to use shale and other gases and combustion gases that often occur as waste products: these contain high proportions of inert gas such as nitrogen or carbon monoxide, but still have some residual energy. “We optimize combustion processes so that no instabilities occur even when the fuel is changed over – and live data supplied by Kistler sensors helps us here.”

Hydrogen – the fuel of the future

Kistler collaborated with MAN ES to develop a customized electronic unit (the Signal Conditioning Unit) that simplifies the entire measuring chain and contributes significantly to cost optimization. “Throughout the entire period, we received vigorous support from the team headed by Marco Gnielka – and that helped us to arrive at what we see as the optimal solution,” Ćosić adds. “The initial challenges were soon overcome, and Christian Heer – my contact partner at Kistler – is a highly proficient expert on the technology. Although we come from different engineering backgrounds, we quickly developed a working relationship based on trust.”

The next step in the ongoing development of the gas turbine is to enable the use of variable gas mixtures with up to 100 percent hydrogen: this advance holds out the prospect of even cleaner combustion, with CO2 emissions approaching zero. MAN ES has commissioned the first MGT8000 in fall 2020 – right here in Sterkrade, a district of the city of Oberhausen, where it will serve the local municipal utility (EVO). “This new, ultramodern gas turbine can already be operated with a hydrogen share of 20 percent. This could be increased to 50 percent in the short term. And in the medium term, 100 percent will even be possible,” Ćosić explains. “Hydrogen is highly reactive, so it changes the combustion characteristic – the flame burns more quickly, so to speak. That means you have to readjust and optimize the system if there is a major increase in the percentage of hydrogen in the gas mixture. But there are no changes to the basic parameters such as power output and efficiency – operators can continue to use our gas turbines as usual.”

Given that gas turbines have life expectancies of 15 years or more, customers of MAN ES view investment protection as an important criterion. If increasing quantities of hydrogen are fed into the natural gas network in the future – or indeed if new, pure hydrogen systems come into being – measurement technology from Kistler will play its part in the evolution of gas turbines from MAN ES – and that applies to optimization of the combustion processes as well as maintenance and monitoring. Summing up, Ćosić comments: “With Kistler, we have a highly reliable partner who is able to support our business across the globe – for instance, if we want to train staff in China. And Kistler also has the flexibility to offer support and development services on an individual, personal basis. That places us in an excellent position to cope with the growth we expect in the coming years and decades as the necessary phase-out of coal and oil proceeds.”

11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
15/06/2015
Measurement Solutions for Automotive Test Systems
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contatto
Max 25 MB