How advanced pressure sensors from Kistler help researchers to understand sloshing

To gain insights into the complex physics inside cargo containment systems (CCS) partially filled with liquefied natural gas (LNG), the Dutch research institute MARIN has developed a new facility named The Atmosphere (ATM). 100 pressure sensors from Kistler inside the ATM deliver accurate feedback on sloshing wave impacts ‒ a major contribution to improving CCS designs not only for LNG but also, potentially, for hydrogen in the near future.

Natural gas is a cornerstone of cleaner and more sustainable energy provision at global level. Pipelines and shipping are both used to transport this fuel from its natural origins to its destination of use, but shipping is the more economical method ‒ especially over longer distances. Liquid gas is carried at temperatures of around ‒162°C by special-purpose ships known as LNG tankers, sometimes recognizable because of their partly visible spherical tanks. More than 600 of these vessels are already in service throughout the world, and the market is expected to continue growing in the coming years. In terms of design, there is still plenty of scope for optimizing the tank geometry of these ships, but this requires groundbreaking research into the fundamental physical mechanisms behind the processes involved. One phenomenon that is not yet fully understood is sloshing ‒ the motion of a liquid (LNG in this case) inside a container due to external forces (such as the ship's movements): and this is where MARIN plays a key role.

The Maritime Research Institute Netherlands (MARIN) in Wageningen is one of the world's leading marine research centers. Since 1932, MARIN has built up a vast stock of expertise based on a combination of numerical simulations and experiments performed in large-scale facilities comprising various basins for ship model tests, together with on-board measurement and testing. With the backing of a public-private partnership including Dutch universities, industry partners and federal funding, a new globally unique facility was commissioned in 2016. The Atmosphere (ATM) is a giant research facility capable of creating different atmospheric conditions by varying the pressure (0.02‒10 bar), temperature (15‒200°C), type of gas (He, N2, SF6 and water vapor), relative humidity (0‒100%) and other parameters that influence the sloshing dynamics in a real LNG tanker. The ATM consists of an autoclave with an outer diameter of 2.5 m and a length of 15 m ‒ people can actually enter it, but events inside are usually observed through one of the 17 inspection windows.

Precise results under varying environmental conditions

Rodrigo Ezeta, a researcher at MARIN who holds a PhD in Fluid Mechanics, explains the approach as follows: “The Atmosphere offers full environmental control of temperature and pressure: this is relevant for LNG carriers, which normally operate close to the boundary between liquid and vapor. This gives us a better understanding of the sloshing phenomena that occur in a real container inside a ship.” Inside the autoclave lies a flume where waves can be created artificially. As soon as these waves hit the impact wall, pressure sensors from Kistler record the impact loads with a very high degree of accuracy. 100 of these sensors are installed in a T-shaped array. Ezeta again: “During the commissioning phase of the facility, we found that this is the best layout to obtain precise impact loads. The upper part of the T-shaped array allows detailed capture of the loads generated by the wave crest, while the lower part of the T registers the effects of the gas pocket that can be `trapped' in between the wave and the wall.” According to Ezeta, research has already shown that these gas pockets ‒ in addition to the loads generated by the wave crests ‒ can have a non-negligible effect, so they could also exert a detrimental influence on the container.

Synchronized signals from a hundred sensors

Due to their high natural frequency and short rise time, the pressure sensors from Kistler can capture the highly dynamic sloshing events inside the flume. They also feature an optimized membrane to minimize the thermal shock that occurs when sensor exposure changes suddenly from gas to liquid. To prevent noise and bias effects, the Kistler engineers developed a special cable solution that transmits the signals from the test chamber through a vacuum tube to the outside of the autoclave. Signal processing and data acquisition are then handled by 25 automatically synchronized LabAmp 5165A charge amplifiers, which directly digitize the signals of all 100 pressure sensors at a rate of 100 kHz.

We’re very happy with the solution from Kistler. It’s reliable and robust, and it works almost flawlessly.”

Rodrigo Ezeta, Research and Development at MARIN

 

What are the main goals of research at MARIN's The Atmosphere, and what results can be expected? “The installation only became fully operational in early 2020, so we're still at the beginning of our research. One major goal is to improve the scaling models that the industry has used until now,” Ezeta explains. At present, sloshing tests are typically conducted with a small tank on a moving hexapod so as to simulate sloshing. But when the sloshing dynamics are upscaled to real-size dimensions, biases arise in the tests due to the complexity of the underlying physical mechanisms at play.

Ezeta continues: “One of our main objectives is to reduce the uncertainty caused by this scaling. And a good way of doing that is to start by trying to understand the physics behind these impacting events. To achieve this, we perform tests with waves under varying temperature, pressure and gas conditions so we can see the effects on the impact loads that are measured by the Kistler sensors. One key question is: why do the pressures vary so much?” The answer to this question is a topic of active research, because it is influenced by other important aspects such as the appearance of small perturbations along the wave crests, the oscillation of entrapped gas pockets and the magnitude of the gas-to-liquid density ratio, which changes with temperature, pressure and different gas mixtures. This turns out to be a key factor for sloshing events, so it also plays an important part in the design of tanks within ships.

Results also expected to benefit hydrogen tanker design

“Research so far has already shown that it is important to take all physical parameters and effects into account,” Ezeta notes. “Our results will give businesses a better understanding of what is happening inside their tanks, and this will help them to keep on improving their testing methodologies. And, last but not least, our research is an enabler for a new type of tanker that will carry hydrogen rather than natural gas.” In theory, hydrogen is even more sustainable than natural gas because its combustion does not produce any greenhouse gases; however, it has a very low liquefaction temperature of 33 Kelvin (corresponding to ‒253°C under atmospheric conditions). The world's first liquefied hydrogen tankers are expected to become operational in 2021. Rodrigo Ezeta sums up his experience with the measurement technology: “We're very satisfied with our collaboration with Kistler, and we're looking forward to many successful tests thanks to sensors that are renowned for their long-term durability and stability. We are also constantly looking for new collaborations within academia and different industries, where the ATM with it unique features can provide accurate measurements. Our Atmosphere is open to everyone!”

11/04/2022
On the road to success with IEPE and MEMS accelerometers for the ISTAR research aircraft – on the ground and in the air.
14/01/2022
KiTraffic Statistics delivers precise WIM data for a railway bridge in central Austria
18/11/2021
Advanced fastener testing with ANALYSE systems for reliable zink flake coatings in the automotive and wind turbine industries
12/10/2021
How Yuchai achieves more precision, transparency and resource efficiency for its production of engines conform to China VI
14/09/2021
A high precision measuring chain with dynamometer, laboratory charge amplifier and software enables objective comparison tests.
09/09/2021
SRA: Find the best spot and the ideal sensor layout for direct enforcement of overloaded vehicles.
03/09/2021
At Estudio de la Pisada in Valencia, a 3D force plate helps podiatry experts to develop treatments and orthoses for patients and athletes.
02/07/2021
Two IEPE accelerometers deliver key data for propulsion validation and optimization of flight characteristics even in the stratosphere
22/06/2021
Capturing micro-vibrations with a dynamometer leads to improved satellite technology
02/06/2021
Zero defect despite high volumes: this is the way quality assurance with Kistler test automation systems works for zinc die casting parts
26/04/2021
A digitally driven brake force measurement system makes the life of service technicians for train maintenance much easier
13/04/2021
Inside "The Atmosphere" at MARIN, 100 of our pressure sensors capture wave impacts under varying environmental conditions
22/03/2021
How MAN Energy Solutions is using sensors from Kistler to make its gas turbines fit for the future
08/02/2021
Measurement technology dedicated to the discipline and biomechanics of pole vault enables high performances
05/10/2020
How does a digital measuring chain for piezoelectric sensors work as part of a complex vehicle test stand?
18/09/2020
Convincing test results: The Ohio Department of Transportation goes on to apply Lineas from Kistler for traffic monitoring.
20/08/2020
Precision is the key to top performance: how measurement technology from Kistler supports the development team at EMUGE-FRANKEN
22/07/2020
Quality assurance solutions by Kistler like ComoNeo ensure highest accuracy at TSP Precision Tooling in Shanghai.
09/06/2020
Kistler supports Ceratizit in the development of HDT. This enables complex geometries to be produced with just one tool.
15/11/2019
Process monitoring systems and cavity pressure sensors from Kistler help to reduce the amount of scrap drastically
23/10/2019
How measurement technology from Kistler contributes toward boosting high-end powertools' quality
15/08/2019
How the ANALYSE system from Kistler is enhancing safety and transparency in the field of fastening technology
17/07/2019
Turkey opts for weight enforcement with WIM technology from Kistler
24/06/2019
For the next manned flight to the moon: safety that can be measured
20/06/2019
Segregation of good and bad parts every 1.5 seconds: process monitoring with Kistler enables high quality for over 5 million parts per year.
14/05/2019
In order to achieve excellent quality for its components and medical devices, Tessy Plastics chose sensors and solutions from Kistler.
18/04/2019
A renowned manufacturer of electrical appliances trusts testing and sorting systems by Vester to improve its quality.
02/04/2019
NFL's Jaguars boost their fitness levels with Kistler.
25/03/2019
By using process monitoring from Kistler, not only the assembly of electric fuses is validated, but even the function of the sensors itself.
18/03/2019
How to determine the fitness level of an athlete efficiently? A practical report on the Quattro Jump force plate system from Kistler.
17/12/2018
Thanks to precise Weigh in Motion technology from Kistler, Hungary's roads are sustainably protected against overloaded vehicles.
27/11/2018
Bang&Clean relies on Kistler's precise measurement of ignition processes and pressure wave propagation
10/10/2018
Sartorius applies the process monitoring system ComoNeo from Kistler and thereby increases the process quality during injection molding
08/10/2018
The Dortmund Technical University tests the new MicroDyn 9109AA cutting force dynamometer from Kistler and breaks new ground for developing its micromachining processes.
31/08/2018
The ZF company operates a software-controlled Kistler fastener test bench with an integrated vibration unit.
14/08/2018
BIG Daishowa, headquartered in Osaka, Japan, is one of the leading producers of tool holders for the machining industry. Each year the company produces over half a million collet chucks. Their products are developed using, among other resources, Kistler’s cutting force measuring device.
16/07/2018
Enhanced quality and efficiency in mobile crane manufacture – thanks to the test stand for torque tools by Kistler
11/04/2018
The world’s largest provider of rail transport technology relies on Kistler’s measurement expertise. Thanks to the only crash wall of its kind in the world, the impact forces of the trains and their components can be precisely measured and analyzed.
14/11/2017
In the development of cooling lubricants, Blaser Swisslube relies on Kistler's measurement expertise.
11/08/2017
Applus IDIADA relies on DTI in-dummy technology from Kistler for Test Device for Human Occupant Restraint (THOR).
04/01/2017
Road safety is a central topic in vehicle development. Through accurate measurements, Kistler helps increase the chance of survival in crashes.
22/12/2016
Kistler makes progress in vehicle development possible
22/12/2016
Kistler Sensor Correvit® SFII measures world record
20/12/2016
Kistler sensors deliver a maximum in data quality under any conditions.
07/11/2016
Kistler pressure sensors enabled the Rosetta space probe to fly for 6.4 billion kilometers.
05/10/2016
Since the end of 2015 FC Basel is using Kistler force plates to reduce the dropout of young talents.
17/08/2016
Kistler makes the difference in the crucial sports moments with its Performance Analysis System for Swimming.
19/02/2016
Determination of Pump Efficiency with Kistler KiTorq Measuring Flange System
04/11/2015
Piezoelectric Measurements with CompactRIO™
15/06/2015
Measurement Solutions for Automotive Test Systems
08/05/2015
Quality Assurance in the Automotive Industry
02/03/2015
How Brose improves the quality of its two-component production and automatically separates defective parts
02/12/2014
The Kistler Group pursues a growth policy that is both ambitious and sustainable – and strategic acquisitions are one of its core elements. ‘Strategic’ means that Kistler deliberately selects companies which can achieve more together with Kistler than they ever could by continuing alone. The takeover of Dr. Staiger Mohilo & Co. GmbH in 2006 enabled Kistler to grow jointly with the acquired company...
02/12/2014
After a ten-year voyage, the Rosetta space probe's Philae landing module finally touched down on the surface of comet ‘Chury’.
23/08/2011
HEWI and its Customers Benefit from Cavity Pressure Technology
15/02/2011
End-to-end process monitoring for critical medical moldings
07/02/2011
Cavity pressure measurement eliminates short shots at Fischer GmbH & Co KG of Sinsheim/Germany
Contatto
Max 25 MB