- GPS-exchange format GPX
- Garmin database files in formats CRS, HST, TCX
- Garmin FIT, a binary format used (for example) by VIRB cameras
- Google KML
- NMEA (National Marine Electronics Association); multiple common datasets are supported
- FAI-IGC, format defined by FAI, specifically designed for gliding competitions
- Other data formats used in the automotive industry (such as MDF4), containing GPS data, etc.
- Photo importer that can export GPS data from the photo metadata